Cut Chiller Energy Costs by 30%

April 2, 2012 A chiller is often the single largest consumer of power in a building, so it’s a logical place to look for reduced energy costs. Chillers expend excess energy when their compressors run at full-rated constant speed, a wasteful and unnecessary operating condition. Most chillers operate at partial load or are off 99% of the time. A chiller’s compressor motor is typically quite large, in the range of 150 hp to 600 hp. Money saved by operating the compressor motor more efficiently can add up quickly. Read article on www.controleng.com