June 16, 2010 Variable frequency drives (VFD) are becoming more common place and more widely used in applications. They are capable of varying the output speed of a motor without the need for mechanical pulleys, thus reducing the number of mechanical components and overall maintenance. But the biggest advantage that a VFD has is the ability to save the user money through its inherit nature to save energy by consuming only the power that’s needed. The main question now is, How does a VFD accomplish this? The simple answer to this question is power conversion. Read Full Article
|