Global SitesHomeSite MapContact UsSearch
Advanced Search

Application Overview: Machine Tool

The Machine Tool application involves the cutting away or eroding a metal casting or block to create a part, using sharp edge tools. It includes a wide range of skills and requires the use of many different types of tools and specialized machines.

Industrial machines are typically installed as capital equipment. Machine tools are key to industrialization of a country. These machines perform such tasks as turning, boring, milling, drilling, tapping in order to machine simple and complex components in many materials ranging from alloys to plastics.

A machining center, for example, will have three or more axes of motion, an automatic tool changer, and will be computer controlled. One of the main parts of a machining center is the spindle head, which holds the tool that is needed to complete a certain task. A spindle is usually belted to an induction motor. Due to the various tasks that are required, the spindle rotates at various speeds and loads. These speed and load requirements can be met using an AC drive in conjunction with a spindle motor.

Various types of machine tools:

Metal Cutting
  • Boring Machines
  • Station-Type Machines
  • Turning Centers
  • Gear Cutting Machines
  • Broaching Machines
  • Shearing Machines
  • Machining Centers
  • Grinding Machines
  • Drilling Machines
  • Polishing
  • Milling Machines
  • Lathes
  • Electrical Discharge (EDM) Machines


Application Challenges
  • Fast acceleration/deceleration
  • Complex I/O interface
  • Large speed range, high speed operation
  • Continuous operation, repeated forward /reverse
  • High speed and position accuracy
  • Constant high torque production
  • Orientation or positioning
  • Low vibration
  • Low maintenance, durability
  • Fast stopping



Applicable Products
Drives ProductsFeaturesBenefits
A1000 or

G7 Drives
Current LimitSpindle motor can accelerate up in current limit thus providing the fastest acceleration rate possible.
Built-in Dynamic Braking Transistor for commonly used Drive sizes in the Machine Tool IndustryReduced costs when applying Dynamic Braking in order to achieve fast deceleration
Overtorque DetectionThe drive can warn the user of a damaging load related fault situation before it occurs by using Overtorque and/or Undertorque Detection.

This is useful to detect any wear or damage along the cutting blades or bits.

BCD/Binary Digital Input (DI-08,16 options)
  • I/O Interface with numerical controls (NC)
  • Multi-function Inputs and Outputs
  • Speed Agree Output
Energy Saving Mode
(reduces the amount of excitation current that arises with lighter loads)
Suppress any vibration or instability that occurs when performing light machining for the finishing of the work piece.
Zero-Servo and Orientation FunctionStop at a fixed location
Maximum FrequencyHigh speed operation for smooth surface finishing

Variable speed levels can be set by the user with a maximum of 400Hz



Application Details

Refer to individual documents for application details on grinders, lathes, and machining centers.

Additional Information
The pdf contains the same information as the web, but in some cases may contain more and should be used if a printed version is required.


 Application Specifics

 Application Help