Global SitesHomeSite MapContact UsSearch
Advanced Search

Yaskawa MotionWorks IEC61131 Basics

Class Number: TRM010-MotionWorksIEC-61131 Basics
Class Location: Web
Class Cost: $900

Class Topics:
The MotionWorks IEC61131 Basics class is designed to give technicians, engineers and programmers the opportunity to learn the IEC61131-3 programming environment. This class provides a starting point for students that do not have any experience in the IEC environment and a solid refresher for those with experience. After attending this class, the student will be better able to understand the product and functions topics taught in the MP2000iec Application Programming using MotionWorks IEC class. This class is taught by Dr. Ken Ryan from Alexandria Technical College over the web. Class topics include but are not limited to:

1. Why IEC61131-3
a. IEC61131-3 in a Nutshell
b. Value Proposition
c. PLCopen Motion Function Blocks
d. Yaskawa - Providers of Functionality
e. PLCopen - (this is needed for PLCopen Certification)
2. IEC61131-3 Software Model
a. Configuration - Application
b. Resource - MP2300Siec
c. Tasks - Logic Task vs. Motion Task
d. Program Organizational Units - Intro
e. Data Access Paths
3. MotionWorksIEC Development Environment
a. Layout
b. Write a very simple program
4. Common Elements
a. Character set
b. Data Typing
c. Variables
d. Comments (* *)
e. POUs
5. Programming Languages
a. Graphic
b. Textual
6. Creating POUs
7. User defined Data Block
a. Create data type (structure) for top level Function Block created in 6b.
b. Create an array of this data type.
c. Demonstrate how to use this array to do recipe based configuration of the top level function block from 6b.
8. Library creation
a. Store top level Function Block and associated data block as library objects and import into a new project.
9. Create simple state machine using SFC and abbreviated OMAC state model
a. Set up linear SFC with Alternative Parallel branching.
10. Task Configuration
a. Task attributes
b. Set up a Logic Task (slow task)
c. Set up a “Motion Task” (fast task)
Wrap-up

Class Material:
This class is presented over the web. Students will receive instructions how to log in to the web training system.

Prerequisites:
1) Two computers with internet connection, or 1 computer with internet connection and dual monitors
2) Telephone or computer headset

Class Format:
NOTE SPECIAL SCHEDULING: The complete course will be comprised of three live, web-based sessions. The first session of the course begins on Day One at the scheduled time and runs for 4 hours. The second and third session will follow on the next two days at the same scheduled time for 4 hours each. The class consists of approximately 40% lecture and 60% programming exercises.

Overview of the technical setup:
1. You'll be looking at two computer screens and listening on the phone. This means you need 2 computers, or else a computer with dual monitors. One screen displays the WebEx presentation. The other screen is the "Virtual Machine".
2. The "Virtual Machine" is simply a PC that you remotely control from your own computer. The instructor can also see the screen of each of these Virtual Machine PCs and assist you during exercises as needed.
3. You'll call in on the phone to a WebEx conference call in order to communicate with the instructor.

You will be given detailed instructions for testing the virtual machine 1-2 days before class starts.

Continuing Education Units:
Continuing Education Units are not awarded for attending this training class. CEU credits awarded for this class: 0.0

Class Cost:
Please provide a PO for $900 to confirm your enrollment.

To Enroll:
To enroll in any class, call Technical Training Services at 1-800-YASKAWA (927-5292) dial 4. Class sizes are limited, so call early to reserve your seat. PO must be net 30 days.

Cancellation Policy:
Yaskawa reserves the right to cancel a scheduled class at anytime due to low enrollment. In this situation the student will be asked to reschedule or the tuition cost will be refunded. Yaskawa is not liable for any charges incurred by the customer (i.e.; airline, hotel, and rental car) due to cancellation.

Cancellation fee for Yaskawa Authorized Distributors: if canceling within 1 week of the scheduled class is 100% of the total.