Product |  | Date Posted |  | Question | |
 | A1000 Drive |
| |
| | 01/04/2011 | | When will a 120VAC digital input interface be available? |  |
| | 01/04/2011 | | Does the A1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else? |  |
| | 01/04/2011 | | What documentation ships with the product? |  |
| | 01/04/2011 | | When should we begin converting existing F7 business to A1000? |  |
| | 01/04/2011 | | Are F7 Options compatible with A1000? Can A1000 Options be used with F7? |  |
| | 01/04/2011 | | What will happen to the F7? |  |
| | 01/04/2011 | | Are the A1000 network communications full function Modbus or Yaskawa standard? |  |
| | 01/04/2011 | | Is the product ready for shipment? |  |
| | 01/04/2011 | | Is the A1000 the same physical size as F7? |  |
| | 01/04/2011 | | What A1000 enclosure types are available? |  |
| | 02/08/2011 | | What do I do if I am having problems connecting to the A1000 USB port? |  |
| | 01/04/2011 | | Can the 600V models be used with a 690VAC input voltage? |  |
| | 01/03/2011 | | When will end caps (NEMA 1 kits) be available for the protected chassis versions? |  |
| | 01/04/2011 | | How can the design life of the A1000 be twice that of the F7? |  |
| | 01/04/2011 | | Can we replace simple servo applications using existing PM servo motors? |  |
| | 01/04/2011 | | What control methods does the A1000 offer? |  |
| | 01/04/2011 | | In Normal Duty mode, is the default carrier frequency higher than 2kHz? |  |
| | 01/04/2011 | | Is the A1000 dual rated? |  |
| | 01/04/2011 | | What are the A1000’s ratings? |  |
| | 01/04/2011 | | What tools are available to help customers convert from F7 and G5 (600V) to A1000? |  |
| | 01/04/2011 | | Where does the A1000 fit into Yaskawa’s family of drives, and what does it offer beyond the F7? |  |
| | 12/21/2010 | | After installation of DriveWizard Plus on a Dell PC, the following Windows error is displayed when attempting to launch the application: "The application failed to initialize properly (0xc000007b). Click on OK to terminate the application" |  |
| | 12/21/2010 | | Are there plans to replace the P5 600V drive with a new 600V fan/pump HVAC drive? |  |
| | 12/21/2010 | | Are there plans for a dedicated 600V micro-drive? |  |
| | 01/04/2011 | | What are the differences between the A1000 600V and A1000 240/480V models? |  |
| | 12/21/2010 | | When will the rest of the A1000 600V models be released? |  |
| | 01/04/2011 | | When will a heatsink through the back solution be available, and what enclosure rating will it be capable of? |  |
| | 01/04/2011 | | What is EN61800-5-1 and TUV? |  |
| | 01/03/2011 | | What is RoHS? |  |
| | 01/04/2011 | | Will there be a remote keypad option? |  |
| | 01/04/2011 | | Will the A1000 be part of the configured drive program? |  |
| | 01/04/2011 | | When will single phase input capacities be available for A1000 and what kind of derating is expected? |  |
| | 01/04/2011 | | Are there plans to replace the P5 600V drive with a new 600V fan/pump HVAC drive? |  |
| | 01/04/2011 | | Has Yaskawa scheduled any A1000 Factory Training yet? If yes, what are the dates? |  |
| | 01/04/2011 | | Where is the A1000 manufactured? |  |
| | 01/04/2011 | | What is the scan rate of the A1000? |  |
| | 01/04/2011 | | Will DriveWizard Industrial be backward compatible? |  |
 | AC Motors |
| |
| | 08/02/2005 | | Is it possible to control multiple motors from a single AC drive? |  |
| | 08/19/2004 | | What are the concerns when operating a motor with a AC drive rated for less output voltage than the motor namplate .
Example: The AC drive rating is 480 VAC and the motor is 600VAC. |  |
 | Any AC Drive |
| |
| | 07/13/2004 | | What happens if the STOP button on the Digital Operator is pressed, while the drive is being controlled remotely by START/STOP circuitry connected to the drives I/O terminal block? Can the drive be restarted locally? |  |
| | 07/13/2004 | | Can I control Start/Stop of my drive by just applying and removing input power? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 07/13/2004 | | What is 2-Wire Control and 3-Wire Control? |  |
| | 08/02/2005 | | Is it possible to control multiple motors from a single AC drive? |  |
| | 08/19/2004 | | What are the concerns when operating a motor with a AC drive rated for less output voltage than the motor namplate .
Example: The AC drive rating is 480 VAC and the motor is 600VAC. |  |
| | 10/27/2005 | | Can the brake coil of a brake-motor be put directly across the motor winding when the motor is run by a VFD? |  |
| | 07/13/2004 | | How does electronic thermal (motor protection) work? |  |
| | 02/12/2003 | | How to reform the DC bus capacitors on an Variable Speed AC drive that has been stored for more than 12 months. |  |
| | 12/13/2002 | | The AC drive repeatedly displays an OV (Overvoltage) fault when the inverter is stopping. What causes this? |  |
| | 06/24/2003 | | What is a "Multi-Function Digital Input"? |  |
 | Bypass Unit |
| |
| | 01/16/2003 | | C21 unit is connected and runs in Hand and Auto fine. But, the input circuit breaker is tripping while attempting to run in Bypass mode. Why? |  |
 | DC5 Converter |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
 | DriveWizard Plus Software |
| |
| | 12/21/2010 | | After installation of DriveWizard Plus on a Dell PC, the following Windows error is displayed when attempting to launch the application: "The application failed to initialize properly (0xc000007b). Click on OK to terminate the application" |  |
 | DriveWizard Software |
| |
| | 11/01/2010 | | What do I do when I receive a "Selected collating sequence not supported by the operating system" error when running DriveWizard 6.2? |  |
| | 11/29/2005 | | What software tools are available to save F7 drive parameter settings to a PC file?
|  |
| | 07/13/2004 | | The Drive Wizard .PARMS file was edited with another program (ie. Microsoft Word, Notepad) and saved. When reopened with DriveWizard, an error code of "File Error" was displayed on-screen. What is the problem and how can this be corrected? |  |
| | 07/13/2004 | | Can the DriveWizard .PARMS files be viewed without running the DriveWizard program? |  |
 | E7 Drive |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/13/2004 | | When the E7 drive trips out on a fault it must be manually reset. Can the E7 be set to restart automatically after a fault? |  |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | How can the Yaskawa E7 drive start a fan that is windmilling in the opposite direction? |  |
| | 07/13/2004 | | Can the E7 keypad display cooling fan operating hours? (for maintenance purposes)
|  |
| | 07/13/2004 | | When entering Motor Rated Current (parameter E2-01) into an E7 drive, an OPE02 fault appears on the display. What can cause this, and how is the fault cleared?
|  |
| | 07/13/2004 | | Resetting a drive fault. |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 03/14/2006 | | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |  |
| | 10/31/2005 | | What is required to start and stop the GPD515/G5 from the digital operator?
|  |
| | 07/13/2004 | | What is the ambient temperature derating (L8-12 setting)? |  |
| | 10/31/2005 | | Can a MCCB rated higher than the recommended rating, be installed ahead of a drive to supply the 3 phase power? |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 03/14/2006 | | How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter? |  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 07/13/2004 | | Is it possible to adjust the brightness for the operator display? |  |
| | 07/13/2004 | | What are some concerns when the motor cable is over 100 meters? |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
| | 02/19/2003 | | What is the specification of 12 pulse input transformer E7 and F7 AC Drives? |  |
 | E7B Drive Bypass |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/28/2004 | | Can a remote Hand/Off/Auto switch be connected to the E7B product? |  |
| | 10/27/2005 | | What is the purpose of the TEST switch on the front panel of an E7B bypass unit? |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 06/29/2006 | | What settings are needed to configure the E7 Bypass for serial communication control in AUTO mode and keypad speed control in HAND mode?
|  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 10/27/2005 | | The E7B bypass unit with the serial communications, option J or option L control comes set up for the start/stop
as well as the speed reference to be controlled through serial communication.
Is it possible to maintain start/stop control through serial communication
while using an analog signal for speed reference? |  |
| | 07/13/2004 | | The E7 drive inside the bypass enclosure unit doesn’t have the Hand, Off or Auto buttons that are shown in the E7 manual. How can the drive be run locally? |  |
 | E7BR Package |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
 | E7C Drive Configured |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
 | E7CR Package |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
 | E7E Drive Engineered |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
 | E7L Drive Bypass |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/13/2004 | | The E7L will not run the motor in Hand or Auto mode.
--OTHER SYMPTOMS:
1. Drive LED flashes.
2. Stop LED is lit.
3. Contol Power LED is lit.
4. No Ready LED.
What can cause this? |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
 | E7N Narrow Bypass Package |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
 | E7S Slim Configured Package |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
 | F7 Drive |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 03/14/2006 | | Power Line Harmonics and Installation Considerations for AC and DC Drives |  |
| | 11/29/2005 | | What software tools are available to save F7 drive parameter settings to a PC file?
|  |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 11/08/2005 | | What are the differences between the set-up of a GPD515/G5 and a F7 drive on DeviceNet when using CM053 or CM056 option cards? |  |
| | 07/13/2004 | | Resetting a drive fault. |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 03/14/2006 | | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |  |
| | 10/31/2005 | | What is required to start and stop the GPD515/G5 from the digital operator?
|  |
| | 07/13/2004 | | What is the ambient temperature derating (L8-12 setting)? |  |
| | 10/31/2005 | | Can a MCCB rated higher than the recommended rating, be installed ahead of a drive to supply the 3 phase power? |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 03/14/2006 | | How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter? |  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 07/13/2004 | | Is it possible to use auto-tuning without rotating the motor? |  |
| | 10/28/2005 | | What kinds of applications is the F7 suited for? |  |
| | 10/28/2005 | | What type of product is the F7? |  |
| | 07/13/2004 | | Is it possible to adjust the brightness for the operator display? |  |
| | 10/31/2005 | | What is the range of voltage fluctuation allowed? |  |
| | 07/13/2004 | | What is the meaning of CAL or CALL on the keypad display?. |  |
| | 07/13/2004 | | What are some concerns when the motor cable is over 100 meters? |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
| | 02/19/2003 | | What is the specification of 12 pulse input transformer E7 and F7 AC Drives? |  |
 | G3 GPD503 Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | Why don’t the page numbers in the parameter section of the instruction manual match the page numbers in the body of the manual?
|  |
| | 07/13/2004 | | On the GPD503, why does the Stop LED continue to flash after the drive has stopped runnning? |  |
 | G5 Drive 600 Volt |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | The GPD/515G5 instruction manual (TOE-S616-10.13) (pages 21-22) specifies that input fuses should be used on the installation of these drives.
--Is fusing required or is a circuit breaker sufficient protection for the inverter.
--If fusing is not required, what characteristics of MCCB should used be to protect the drive adequately. |  |
| | 11/08/2005 | | What are the differences between the set-up of a GPD515/G5 and a F7 drive on DeviceNet when using CM053 or CM056 option cards? |  |
| | 07/13/2004 | | Resetting a drive fault. |  |
| | 03/14/2006 | | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |  |
| | 10/31/2005 | | What is required to start and stop the GPD515/G5 from the digital operator?
|  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 03/14/2006 | | How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter? |  |
| | 07/13/2004 | | Why don’t the page numbers in the parameter section of the instruction manual match the page numbers in the body of the manual?
|  |
| | 07/13/2004 | | Is there a way to "lock out" unauthorized programming of the GPD515/G5? |  |
| | 11/28/2005 | | Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters? |  |
| | 07/13/2004 | | On the GPD 515/G5, If Terminal 1 to 11 are closed, but the GPD515/G5 inverter still does not run. What is wrong? |  |
| | 07/13/2004 | | The GPD 515/G5 displays a parameter, but does not let me change it. Why? |  |
| | 07/13/2004 | | Can the 'run' contact output of the GPD 515/G5 be used to release a mechanical brake? |  |
| | 10/11/2004 | | Can the GPD 506/P5 be programmed in other languages? |  |
| | 07/13/2004 | | On the GPD 515/G5, can the 15V at pin-15 power a proximity sensor? |  |
| | 07/13/2004 | | What is the current rating for the Run and Fault output contacts on a GPD 515/G5? |  |
| | 07/13/2004 | | Can an external 24V power supply be used with the GPD515/G5 Logic Inputs? |  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 07/13/2004 | | In what languages can the GPD 515/G5 display? |  |
| | 07/13/2004 | | What overload protection does the GPD 515/G5 have? |  |
| | 07/13/2004 | | Can the GPD 515/G5 do closed loop speed control? |  |
| | 07/13/2004 | | CALL SI-F/G ComCall -- Fault Code Description |  |
| | 07/13/2004 | | CALL -- Fault Code Description |  |
| | 07/13/2004 | | OPE11 -- Fault Code Description |  |
| | 07/13/2004 | | OPE10 -- Fault Code Description |  |
| | 07/13/2004 | | OPE08 -- Fault Code Description |  |
| | 07/13/2004 | | OPE07 - Fault Code Description |  |
| | 07/13/2004 | | OPE06 -- Fault Code Description |  |
| | 07/13/2004 | | OPE05 -- Fault Code Description |  |
| | 07/13/2004 | | OPE03 -- Fault Code Description |  |
| | 07/13/2004 | | OPE02 -- Fault Code Description |  |
| | 07/13/2004 | | OPE01 -- Fault Code Description |  |
| | 07/13/2004 | | BB -- Fault Code Description |  |
| | 07/13/2004 | | EF -- Fault Code Description |  |
| | 07/13/2004 | | OH2 -- Fault Code Description |  |
| | 07/13/2004 | | OH -- Fault Code Description |  |
| | 07/13/2004 | | OV -- Fault Code Description |  |
| | 07/13/2004 | | UV -- Fault Code Description |  |
| | 07/13/2004 | | CPF23 -- Fault Code Description |  |
| | 07/13/2004 | | CPF22 -- Fault Code Description |  |
| | 07/13/2004 | | CPF21 -- Fault Code Description |  |
| | 07/13/2004 | | CPF20 -- Fault Code Description |  |
| | 07/13/2004 | | CPF06 -- Fault Code Description |  |
| | 07/13/2004 | | CPF05 -- Fault Code Description |  |
| | 07/13/2004 | | CPF04 -- Fault Code Desciption |  |
| | 07/13/2004 | | CPF03 -- Fault Code Description |  |
| | 07/13/2004 | | CPF02 -- Fault Code Description |  |
| | 07/13/2004 | | CPF01 -- Fault Code Description |  |
| | 07/13/2004 | | CPF00 -- Fault Code Description |  |
| | 07/13/2004 | | ERR -- Fault Code Description |  |
| | 07/13/2004 | | DEV -- Fault Code Description |  |
| | 07/13/2004 | | EF0 -- Fault Code Description |  |
| | 07/13/2004 | | EF4~8 -- Fault Code Description |  |
| | 07/13/2004 | | EF3 -- Fault Code Description |  |
| | 07/13/2004 | | CE -- Fault Code Description |  |
| | 07/13/2004 | | BUS -- Fault Code Description |  |
| | 07/13/2004 | | E-15 -- Fault Code Description |  |
| | 07/13/2004 | | E-10 -- Fault Code Description |  |
| | 07/13/2004 | | OPR -- Fault Code Description |  |
| | 07/13/2004 | | OH1 -- Fault Code Description |  |
| | 07/13/2004 | | SVE -- Fault Code Description |  |
| | 07/13/2004 | | CF -- Fault Code Description |  |
| | 07/13/2004 | | RH -- Fault Code Description |  |
| | 07/13/2004 | | RR -- Fault Code Description |  |
| | 07/13/2004 | | PGO -- Fault Code Description |  |
| | 07/13/2004 | | OS -- Fault Code Description |  |
| | 07/13/2004 | | LF -- Fault Code Description |  |
| | 07/13/2004 | | PF - Fault Code Description |  |
| | 07/13/2004 | | OL4 -- Fault Code Description |  |
| | 07/13/2004 | | OL3 -- Fault Code Description |  |
| | 07/13/2004 | | OL2 -- Fault Code Description |  |
| | 07/13/2004 | | OL1 -- Fault Code Description |  |
| | 07/13/2004 | | PUF -- Fault Code Description |  |
| | 07/13/2004 | | SC - Fault Code Description |  |
| | 07/13/2004 | | GF - Fault Code Description |  |
| | 07/13/2004 | | OC -- Fault Code Description |  |
| | 07/13/2004 | | OV - Fault Code Description |  |
| | 07/13/2004 | | UV3 - Fault Code Description |  |
| | 07/13/2004 | | UV2 - Fault Code Description |  |
| | 07/13/2004 | | UV1 - Fault Code Description |  |
| | 07/13/2004 | | oH1 fault - Fault Code Description |  |
| | 07/13/2004 | | Can the inverter still be used if the input voltage exceeds the permissible voltage fluctuation range (-15% to +10%)? |  |
| | 07/13/2004 | | What are some concerns when the motor cable is over 100 meters? |  |
| | 07/13/2004 | | Is there a way to perform an initialization without losing the parameter settings? |  |
| | 11/28/2005 | | Is there a way to clear the fault history? |  |
| | 10/27/2005 | | If the drives carrier frequency is changed , is it necessary to re-autotune the drive?
|  |
| | 08/19/2004 | | What is the cable pin out for the following cable.
P/N uwr00103-1 for used with the Drive Wizard ?
|  |
| | 10/26/2005 | | Can the G5 GPD515 drive in flux vector mode can run above 1750 RPM/60 Hz. If so what parameters would need to be changed to accomplish this. We only want to go to 2100 RPM/72 Hz. |  |
| | 02/24/2003 | | How to identify a G5 vs. G5+ AC drive. |  |
| | 01/10/2003 | | Can a negative speed reference be used to command the drive to reverse direction when using the Profibus option? |  |
 | G5 GPD515 Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | The GPD/515G5 instruction manual (TOE-S616-10.13) (pages 21-22) specifies that input fuses should be used on the installation of these drives.
--Is fusing required or is a circuit breaker sufficient protection for the inverter.
--If fusing is not required, what characteristics of MCCB should used be to protect the drive adequately. |  |
| | 11/08/2005 | | What are the differences between the set-up of a GPD515/G5 and a F7 drive on DeviceNet when using CM053 or CM056 option cards? |  |
| | 07/13/2004 | | Resetting a drive fault. |  |
| | 10/31/2005 | | What is required to start and stop the GPD515/G5 from the digital operator?
|  |
| | 07/13/2004 | | Why don’t the page numbers in the parameter section of the instruction manual match the page numbers in the body of the manual?
|  |
| | 07/13/2004 | | Is there a way to "lock out" unauthorized programming of the GPD515/G5? |  |
| | 11/28/2005 | | Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters? |  |
| | 07/13/2004 | | On the GPD 515/G5, If Terminal 1 to 11 are closed, but the GPD515/G5 inverter still does not run. What is wrong? |  |
| | 07/13/2004 | | The GPD 515/G5 displays a parameter, but does not let me change it. Why? |  |
| | 07/13/2004 | | Can the 'run' contact output of the GPD 515/G5 be used to release a mechanical brake? |  |
| | 10/11/2004 | | Can the GPD 506/P5 be programmed in other languages? |  |
| | 07/13/2004 | | On the GPD 515/G5, can the 15V at pin-15 power a proximity sensor? |  |
| | 07/13/2004 | | What is the current rating for the Run and Fault output contacts on a GPD 515/G5? |  |
| | 07/13/2004 | | Can an external 24V power supply be used with the GPD515/G5 Logic Inputs? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 07/13/2004 | | In what languages can the GPD 515/G5 display? |  |
| | 07/13/2004 | | What overload protection does the GPD 515/G5 have? |  |
| | 07/13/2004 | | Can the GPD 515/G5 do closed loop speed control? |  |
| | 07/13/2004 | | CALL SI-F/G ComCall -- Fault Code Description |  |
| | 07/13/2004 | | CALL -- Fault Code Description |  |
| | 07/13/2004 | | OPE11 -- Fault Code Description |  |
| | 07/13/2004 | | OPE10 -- Fault Code Description |  |
| | 07/13/2004 | | OPE08 -- Fault Code Description |  |
| | 07/13/2004 | | OPE07 - Fault Code Description |  |
| | 07/13/2004 | | OPE06 -- Fault Code Description |  |
| | 07/13/2004 | | OPE05 -- Fault Code Description |  |
| | 07/13/2004 | | OPE03 -- Fault Code Description |  |
| | 07/13/2004 | | OPE02 -- Fault Code Description |  |
| | 07/13/2004 | | OPE01 -- Fault Code Description |  |
| | 07/13/2004 | | BB -- Fault Code Description |  |
| | 07/13/2004 | | EF -- Fault Code Description |  |
| | 07/13/2004 | | OH2 -- Fault Code Description |  |
| | 07/13/2004 | | OH -- Fault Code Description |  |
| | 07/13/2004 | | OV -- Fault Code Description |  |
| | 07/13/2004 | | UV -- Fault Code Description |  |
| | 07/13/2004 | | CPF23 -- Fault Code Description |  |
| | 07/13/2004 | | CPF22 -- Fault Code Description |  |
| | 07/13/2004 | | CPF21 -- Fault Code Description |  |
| | 07/13/2004 | | CPF20 -- Fault Code Description |  |
| | 07/13/2004 | | CPF06 -- Fault Code Description |  |
| | 07/13/2004 | | CPF05 -- Fault Code Description |  |
| | 07/13/2004 | | CPF04 -- Fault Code Desciption |  |
| | 07/13/2004 | | CPF03 -- Fault Code Description |  |
| | 07/13/2004 | | CPF02 -- Fault Code Description |  |
| | 07/13/2004 | | CPF01 -- Fault Code Description |  |
| | 07/13/2004 | | CPF00 -- Fault Code Description |  |
| | 07/13/2004 | | ERR -- Fault Code Description |  |
| | 07/13/2004 | | DEV -- Fault Code Description |  |
| | 07/13/2004 | | EF0 -- Fault Code Description |  |
| | 07/13/2004 | | EF4~8 -- Fault Code Description |  |
| | 07/13/2004 | | EF3 -- Fault Code Description |  |
| | 07/13/2004 | | CE -- Fault Code Description |  |
| | 07/13/2004 | | BUS -- Fault Code Description |  |
| | 07/13/2004 | | E-15 -- Fault Code Description |  |
| | 07/13/2004 | | E-10 -- Fault Code Description |  |
| | 07/13/2004 | | OPR -- Fault Code Description |  |
| | 07/13/2004 | | OH1 -- Fault Code Description |  |
| | 07/13/2004 | | SVE -- Fault Code Description |  |
| | 07/13/2004 | | CF -- Fault Code Description |  |
| | 07/13/2004 | | RH -- Fault Code Description |  |
| | 07/13/2004 | | RR -- Fault Code Description |  |
| | 07/13/2004 | | PGO -- Fault Code Description |  |
| | 07/13/2004 | | OS -- Fault Code Description |  |
| | 07/13/2004 | | LF -- Fault Code Description |  |
| | 07/13/2004 | | PF - Fault Code Description |  |
| | 07/13/2004 | | OL4 -- Fault Code Description |  |
| | 07/13/2004 | | OL3 -- Fault Code Description |  |
| | 07/13/2004 | | OL2 -- Fault Code Description |  |
| | 07/13/2004 | | OL1 -- Fault Code Description |  |
| | 07/13/2004 | | PUF -- Fault Code Description |  |
| | 07/13/2004 | | SC - Fault Code Description |  |
| | 07/13/2004 | | GF - Fault Code Description |  |
| | 07/13/2004 | | OC -- Fault Code Description |  |
| | 07/13/2004 | | OV - Fault Code Description |  |
| | 07/13/2004 | | UV3 - Fault Code Description |  |
| | 07/13/2004 | | UV2 - Fault Code Description |  |
| | 07/13/2004 | | UV1 - Fault Code Description |  |
| | 07/13/2004 | | oH1 fault - Fault Code Description |  |
| | 07/13/2004 | | Can the inverter still be used if the input voltage exceeds the permissible voltage fluctuation range (-15% to +10%)? |  |
| | 07/13/2004 | | What are some concerns when the motor cable is over 100 meters? |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
| | 07/13/2004 | | Is there a way to perform an initialization without losing the parameter settings? |  |
| | 11/28/2005 | | Is there a way to clear the fault history? |  |
| | 10/27/2005 | | If the drives carrier frequency is changed , is it necessary to re-autotune the drive?
|  |
| | 08/19/2004 | | What is the cable pin out for the following cable.
P/N uwr00103-1 for used with the Drive Wizard ?
|  |
| | 10/26/2005 | | Can the G5 GPD515 drive in flux vector mode can run above 1750 RPM/60 Hz. If so what parameters would need to be changed to accomplish this. We only want to go to 2100 RPM/72 Hz. |  |
| | 02/24/2003 | | How to identify a G5 vs. G5+ AC drive. |  |
| | 01/10/2003 | | Can a negative speed reference be used to command the drive to reverse direction when using the Profibus option? |  |
 | G5HHP Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 03/14/2006 | | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |  |
| | 10/31/2005 | | What is required to start and stop the GPD515/G5 from the digital operator?
|  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 03/14/2006 | | How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter? |  |
| | 07/13/2004 | | Is there a way to "lock out" unauthorized programming of the GPD515/G5? |  |
| | 11/28/2005 | | Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters? |  |
| | 10/11/2004 | | Can the GPD 506/P5 be programmed in other languages? |  |
| | 07/13/2004 | | What is the current rating for the Run and Fault output contacts on a GPD 515/G5? |  |
| | 07/13/2004 | | Can an external 24V power supply be used with the GPD515/G5 Logic Inputs? |  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 07/13/2004 | | In what languages can the GPD 515/G5 display? |  |
| | 07/13/2004 | | What overload protection does the GPD 515/G5 have? |  |
| | 07/13/2004 | | Can the GPD 515/G5 do closed loop speed control? |  |
| | 07/13/2004 | | CPF23 -- Fault Code Description |  |
| | 07/13/2004 | | CPF22 -- Fault Code Description |  |
| | 07/13/2004 | | CPF06 -- Fault Code Description |  |
| | 07/13/2004 | | CPF05 -- Fault Code Description |  |
| | 07/13/2004 | | CPF04 -- Fault Code Desciption |  |
| | 07/13/2004 | | CPF03 -- Fault Code Description |  |
| | 07/13/2004 | | CPF02 -- Fault Code Description |  |
| | 07/13/2004 | | CPF01 -- Fault Code Description |  |
| | 07/13/2004 | | CPF00 -- Fault Code Description |  |
| | 07/13/2004 | | ERR -- Fault Code Description |  |
| | 07/13/2004 | | DEV -- Fault Code Description |  |
| | 07/13/2004 | | EF0 -- Fault Code Description |  |
| | 07/13/2004 | | EF3 -- Fault Code Description |  |
| | 07/13/2004 | | CE -- Fault Code Description |  |
| | 07/13/2004 | | BUS -- Fault Code Description |  |
| | 07/13/2004 | | E-15 -- Fault Code Description |  |
| | 07/13/2004 | | E-10 -- Fault Code Description |  |
| | 07/13/2004 | | OPR -- Fault Code Description |  |
| | 07/13/2004 | | OH1 -- Fault Code Description |  |
| | 07/13/2004 | | RR -- Fault Code Description |  |
| | 07/13/2004 | | LF -- Fault Code Description |  |
| | 07/13/2004 | | PF - Fault Code Description |  |
| | 07/13/2004 | | OL4 -- Fault Code Description |  |
| | 07/13/2004 | | OL3 -- Fault Code Description |  |
| | 07/13/2004 | | OL2 -- Fault Code Description |  |
| | 07/13/2004 | | OL1 -- Fault Code Description |  |
| | 07/13/2004 | | PUF -- Fault Code Description |  |
| | 07/13/2004 | | SC - Fault Code Description |  |
| | 07/13/2004 | | GF - Fault Code Description |  |
| | 07/13/2004 | | UV1 - Fault Code Description |  |
| | 07/13/2004 | | What are some counter-measures to reduce harmonics created by AC drives? |  |
| | 07/13/2004 | | Can the inverter still be used if the input voltage exceeds the permissible voltage fluctuation range (-15% to +10%)? |  |
| | 07/13/2004 | | What are some concerns when the motor cable is over 100 meters? |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
| | 07/13/2004 | | Is there a way to perform an initialization without losing the parameter settings? |  |
| | 10/26/2005 | | Can the G5 GPD515 drive in flux vector mode can run above 1750 RPM/60 Hz. If so what parameters would need to be changed to accomplish this. We only want to go to 2100 RPM/72 Hz. |  |
| | 01/10/2003 | | Can a negative speed reference be used to command the drive to reverse direction when using the Profibus option? |  |
 | G7 Drive |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | Resetting a drive fault. |  |
| | 07/13/2004 | | What is the ambient temperature derating (L8-12 setting)? |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 07/13/2004 | | Is it possible to use auto-tuning without rotating the motor? |  |
| | 07/13/2004 | | Is it possible to adjust the brightness for the operator display? |  |
| | 07/13/2004 | | What are some counter-measures to reduce harmonics created by AC drives? |  |
| | 07/13/2004 | | What is the meaning of CAL or CALL on the keypad display?. |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
 | H5 Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
 | iQPUMP Controller |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
 | J1000 Drive |
| |
| | 12/21/2010 | | After installation of DriveWizard Plus on a Dell PC, the following Windows error is displayed when attempting to launch the application: "The application failed to initialize properly (0xc000007b). Click on OK to terminate the application" |  |
| | 08/04/2008 | | Does the J1000 have a removable terminal block with parameter copy capability, like the V1000? |  |
| | 07/31/2008 | | Does the J1000 have DWEZ capability? |  |
| | 07/31/2008 | | What about CASE Software? |  |
| | 07/31/2008 | | Will DriveWizardTM Plus be backward compatible? |  |
| | 07/31/2008 | | Do we have a USB cable interface (instead of serial) for hookup to laptops for DriveWizardTM Plus? |  |
| | 07/31/2008 | | Is the Copy function available with the standard LED keypad? |  |
| | 07/31/2008 | | Are J7 Options compatible with J1000? |  |
| | 07/31/2008 | | What documentation ships with the product? |  |
| | 07/31/2008 | | Does the J1000 have any network communications capability? |  |
| | 07/31/2008 | | What enclosure types are available? |  |
| | 07/31/2008 | | Is the J1000 the same physical size as J7? |  |
| | 07/31/2008 | | Is the design life of the J1000 twice that of the J7? |  |
| | 07/31/2008 | | Does the J1000 have dynamic braking capability now? |  |
| | 07/31/2008 | | Does the J1000 mount contactor-style, like the J7 did? |  |
| | 07/31/2008 | | Does J1000 have UL Listing for single phase? |  |
| | 07/31/2008 | | Does the J1000 have RoHS compliance? What is RoHS? |  |
| | 07/31/2008 | | What Control Methods does the J1000 offer? |  |
| | 07/31/2008 | | In Normal Duty mode, is the default carrier frequency higher than 2kHz? |  |
| | 07/31/2008 | | Is the J1000 dual rated? |  |
| | 07/31/2008 | | Do you or will you offer 115V single-phase? |  |
| | 07/31/2008 | | What are the J1000’s ratings? |  |
| | 07/31/2008 | | When should we begin converting existing J7 business to J1000? |  |
| | 07/31/2008 | | Has Yaskawa scheduled any J1000 Factory Training yet? If yes what are the dates? |  |
| | 07/31/2008 | | Where is the J1000 manufactured? |  |
| | 07/31/2008 | | Does the J1000 replace the J7? |  |
| | 07/31/2008 | | What are the differences between J7 and J1000? |  |
 | J7 Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 03/14/2006 | | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 03/14/2006 | | How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter? |  |
| | 07/13/2004 | | Why don’t the page numbers in the parameter section of the instruction manual match the page numbers in the body of the manual?
|  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 10/11/2004 | | Can a Dynamic Braking resistor be installed on a J7 Drive? |  |
| | 10/27/2005 | | Is PID available on the J7 Drive? |  |
| | 07/13/2004 | | What is the meaning of CAL or CALL on the keypad display?. |  |
| | 10/27/2005 | | Can the J7 Drive be used with a single-phase, 100V input? |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
| | 07/13/2004 | | What happens if a forward command and a reverse command are closed on the terminal block at the same time? |  |
| | 07/13/2004 | | How do I enter the Run Command from the control circuit terminals? |  |
| | 10/27/2005 | | Can a J7 Drove fault be indicated by a drive relay output signal? |  |
| | 11/28/2005 | | Can output current be monitored via Analog Output? |  |
| | 07/13/2004 | | How can the gain be changed for an Analog Input? |  |
| | 07/13/2004 | | On the J7 drive, can the input reference terminal FR still be used when the drive is programmed for Up/Down control? |  |
| | 11/28/2005 | | Can the keypad from J7 Drive be removed and installed at a remote location? If yes what is the part no. of the cable and what is the distance it can support? |  |
| | 10/27/2005 | | I am currently using the V7 Drive with a frequency input (terminal RP) and a want to use the J7 Drive in its place. Is this going to work? |  |
| | 12/13/2002 | | The J7 drive will only allow the parameter to viewed but not changed.
What must be done to change parameter values in the J7/305 AC drive? |  |
| | 06/23/2003 | | How is the inverter reset after an alarm has gone off? |  |
 | Network Comms-DeviceNet |
| |
| | 11/08/2005 | | What are the differences between the set-up of a GPD515/G5 and a F7 drive on DeviceNet when using CM053 or CM056 option cards? |  |
 | Network Comms-Lonworks |
| |
| | 07/13/2004 | | Serial communication is lost intermittently between the building automation system (BAS) and a Lonworks board on the GPD506 / P5 drive. What might be causing this? |  |
 | Network Comms-Modbus |
| |
| | 07/13/2004 | | Does the Modbus port on the V7 Drive need a termination resistor? |  |
 | Network Comms-Profibus |
| |
| | 01/10/2003 | | Can a negative speed reference be used to command the drive to reverse direction when using the Profibus option? |  |
 | Network Comms - Landis FLN |
| |
| | 07/13/2004 | | A Siemens Apogee FLN option board is installed on GPD506 bypass drive so a run command can be initiated through network communications. After a safety circuit fault has been reset, the drive will not run again even though it has been commanded to. Why is this happening? |  |
 | P5 Drive 600 Volt |
| |
| | 12/21/2010 | | Are there plans to replace the P5 600V drive with a new 600V fan/pump HVAC drive? |  |
| | 07/13/2004 | | What is the vertical and horizontal clearance specification (in inches) for mounting any of the GPD506/P5 stand alone drives? |  |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | What is the purpose of a softcharge resistor and contactor in a GPD506 / P5 drive? |  |
| | 03/14/2006 | | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |  |
| | 11/28/2005 | | Which PID parameters require set-up when configuring the GPD506 / P5 drive for PID pumping applications? |  |
| | 07/13/2004 | | Serial communication is lost intermittently between the building automation system (BAS) and a Lonworks board on the GPD506 / P5 drive. What might be causing this? |  |
| | 07/13/2004 | | How is the kW output scaled on the Dual Analog Output option board (Model DS418)? |  |
| | 07/13/2004 | | The "sleep" function can only be used when PID is enabled. If an analog (0-10VDC or 4-20mA) signal for speed reference is used, is there any way to use "sleep" without enabling PID? |  |
| | 03/14/2006 | | How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter? |  |
| | 07/13/2004 | | I want the motor never to run below a certain speed and I am using PID, but there may be times when this low speed will be "too much". Is there a solution for this? |  |
| | 11/29/2005 | | The P5/506 bypass panel "Fault" light is ON, but no fault code is shown on the keypad display. What's wrong? |  |
| | 07/13/2004 | | The P5/GPD506 inverter is displaying an "OH2" fault that will not clear. The heat sink fan(s) is running, and the drive is cool. Why won't it clear? |  |
| | 07/13/2004 | | How can the P5/GPD506 parameter settings be adjusted or changed while the bypass drive is running in bypass mode? |  |
| | 11/28/2005 | | Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters? |  |
| | 10/11/2004 | | Can the GPD 506/P5 be programmed in other languages? |  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 07/13/2004 | | On a GPD 506/P5 Bypass unit, what is the Normal/Test switch used for and when would it be needed in an operation? |  |
| | 07/13/2004 | | What overload protection does the GPD 506/P5V have? |  |
| | 10/11/2004 | | On what applications should the GPD 506/P5 be used? |  |
| | 07/13/2004 | | CALL -- Fault Code Description |  |
| | 07/13/2004 | | OPE10 -- Fault Code Description |  |
| | 07/13/2004 | | OPE03 -- Fault Code Description |  |
| | 07/13/2004 | | OPE02 -- Fault Code Description |  |
| | 07/13/2004 | | OPE01 -- Fault Code Description |  |
| | 07/13/2004 | | BB -- Fault Code Description |  |
| | 07/13/2004 | | EF -- Fault Code Description |  |
| | 07/13/2004 | | OH2 -- Fault Code Description |  |
| | 07/13/2004 | | OH -- Fault Code Description |  |
| | 07/13/2004 | | OV -- Fault Code Description |  |
| | 07/13/2004 | | UV -- Fault Code Description |  |
| | 07/13/2004 | | CPF04 -- Fault Code Desciption |  |
| | 07/13/2004 | | CPF03 -- Fault Code Description |  |
| | 07/13/2004 | | CPF01 -- Fault Code Description |  |
| | 07/13/2004 | | CPF00 -- Fault Code Description |  |
| | 07/13/2004 | | EF2 -- Fault Code Description |  |
| | 07/13/2004 | | EF0 -- Fault Code Description |  |
| | 07/13/2004 | | EF4~8 -- Fault Code Description |  |
| | 07/13/2004 | | EF3 -- Fault Code Description |  |
| | 07/13/2004 | | CE -- Fault Code Description |  |
| | 07/13/2004 | | OPR -- Fault Code Description |  |
| | 07/13/2004 | | OH1 -- Fault Code Description |  |
| | 07/13/2004 | | RH -- Fault Code Description |  |
| | 07/13/2004 | | RR -- Fault Code Description |  |
| | 07/13/2004 | | PF - Fault Code Description |  |
| | 07/13/2004 | | OL4 -- Fault Code Description |  |
| | 07/13/2004 | | OL3 -- Fault Code Description |  |
| | 07/13/2004 | | OL2 -- Fault Code Description |  |
| | 07/13/2004 | | OL1 -- Fault Code Description |  |
| | 07/13/2004 | | PUF -- Fault Code Description |  |
| | 07/13/2004 | | SC - Fault Code Description |  |
| | 07/13/2004 | | GF - Fault Code Description |  |
| | 07/13/2004 | | OC -- Fault Code Description |  |
| | 07/13/2004 | | OV - Fault Code Description |  |
| | 07/13/2004 | | UV3 - Fault Code Description |  |
| | 07/13/2004 | | UV2 - Fault Code Description |  |
| | 07/13/2004 | | UV1 - Fault Code Description |  |
| | 07/13/2004 | | When using the analog output function on a GPD506/P5, how is the output scaled when output current is selected? |  |
| | 07/13/2004 | | Harmonic current distortion data. |  |
| | 11/29/2005 | | Can a contactor be installed between a drive and motor to start and stop the motor? |  |
| | 02/19/2003 | | Specification of 12 pulse input transformer for GPD505/506- PC5/P5 series AC drive. |  |
 | P5 GPD506 Drive |
| |
| | 07/13/2004 | | What is the vertical and horizontal clearance specification (in inches) for mounting any of the GPD506/P5 stand alone drives? |  |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | What is the purpose of a softcharge resistor and contactor in a GPD506 / P5 drive? |  |
| | 11/28/2005 | | Which PID parameters require set-up when configuring the GPD506 / P5 drive for PID pumping applications? |  |
| | 07/13/2004 | | Serial communication is lost intermittently between the building automation system (BAS) and a Lonworks board on the GPD506 / P5 drive. What might be causing this? |  |
| | 07/13/2004 | | How is the kW output scaled on the Dual Analog Output option board (Model DS418)? |  |
| | 07/15/2004 | | C21 unit is connected and runs in Hand and Auto fine. But, the input circuit breaker is tripping while attempting to run in Bypass mode. Why? |  |
| | 07/13/2004 | | The "sleep" function can only be used when PID is enabled. If an analog (0-10VDC or 4-20mA) signal for speed reference is used, is there any way to use "sleep" without enabling PID? |  |
| | 07/13/2004 | | I want the motor never to run below a certain speed and I am using PID, but there may be times when this low speed will be "too much". Is there a solution for this? |  |
| | 11/29/2005 | | The P5/506 bypass panel "Fault" light is ON, but no fault code is shown on the keypad display. What's wrong? |  |
| | 07/13/2004 | | The P5/GPD506 inverter is displaying an "OH2" fault that will not clear. The heat sink fan(s) is running, and the drive is cool. Why won't it clear? |  |
| | 07/13/2004 | | How can the P5/GPD506 parameter settings be adjusted or changed while the bypass drive is running in bypass mode? |  |
| | 11/28/2005 | | Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters? |  |
| | 10/11/2004 | | Can the GPD 506/P5 be programmed in other languages? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 07/13/2004 | | On a GPD 506/P5 Bypass unit, what is the Normal/Test switch used for and when would it be needed in an operation? |  |
| | 07/13/2004 | | What overload protection does the GPD 506/P5V have? |  |
| | 10/11/2004 | | On what applications should the GPD 506/P5 be used? |  |
| | 07/13/2004 | | CALL -- Fault Code Description |  |
| | 07/13/2004 | | OPE10 -- Fault Code Description |  |
| | 07/13/2004 | | OPE03 -- Fault Code Description |  |
| | 07/13/2004 | | OPE02 -- Fault Code Description |  |
| | 07/13/2004 | | OPE01 -- Fault Code Description |  |
| | 07/13/2004 | | BB -- Fault Code Description |  |
| | 07/13/2004 | | EF -- Fault Code Description |  |
| | 07/13/2004 | | OH2 -- Fault Code Description |  |
| | 07/13/2004 | | OH -- Fault Code Description |  |
| | 07/13/2004 | | OV -- Fault Code Description |  |
| | 07/13/2004 | | UV -- Fault Code Description |  |
| | 07/13/2004 | | CPF04 -- Fault Code Desciption |  |
| | 07/13/2004 | | CPF03 -- Fault Code Description |  |
| | 07/13/2004 | | CPF01 -- Fault Code Description |  |
| | 07/13/2004 | | CPF00 -- Fault Code Description |  |
| | 07/13/2004 | | EF2 -- Fault Code Description |  |
| | 07/13/2004 | | EF0 -- Fault Code Description |  |
| | 07/13/2004 | | EF4~8 -- Fault Code Description |  |
| | 07/13/2004 | | EF3 -- Fault Code Description |  |
| | 07/13/2004 | | CE -- Fault Code Description |  |
| | 07/13/2004 | | OPR -- Fault Code Description |  |
| | 07/13/2004 | | OH1 -- Fault Code Description |  |
| | 07/13/2004 | | RH -- Fault Code Description |  |
| | 07/13/2004 | | RR -- Fault Code Description |  |
| | 07/13/2004 | | PF - Fault Code Description |  |
| | 07/13/2004 | | OL4 -- Fault Code Description |  |
| | 07/13/2004 | | OL3 -- Fault Code Description |  |
| | 07/13/2004 | | OL2 -- Fault Code Description |  |
| | 07/13/2004 | | OL1 -- Fault Code Description |  |
| | 07/13/2004 | | PUF -- Fault Code Description |  |
| | 07/13/2004 | | SC - Fault Code Description |  |
| | 07/13/2004 | | GF - Fault Code Description |  |
| | 07/13/2004 | | OC -- Fault Code Description |  |
| | 07/13/2004 | | OV - Fault Code Description |  |
| | 07/13/2004 | | UV3 - Fault Code Description |  |
| | 07/13/2004 | | UV2 - Fault Code Description |  |
| | 07/13/2004 | | UV1 - Fault Code Description |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
| | 07/13/2004 | | When using the analog output function on a GPD506/P5, how is the output scaled when output current is selected? |  |
| | 07/13/2004 | | Harmonic current distortion data. |  |
| | 11/29/2005 | | Can a contactor be installed between a drive and motor to start and stop the motor? |  |
| | 02/19/2003 | | Specification of 12 pulse input transformer for GPD505/506- PC5/P5 series AC drive. |  |
 | P7 Drive |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
| | 07/13/2004 | | Resetting a drive fault. |  |
| | 07/18/2007 | | UV3 -- Fault Code Description |  |
| | 07/18/2007 | | UV2 -- Fault Code Description |  |
| | 07/18/2007 | | UV1 -- Fault Code Description |  |
| | 07/18/2007 | | UL3 -- Fault Code Description |  |
| | 07/18/2007 | | RR -- Fault Code Description |  |
| | 07/03/2003 | | RH -- Fault Code Description |  |
| | 07/18/2007 | | PUF -- Fault Code Description |  |
| | 07/18/2007 | | PF -- Fault Code Description |  |
| | 07/18/2007 | | OV -- Fault Code Description |  |
| | 07/18/2007 | | OPR -- Fault Code Description |  |
| | 07/18/2007 | | OL3 -- Fault Code Description |  |
| | 07/18/2007 | | OL2 -- Fault Code Descriptions |  |
| | 07/18/2007 | | OL1 -- Fault Code Description |  |
| | 07/18/2007 | | OH4 -- Fault Code Description |  |
| | 07/18/2007 | | OH3 -- Fault Code Description |  |
| | 07/18/2007 | | OH1 -- Fault Code Description |  |
| | 07/18/2007 | | OC -- Fault Code Description |  |
| | 07/18/2007 | | GF -- Fault Code Description |  |
| | 07/18/2007 | | FBL -- Fault Code Description |  |
| | 07/18/2007 | | EF7 -- Fault Code Description |  |
| | 07/18/2007 | | EF6 -- Fault Code Description |  |
| | 07/18/2007 | | EF5 -- Fault Code Description |  |
| | 07/18/2007 | | EF4 -- Fault Code Description |  |
| | 07/18/2007 | | EF3 -- Fault Code Description |  |
| | 07/18/2007 | | EF0 -- Fault Code Description |  |
| | 07/18/2007 | | CPF23 -- Fault Code Description |  |
| | 07/18/2007 | | CPF22 -- Fault Code Description |  |
| | 07/18/2007 | | CPF21 -- Fault Code Description |  |
| | 07/18/2007 | | CPF20 -- Fault Code Description |  |
| | 07/18/2007 | | CPF10 -- Fault Code Description |  |
| | 07/18/2007 | | CPF09 -- Fault Code Description |  |
| | 07/18/2007 | | CPF08 -- Fault Code Description |  |
| | 07/18/2007 | | CPF07 -- Fault Code Description |  |
| | 07/18/2007 | | CPF05 -- Fault Code Description |  |
| | 07/18/2007 | | CPF04 -- Fault Code Description |  |
| | 07/18/2007 | | CPF03 -- Fault Code Description |  |
| | 07/18/2007 | | CPF02 -- Fault Code Description |  |
| | 07/18/2007 | | CPF01 -- Fault Code Description |  |
| | 07/18/2007 | | CPF00 -- Fault Code Description |  |
| | 11/16/2009 | | CE -- Fault Code Description |  |
| | 07/18/2007 | | BUS -- Fault Code Description |  |
| | 03/14/2006 | | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |  |
| | 07/18/2007 | | Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |  |
| | 10/27/2005 | | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |  |
| | 10/21/2005 | | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |  |
| | 11/28/2005 | | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |  |
| | 07/13/2004 | | What are some counter-measures to reduce harmonics created by AC drives? |  |
| | 10/31/2005 | | Can multiple motors be used with a single inverter? |  |
 | P7B Drive Bypass |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
 | P7BR Package |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
 | P7C Drive Configured |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
 | P7CR Package |
| |
| | 11/03/2009 | | How do I order touch up paint? |  |
 | PS5 Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
 | R3 Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
 | RC5 Converter |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
 | SS5 Drive |
| |
| | 10/28/2005 | | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |  |
 | V1000-4X Drive |
| |
| | 06/21/2010 | | Does the V1000-4x meet NEMA 4X? |  |
| | 06/21/2010 | | Is the V1000-4X coated with food-grade paint? |  |
| | 06/21/2010 | | Does the V1000-4X meet BISSC? |  |
| | 06/21/2010 | | Does the V1000-4X meet NSF? |  |
| | 06/21/2010 | | Is the V1000-4X corrosion-resistant? |  |
| | 06/21/2010 | | Does the V1000-4X meet IP66? |  |
| | 06/21/2010 | | Does the V1000-4X meet UL? |  |
| | 06/21/2010 | | Is the product ready for shipment? |  |
| | 06/21/2010 | | When should we begin converting existing V74X business to V1000-4X? |  |
| | 06/21/2010 | | What about CASE Software? |  |
| | 06/21/2010 | | Is the Copy function available with the standard LED keypad? |  |
| | 06/21/2010 | | Are V1000 Options compatible with V1000-4X? |  |
| | 06/21/2010 | | Can V1000-4X Options be used with V74X? |  |
| | 06/21/2010 | | Are V74X Options compatible with V1000-4X? |  |
| | 06/21/2010 | | What is the price difference between V74X and V1000-4X? |  |
| | 06/21/2010 | | What documentation ships with the product? |  |
| | 06/21/2010 | | Which ratings have internal or external fans? |  |
| | 06/21/2010 | | Are the external fans rated NEMA 4X? |  |
| | 06/21/2010 | | What are the operator overlay specs? |  |
| | 06/21/2010 | | Do the factory-provided grommets meet the UL Type 4X specification? |  |
| | 06/21/2010 | | Is there a shake proof version of the V1000-4X? |  |
| | 06/21/2010 | | Will there be a stainless steel version? |  |
| | 06/21/2010 | | Is the V1000 the same physical size as V7? |  |
| | 06/21/2010 | | Can the LCD Operator be used for programming and maintenance of the V1000-4X? |  |
| | 06/21/2010 | | Is the V1000-4X rated for outdoor use? |  |
| | 06/21/2010 | | What are the V1000-4X’s ratings? |  |
 | V1000 Drive |
| |
| | 12/21/2010 | | After installation of DriveWizard Plus on a Dell PC, the following Windows error is displayed when attempting to launch the application: "The application failed to initialize properly (0xc000007b). Click on OK to terminate the application" |  |
| | 11/03/2009 | | How do I order touch up paint? |  |
| | 07/27/2007 | | Is the product ready for shipment? |  |
| | 07/27/2007 | | When should we begin converting existing V7 business to V1000? |  |
| | 07/27/2007 | | How many connections can DWEZ Pro handle? |  |
| | 07/27/2007 | | Has Yaskawa scheduled any V1000 Factory Training yet? If yes what are the dates? |  |
| | 07/27/2007 | | Is the Copy function available with the standard LED keypad? |  |
| | 07/27/2007 | | Do we have a USB cable interface (instead of serial) for hookup to laptops for DriveWizardTM Plus? |  |
| | 07/27/2007 | | Will DriveWizardTM Plus be backward compatible? |  |
| | 07/27/2007 | | Will there be a remote keypad option? If yes what ratings? |  |
| | |