Global SitesHomeSite MapContact UsSearch
Advanced Search

eLM Remedy #6

Remedy #6

Some of the eLearning Modules use a file called “stealthray.swf” to launch the eLM in a new window. Adobe flash player blocks this file by default and without this file the eLM will not function properly. If this situation arises, the following “Adobe Flash Player Security” window will be displayed.



To remedy this situation, follow these simple steps:
1.) Click on the “Settings” button on the “Adobe Flash Player Security” window.
2.) A new explorer window will open and display the “Adobe Flash Player Settings Manager” (which is shown here)



3.) Click on “Edit Locations”
4.) Choose “Add location”
5.) Click on “Browse for folder”
6.) Navigate to “C:\YASKAWA_eLearning”
7.) Select “C:\YASKAWA_eLearning” (should be highlighted blue)
8.) Click on “OK”
9.) Close this explorer window and the eLM explorer window.
10.) Relaunch the eLearning Module.