Global SitesHomeSite MapContact UsSearch
Advanced Search

MP2000 Series Application Programming using MotionWorks Version 6

Class Number: TRM010-MP2000-AppProg
Class Location: HQ
Class Cost: $735

Class Topics:
The MP2000 Series Application Programming using MotionWorks Version 6 class is designed to give technicians, engineers and programmers the opportunity to learn to program an MP2300 controller using three programming methods: (1) Motion Command Code, (2) Function Blocks, and (3) Structured Text Motion Programming. The class is heavily weighted toward Function Block programming. Since MP2000 applications tend to be highly specific and unique, the goal is to learn the most common software navigation skills and programming features, and to learn how to use the resources available. Class topics include but are not limited to:

  • MP2000 Memory Structure
  • Application Startup Procedure
  • Simple Motion Command Code application
  • Function Block Startup Procedure
  • Simple Function Block application
  • Function Block Template
  • Function Block application exercises
  • Advanced Function Block Template
  • Function Block Troubleshooting
  • Module Configuration
  • Data Trace
  • Tuning
  • Motion Programming Basics

Class Materials:
Students will receive a copy of the class training manual as well as selected product user and instruction manuals in paper and/or electronic format.

Prerequisites:
This is a highly technical class intended only for the highest-level users. Experience with ladder programming is required. This class will NOT concentrate on ladder programming techniques required for successful implementation of an application, but rather it will concentrate on how different controller features work individually.

Each student must complete ALL MP2300 eLearning modules and pass the eLearning/Sales quiz before coming to class. A good working knowledge of the binary and hexadecimal numbering systems is also required. If you’re not sure if this class is right for you, call Technical Training Services at 1-800-YASKAWA (927-5292) dial 4.

If you do not have a high-speed Internet connection and would like a copy of this e-Learning Module on CD, please send an e-mail to training@yaskawa.com with your request. Please make sure to include your name, company name and address.

When you have completed the eLearning modules, complete the MP2300 certification test.

Class Format:
This class runs from 8:30 to 5:00 pm each day, with a one-hour lunch and two 15-minute breaks. The class consists of approximately 40% lecture and 60% programming exercises.

Continuing Education Units:

Continuing Education Units will be awarded to those students that attend this training class in its entirety and pass the certification test with a score of 85% or better. Yaskawa does not provide partial CEU credits for less than 100% attendance. As an IACET Authorized Provider, Yaskawa America Inc. offers CEUs for its programs that qualify under the ANSI/IACET Standard. Yaskawa America, Inc. is authorized by IACET to offer 2.1 CEUs for this program.


Class Cost:
Contact Yaskawa for pricing at 1-800-YASKAWA (927-5292) dial 4. The fee that you will be charged includes all training documents, a light snack each morning, and a lunch each day. Costs associated with travel, lodging, and evening meals are not included and are the student's responsibility.

To Enroll:
To enroll in any class, call Technical Training Services at 1-800-YASKAWA (927-5292) dial 4 or email training@yaskawa.com. Please have a PO ready when you call. Class sizes are limited, so call early to reserve your seat. PO must be net 30 days.

Cancellation Policy:
Yaskawa reserves the right to cancel a scheduled class at anytime due to low enrollment. In this situation the student will be asked to reschedule or the tuition cost will be refunded. Yaskawa is not liable for any charges incurred by the customer (i.e.-airline, hotel, and rental car) due to cancellation.

Cancellation fee for customers: if canceling within 1 week of the scheduled class is 50% of the total.
Cancellation fee for ASC/Partners: if canceling within 1 week of the scheduled class is 100% of the total.