Browse FAQ's by Product

Don't see your question? Ask us now.

Next PagePrev PageExpandCollapse
Date PostedQuestion
08/31/2012When reading 42h it does not match U1-03? Using Ethernet or Modbus protocols.
11/16/2009Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive?
06/08/2007Can multiple motors be used with a single inverter?
06/08/2007OL4 -- Fault Code Description
03/14/2006When dealing with harmonic noise, which is better-- an AC or a DC reactor?
03/14/2006How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter?
11/28/2005What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure?
11/28/2005Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters?
10/31/2005What is required to start and stop the GPD515/G5 from the digital operator?
10/28/2005What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time?
10/27/2005Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration?
10/26/2005Can the G5 GPD515 drive in flux vector mode can run above 1750 RPM/60 Hz. If so what parameters would need to be changed to accomplish this. We only want to go to 2100 RPM/72 Hz.
10/21/2005What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display?
10/11/2004Can the GPD 506/P5 be programmed in other languages?
07/13/2004What are some concerns when the motor cable is over 100 meters?
07/13/2004Is there a way to perform an initialization without losing the parameter settings?
07/13/2004Can the inverter still be used if the input voltage exceeds the permissible voltage fluctuation range (-15% to +10%)?
07/13/2004Can the GPD 515/G5 do closed loop speed control?
07/13/2004What overload protection does the GPD 515/G5 have?
07/13/2004In what languages can the GPD 515/G5 display?
07/13/2004Can an external 24V power supply be used with the GPD515/G5 Logic Inputs?
07/13/2004What is the current rating for the Run and Fault output contacts on a GPD 515/G5?
07/13/2004Is there a way to "lock out" unauthorized programming of the GPD515/G5?
07/13/2004What are some counter-measures to reduce harmonics created by AC drives?
07/13/2004UV1 - Fault Code Description
07/13/2004GF - Fault Code Description
07/13/2004SC - Fault Code Description
07/13/2004PUF -- Fault Code Description
07/13/2004OL1 -- Fault Code Description
07/13/2004OL2 -- Fault Code Description
07/13/2004OL3 -- Fault Code Description
07/13/2004PF - Fault Code Description
07/13/2004LF -- Fault Code Description
07/13/2004RR -- Fault Code Description
07/13/2004OH1 -- Fault Code Description
07/13/2004OPR -- Fault Code Description
07/13/2004E-10 -- Fault Code Description
07/13/2004E-15 -- Fault Code Description
07/13/2004BUS -- Fault Code Description
07/13/2004CE -- Fault Code Description
07/13/2004EF3 -- Fault Code Description
07/13/2004EF0 -- Fault Code Description
07/13/2004DEV -- Fault Code Description
07/13/2004ERR -- Fault Code Description
07/13/2004CPF00 -- Fault Code Description
07/13/2004CPF01 -- Fault Code Description
07/13/2004CPF02 -- Fault Code Description
07/13/2004CPF03 -- Fault Code Description
07/13/2004CPF04 -- Fault Code Desciption
07/13/2004CPF05 -- Fault Code Description
07/13/2004CPF06 -- Fault Code Description
07/13/2004CPF22 -- Fault Code Description
07/13/2004CPF23 -- Fault Code Description
01/10/2003Can a negative speed reference be used to command the drive to reverse direction when using the Profibus option?