Browse FAQ's by Product

Don't see your question? Ask us now.

Next PagePrev PageExpandCollapse
Date PostedQuestion
06/08/2007Can multiple motors be used with a single inverter?
06/22/2006OH -- Fault Code Description
03/14/2006When dealing with harmonic noise, which is better-- an AC or a DC reactor?
03/14/2006How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter?
11/28/2005Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters?
10/28/2005What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time?
10/27/2005Can the PID in the V7 Drive be used for positioning?
10/27/2005Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration?
10/27/2005What does "with volume" and "without volume" refer to? Some V7 manuals and catalogs use this terminology.
10/27/2005Can the V7 provide an analog output signal programmed for motor output current?
10/27/2005Is a braking resistor internally installed?
10/27/2005Can a motor with less capacity than the capacity of the V7 Drive be used?
10/21/2005What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display?
10/11/2004Can a Dynamic Braking resistor be installed on a J7 Drive?
07/13/2004In some pumping systems the motor speed is normally about 80% of rated motor speed. However, periodic purging of the pumping system requires the pump to go to full speed for a while, then return to normal. How is this done with the V7 Drive?
07/13/2004Can the speed reference to a V7 Drive be switched 'on the fly' between run and jog?
07/13/2004On the V7 Drive are the Logic inputs and the Logic Common terminal (SC) electrically isolated from the Frequency Reference Common (FC)?
07/13/2004Does the Modbus port on the V7 Drive need a termination resistor?
07/13/2004The V7 Drive Jog Reference (S7) command is given. Why doesn't the motor move?
07/13/2004What is the meaning of CAL or CALL on the keypad display?.
07/13/2004What parameter sets the maximum output frequency?
07/13/2004What happens when switching to reverse while the motor is rotating forward (FWD=OFF, REV=ON)?
07/13/2004Why are the parameters on the digital operator hidden or locked?
07/13/2004What does it mean that, "motor protection time constant for the electrical termal device is 8 minutes"?
07/13/2004Why don’t the page numbers in the parameter section of the instruction manual match the page numbers in the body of the manual?
07/13/2004What are some counter-measures to reduce harmonics created by AC drives?
07/13/2004OL3 -- Fault Code Description
07/13/2004SER - Fault Code Description
07/13/2004bb -- Fault Code Description
07/13/2004EF -- Fault Code Description
07/13/2004STP -- Fault Code Description
07/13/2004UL3 -- Fault Code Description
07/13/2004FAN -- Fault Code Description
07/13/2004UL3 (blinking) -- Fault Code Description
07/13/2004OC -- Fault Code Description
07/13/2004UV1 -- Fault Code Description
07/13/2004UV2 -- Fault Code Description
07/13/2004OL1 -- Fault Code Description
07/13/2004OL2 -- Fault Code Description
07/13/2004OL3 -- Fault Code Description
07/13/2004EF -- Fault Code Description
07/13/2004F00 -- Fault Code Description
07/13/2004F01 -- Fault Code Description
07/13/2004F04 -- Fault Code Description
07/13/2004F05 -- Fault Code Description
07/13/2004F06 -- Fault Code Description
07/13/2004F07 -- Fault Code Description
07/13/2004oPA - Fault Code Description
07/13/2004CE -- Fault Code Description
07/13/2004STP -- Fault Code Description
07/13/2004(0ff) -- Fault Code Description
07/13/2004What is required to replace the digital operator on the V7 NEMA 4 drive? What is the replacement part number?
01/10/2003Can a negative speed reference be used to command the drive to reverse direction when using the Profibus option?