| Date Posted | Question |
09/13/2012 | How do I order touch up paint? |
06/08/2007 | Can multiple motors be used with a single inverter? |
06/22/2006 | OH -- Fault Code Description |
03/14/2006 | When dealing with harmonic noise, which is better-- an AC or a DC reactor? |
03/14/2006 | How can I set this AC drive so my motor can’t run below 20hz? Is it the Frequency min. parameter? |
11/28/2005 | What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |
11/28/2005 | Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters? |
10/28/2005 | What are the maintenance recommendations for drives that sit on shelves for a couple years without power? Should the drives be powered up from time to time? |
10/27/2005 | Can the PID in the V7 Drive be used for positioning? |
10/27/2005 | Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |
10/27/2005 | Is a braking resistor internally installed? |
10/27/2005 | Can a motor with less capacity than the capacity of the V7 Drive be used? |
10/27/2005 | Can the operator on the V7 Drive be removed and remotely mounted? |
10/21/2005 | What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |
10/11/2004 | Can a Dynamic Braking resistor be installed on a J7 Drive? |
07/13/2004 | In some pumping systems the motor speed is normally about 80% of rated motor speed. However, periodic purging of the pumping system requires the pump to go to full speed for a while, then return to normal. How is this done with the V7 Drive? |
07/13/2004 | Can the speed reference to a V7 Drive be switched 'on the fly' between run and jog? |
07/13/2004 | What is the meaning of CAL or CALL on the keypad display?. |
07/13/2004 | What parameter sets the maximum output frequency? |
07/13/2004 | What does it mean that, "motor protection time constant for the electrical termal device is 8 minutes"? |
07/13/2004 | What are some counter-measures to reduce harmonics created by AC drives? |
07/13/2004 | OL3 -- Fault Code Description |
07/13/2004 | SER - Fault Code Description |
07/13/2004 | bb -- Fault Code Description |
07/13/2004 | EF -- Fault Code Description |
07/13/2004 | STP -- Fault Code Description |
07/13/2004 | UL3 -- Fault Code Description |
07/13/2004 | FAN -- Fault Code Description |
07/13/2004 | UL3 (blinking) -- Fault Code Description |
07/13/2004 | OC -- Fault Code Description |
07/13/2004 | UV1 -- Fault Code Description |
07/13/2004 | UV2 -- Fault Code Description |
07/13/2004 | OL1 -- Fault Code Description |
07/13/2004 | OL2 -- Fault Code Description |
07/13/2004 | OL3 -- Fault Code Description |
07/13/2004 | EF -- Fault Code Description |
07/13/2004 | F00 -- Fault Code Description |
07/13/2004 | F01 -- Fault Code Description |
07/13/2004 | F04 -- Fault Code Description |
07/13/2004 | F05 -- Fault Code Description |
07/13/2004 | F06 -- Fault Code Description |
07/13/2004 | F07 -- Fault Code Description |
07/13/2004 | oPA - Fault Code Description |
07/13/2004 | CE -- Fault Code Description |
07/13/2004 | STP -- Fault Code Description |
07/13/2004 | (0ff) -- Fault Code Description |