Industry News Display

2014-01-02   Consulting Specifying Engineer

Echelon’s Varun Nagaraj answers one-on-one questions, explaining how the Internet of Things can and should be used by engineers.


By: Amara Rozgus, Consulting-Specifying Engineer

Consulting-Specifying Engineer (CSE) asked Varun Nagaraj, senior vice president and general manager, Internet of Things at Echelon Corp., for some insights on how the Internet of Things (IoT) will be viewed by consulting engineers

Nagaraj has more than 20 years of high-tech product planning and strategy experience. He holds a BSEE from IIT Bombay, a master’s in computer engineering from North Carolina State University, and an MBA from Boston University.  

Read his July 2013 article “IP-all-the-way is the way to go.”

CSE: How will the Internet of Things directly affect consulting engineers?

Nagaraj: The IoT takes advantage of Internet protocol (IP) as a kind of unifying force, creating bridges among previously parallel or incompatible protocols. As a result, the IoT will both simplify and expand the role of consulting engineers, allowing them to concentrate on higher-level considerations of an application, rather than being restricted to a single set of protocols for any given project.

CSE: How will the IoT directly affect the products and systems that consulting engineers specify?

Nagaraj: When IP is driven to the device level, consulting engineers will be able to focus on specifying products based on their functionality rather than worrying about protocols and communication transport compatibility issues. And because developers can create single products/systems that work with multiple protocols, consulting engineers will have available a wider range of product/system options available to specify for each project they work on.

CSE: Which of the following —lighting, fire/life safety, HVAC, or electrical/power products —do you see moving most quickly into the IoT?

Nagaraj: I would expect lighting to move most quickly into the IoT space, followed by HVAC and fire/life safety.

CSE: Why?

Nagaraj: Economics and emerging regulations will drive widespread adoption of LED lights with controls in commercial buildings and in public spaces. It will be important for the consulting engineer to specify systems that can grow, are not vendor-dependent, and can serve as a platform for other control applications. The use of IP at every level in a lighting system will facilitate these objectives.

CSE: What’s the projected growth for products in this fastest-growth area?

Nagaraj: Forecasts can vary widely. For example, IHS, a well-known research firm is forecasting that nearly 50% of the 1B “industrial or commercial” IoT devices installed in 2017 could be lights.

CSE: With regard to building automation systems (BAS) and building management systems (BMS), what future trends do you see?

Nagaraj: I see three trends:

1. A multi-protocol future based on the IP protocol as the unifying layer—not just at the management layer where it is used today, but also at the device of fieldbus level. This will hopefully result in the ending of the counterproductive LonWorks versus BACnet discussion that is so ingrained in our specification world view today. The right answer should be either LonWorks or BACnet—but over IP!

2. The use of big data collection and analysis techniques to identify opportunities for system optimization.

3. A continued use of wired communications even as there is an increasing use of wireless options.  

View the original article and related content on Consulting Specifying Engineer