Industry News Display

2010-10-28   Consulting Specifying Engineer

When it comes to equipment operation, user interface is the most visible system component. The user interface can include anything from the steering wheel and instrument cluster on a vehicle’s dashboard to the operating system on your computer. Regardless of the scale of the application, the purpose is ...


By: Jim Martz, Governor Control Systems Inc. Fort Lauderdale, Fla.

When it comes to equipment operation, user interface is the most visible system component. The user interface can include anything from the steering wheel and instrument cluster on a vehicle’s dashboard to the operating system on your computer. Regardless of the scale of the application, the purpose is the same: it must allow human interface into a system, it must provide the user with a means to control the equipment, it must provide feedback from the equipment to show operational conditions, and it must tell us when something is wrong. The interface should do these things efficiently, be easy to use, and be visually and ergonomically pleasing. In the case of industrial or commercial control systems, these concepts are the same, but the interface can be controlling a potentially complex system or series of systems behind it. 

Human-machine interface

Although there are many different terms for an interface to an industrial control system, the term “human-machine interface” (HMI) is the most widely used. While the term itself can be interpreted differently depending on context, most often it is defined as a system that provides a window into the operation of a single machine or simple network of multiple machines in a common control system.

Today’s HMI systems offer advanced hardware platforms along with powerful software development suites to allow an engineer to create an interface completely customized to meet any system requirements. Modern HMI hardware can combine a touch screen interface with a fan-less cooling system, and integrated Windows-based operating system. Since the hardware is designed for installation in switchgear panels or other industrial environments often high in temperature and vibration, flash memory is used to eliminate the moving parts in a traditional hard drive, which improves robustness. The software suite provides an environment to create a customized series of screens for your application to allow simple control of the machine or system, display current and historical information, and handle alarms. In addition, more complex operations can be integrated, such as data acquisition and graphical trending. Windows-based operating systems easily interface to external programs such as Excel, which allows data to be manipulated for additional formatting and charting.

Access the Internet remotely 

One of the most useful features of an HMI system is remote access via the Internet.  This functionality allows an operator or plant manager to access the system from most computers with an Internet connection. Remote accessibility provides a convenient way to troubleshoot or control the system without maintaining full-time operator personnel, which reduces cost, billable hours, and response time to a problem. Furthermore, with modern HMI systems it may not even be necessary for any operator, regardless of location, to monitor the system actively. In the event of a warning or alarm condition, most systems can be set up to send an automatic e-mail or even a phone message via text to operations personnel.

SCADA system implementation

While an HMI can provide a window into a specific machine or local system, many operations require greater capability for their facilities. HMI systems are usually building blocks in Supervisory Control and Data Acquisition (SCADA) systems, a higher-level system that incorporates multiple processes into one integrated package controlling and monitoring remote systems from a central location. SCADA systems help users monitor and control electrical systems from the same interface, as well as mechanical processes, fire systems, water and wastewater treatment, communications and alarm systems, and HVAC systems.

Change over time

Certainly much has changed in the HMI/SCADA industry since the first systems began entering the market in the 1970s. We have come a long way from the days of individual Remote Terminal Units (RTUs), computer systems with bulky communication infrastructure, and inefficient software interfaces. With developments in electronics design and communication protocols, today’s systems are smaller, faster, more efficient, more configurable, and more scalable than ever. Smaller SCADA systems may consist of a single HMI, while larger systems can incorporate multiple HMIs, distributed I/O, and redundant communications networks with multiple controls or PLCs.

Regardless of the size, plant-level, facility-level, or multiple-facility monitoring and control are the functions of the SCADA system with individual processes under the control of a local system. For example, in a power generation facility, an engine or turbine control will perform most functions, such as maintaining the speed of the prime mover or maintaining a process like air-fuel ratio or steam header pressure control. A generator control will maintain a base load power output or share the plant electrical load among multiple generators.

The SCADA system provides the operator with the interface through which he or she can enter a desired setpoint like a base load or process reference. These setpoints are then transferred to the local machine controls that perform the desired function. The supervisory system will also provide detailed information such as valve and circuit breaker positions, power flows, alarm conditions, and many other parameters, most of which can be used in graphical trending and historical data logging. The operator will use this information to determine if any changes need to be made based on the operating conditions for the overall plant, and the system also provides the user interface through which those changes are made.

Speed of data transfer

The speed and efficiency at which this data is transferred has greatly improved with developments and standardization of communication protocols. Most hardware manufacturers now use open and nonproprietary protocols such as Modbus or OPC to enable system designers to easily integrate multiple controls or hardware platforms. Ethernet has become a widely used network for the interface between controls and HMI/SCADA systems, as many protocols that were originally developed for serial communications have been adapted for TCP/IP.

Today’s HMI and SCADA systems are now more affordable as well. Smaller companies and organizations can take advantage of the convenience these systems provide. If a project calls for the construction of a new facility with new communications infrastructure, that is the ideal time to consider implementing a SCADA system. However, with the hardware and software available on the market today, systems have become more expandable than in the past. Organizations that do not have SCADA systems in their facilities or that have very simple small HMIs and are looking to either upgrade or expand their systems have many implementation options. Some organizations choose to install single or multiple HMIs monitoring a dedicated machine or a single system in the facility. Others choose to first implement a simple master station in a remote control room and then add to the system over time.

Control system integrators, such as Governor Control Systems Inc., who offer HMI and SCADA systems as part of their product and service offering, have experience in many applications across multiple industries. These companies develop a library of standard screens that can be applied to new projects. While every project and site is different and will require some customization, much of the development time is eliminated through the reuse of screens and concepts from past development. Taking advantage of this type of experience can not only result in a better system but also eliminate some of the costs associated with installing and commissioning a SCADA system.

Regardless of your industry, the benefits of SCADA systems are many. As with any investment, there must be a return. The savings that come from operating more efficiently will quickly offset the initial cost of installing a SCADA system. With the advancements in modern HMI and SCADA technology, the possibilities are endless, dependent only on your budget and imagination.

Martz is an applications engineer for Governor Control Systems Inc. in Fort Lauderdale, Fla. Martz has engine control systems design experience with Caterpillar, Inc. and engine and power management systems experience with Woodward Governor Company.

View the original article and related content on Consulting Specifying Engineer