Industry News Display

2021-09-13   Control Engineering   Plant Engineering

There are several types of linear servo motors and knowing the strengths and weaknesses of each, along with the application they’re best-suited for, is critical.


By: Matt Pelletier

 

Learning Objectives

  • Linear servo motors come in many types, and each have their own strengths.
  • Cost, environment, length and load mass are among many considerations users should take into account for linear actuators.
  • Long-term cost and performance is another critical factor for linear actuators.

It is beneficial to know when and how to apply linear servo motor technology. This requires knowing the components that comprise a linear motor stage and the components used to make other linear actuators, such as ballscrews, belts, and rack and pinion, which rely on rotary servo motors.

The advantages and limitations of each mechanism are crucial when deciding how to apply the technology. Use this information to identify the most effective mechanism for a given application.

Four linear actuator types

A wide array of linear actuators exists in the motion control industry. However, these four are quite common: linear motors, ballscrews, belts, and rack and pinion.

1. Linear motor stage

Let’s begin with a definition of a linear motor stage. The distinguishing feature of a linear motor is the load moves without any mechanical power conversion. The linear force generated by the motor coil is directly connected to the load. In a linear motor, the motor coil propels itself along the magnet track. The motor coil is attached to the carriage, sometimes called a “slide.”  The load is bolted directly to the carriage. The carriage is held in place by linear bearings with rails secured to the base. The linear bearings are the only point of mechanical contact and frictional wear, apart from and the bending of cables. This simple fact results in huge performance benefits for a linear motor stage. The position of the carriage is reported to the control system through a linear encoder. The encoder has two parts – the scale mounted to the base, and the moving read head. Other parts of a typical linear motor stage are the cable management system and end stops.

2. Ballscrew actuator

The ballscrew is the standard go-to actuator for a wide variety of applications.  These also have a carriage that moves on linear bearings and rails. But the force to move it is transmitted through a nut from a rotating screw. This nut is often comprised of a system of enclosed recirculating ball bearings which minimize friction. The screw is driven by a rotary motor. The encoder in the motor provides position feedback to the control system. The screw is held in place with bearings at each end and connects to the motor through a flexible coupling.

3. Belt actuator

A belt actuator also has a carriage which moves on rails with linear bearings. This carriage is driven by direct connection to a timing belt riding on two pulleys.  The pulleys are held in place with bearings and connect to the motor with a flexible coupling. The encoder on the motor provides position feedback to the control system.

4. Rack and pinion

A rack and pinion system is often comprised of a motor that drives a pinion, moving itself along a fixed rack, like a train on a track. The motor is mounted to the carriage, driving the pinion through a gear reduction to move the entire assembly.

Comparative metrics for linear actuation

Now let’s look at how each of these technologies compare in metrics such as initial cost, speed and acceleration, and other factors as listed in figure 5. It is important to define each of these metrics before discussing the strengths and weaknesses of each technology. This is not an evaluation, but it does represent general industry trends.

Linear actuator initial cost

Let’s start with the bottom line – initial cost. The linear motor often has the highest overall performance. Stands to reason, therefore, the initial cost is also generally higher than other technologies. Ballscrews are less expensive than linear motors. However, they are more expensive than belt actuators, which tend toward the low end of the cost spectrum. Rack and pinion is tough to compare. These tend to be used in large systems with much larger and heavier payloads. The cost of rack and pinion is lower at that scale than linear motors, ballscrews, and belts. At a smaller scale, the advantage is often less distinguishable.

Speed and acceleration for linear actuators

Motion control systems have the need for speed. Faster better and more means a quick return on the investment. This translates to not just top speed, but fast acceleration.

The linear motor can accelerate quickly to reach high speeds, typically around 5 m/s. It is the performance champion for the mechanism with both high speed and acceleration.

Screw driven actuators can have strong acceleration, but above the critical speed a screw will oscillate. This critical rpm design limitation is dependent on the diameter and length of the screw. The screw lead can be designed to move further for every turn. This increases the linear speed for the same motor rpm. But it also means more motor torque is required to move the same load. It also may negatively affect the repeatability and accuracy (more on that later). With a faster screw the reflected inertia also increases, thereby reducing control loop stability and increasing settling time. As a result, a larger, more expensive motor may be required. Occasionally these constraints have a snowball effect resulting in a very oversized or even impossible solution.

Belts can also be fast, about the same as linear motors. But as we’ll see later, they have nowhere near the same precision. Rack and pinion systems can reach very high speeds, higher even than linear motors. They often don’t accelerate quickly since they are designed to move large and heavy loads longer distances.

Length for linear actuators

The large systems driven by rack and pinion can also be quite long and it is cost effective to increase the length with additional rack segments with little impact on performance.

Linear motors can also be used in applications with long stroke, but the cost of magnet track and absolute encoder tape is significant. Performance, however, is unaffected by overall length.

Ballscrew length is limited once again by the critical speed of the screw. Longer screws begin to oscillate at a lower RPM, and negatively impact tuning by lowering resonant frequencies. We’ll discuss this more later. A larger screw diameter helps to achieve useable speeds. This means large motors are required to drive the longer screws, even with a small load, unless the speed is very slow.

Belt drive designs are lengthened with minimal increase in cost. However, the effect of belt stretch becomes proportionally worse, resulting in reduced accuracy and repeatability. And like the ballscrew, along with increased length comes decreased stiffness and lower resonant frequencies.

Vertical load for linear actuators

Horizontally oriented motion is the most common, but vertical or inclined axes are required in many applications. This means the force of gravity is constantly pushing the load down. This force must be overcome by the motor while the axis moves or holds position. When the machine powers off, a braking system can prevent the vertical axis from falling.

Rotary holding brakes are commonly found in servomotor designs to lock the motor shaft when powered down. This makes the ballscrew or belt an excellent choice for vertical loads. A vertical rack and pinion also works well for the same reasons.

Linear motors are a bit more complex with vertical loads. A counterbalance or linear holding brake should always be used. A linear holding brake may be mounted externally or fit under the carriage to brake against the rail.

Rigidity for linear actuators

Machine rigidity, or stiffness, and its inverse, compliance, are important to understand. Every mechanically connected element has a level of rigidity – a spring constant. This rigidity, along with the mass of each element, defines the natural frequencies of oscillation for the system. If these frequencies are too low, the release of energy can cause a significant disturbance to the motor. This interferes with the control system algorithms that position the load.

Belt drive systems often have the lowest rigidity and therefore the lowest natural frequencies. The belt is like a spring and there are natural frequencies between the carriage and the pulleys. Another loss of rigidity occurs between the drive pulley and the motor coupling. As the motor begins to turn, first the coupling deflects according to its spring constant. Then the belt deflects, before the load moves. The rigidity is further complicated since it depends on the position of the carriage and resulting length of belt in the direction of the force exerted through the pulley.

Ballscrews have much higher rigidity, but the same principles apply. The motor turns the coupling, which deflects, which turns the screw which also deflects to some extent. Long, thin screws will have lower rigidity than short wide ones.

Rack and pinion is a little different. These maintain a constant and high rigidity at the point of mechanical connection regardless of the load position. Oscillations are likely to originate within the load itself if it is large and complex.

The most rigid of all these actuator technologies is the linear motor. There is no coupling or mechanical linkage to deflect. The load is connected to the motor through the carriage. If there are any frequencies of oscillation, they will come from the load itself and not from the mechanical system.

Load mass for linear actuators

Rigidity and resonant frequency are related to load mass. This is summarized in a key performance metric called the load to motor inertia ratio. Servo systems are commonly sized for a load to motor inertia ratio less than 10:1 for acceptable control of the load by the motor through the flexible coupling. Load mass is one of the most elements in mechanical system selection, so it is important to understand these well.

Load to motor inertia ratio is more accurately called mass ratio and is of less importance in a linear stage because the motor is directly coupled to the load. The load on a linear motor is more like an extension of the carriage itself. A linear motor has no coupling to reduce the rigidity of the system. Load mass is nevertheless important for linear motors, as it limits the acceleration and deceleration rate according to Newton’s Law. It also affects linear bearing life. Low friction also means almost all of the power to stop a moving load must be supplied by the electronic drive system, which can also limit the maximum load.

While it’s not the fastest to accelerate, the clear winner on moving heavy loads is the rack and pinion. These are often used on large gantry systems.

Ballscrews can also be sized to move very heavy loads, commonly applied in applications with moderate length and speed requirements. However, the inertia ratio and low resonant frequencies associated with heavy loads tend to limit the application.

Belt mechanisms tend to have lower practical weight limits, as do linear motors. Acceleration and therefore top speed can be limited with heavy loads.

Backlash for linear actuators

The performance of linear actuators can suffer from an effect called backlash. This is lost motion when the mechanism reverses. The ballscrew has a level of backlash between the nut and the screw. This can be reduced with preload, which in turn causes the nut to wear out faster. For the belt system, backlash occurs between the teeth of the belt and pulley. The same can occur between the teeth of the rack and pinion and within the teeth of any gearbox.

Manufacturers have developed ways to reduce the backlash in actuator technologies and electronically compensate for it in the control system. There always is some level of backlash and it tends to get worse as the mechanism wears. It also means the position of the load cannot be exactly determined by the position of the motor encoder. This can also lead to tuning instability and noisy operation as the load disconnects from the motor for a short time upon reversal.

The linear motor is the only mechanism that can claim zero backlash. Position feedback is measured with a linear scale. With the read head, carriage, and load bolted together as one piece.

Settling time for linear actuators

Rigidity, load mass, inertia ratio, and backlash are all interrelated factors that worsen the position settling time of a mechanism. Position settling time is the time delay between the end of the commanded move and when the mechanism stops. Reducing this delay is especially important for applications with many short moves. Waiting for the machine to stop can represent a significant fraction of the cycle time.

The settling time in a linear motor can often be reduced to zero with good tuning, due to its high rigidity and zero backlash. It may be necessary to mitigate vibrations originating in the load itself. Achievable settling times for the ballscrew and belt usually follow the level of mechanical rigidity and backlash with screws often outperforming belts. Same goes for rack and pinion, although fast moves and low settling time are typically not the focus with these larger machines.

The position of these mechanisms is measured through the rotary servomotor’s encoder. The encoder may indicate the load has settled with a low settling time. What that means is the encoder has stopped moving. The load may still be in motion and not yet settled or experiencing vibration and oscillation. Rigidity and backlash interferes with the measurement of settling time through the encoder of a rotary servomotor. However, in the linear motor, the encoder is fixed to the load itself, reporting the true settling time of the load.

Accuracy and repeatability for linear actuators

Backlash and rigidity also contribute to a mechanism’s positioning accuracy and repeatability. Accuracy is a measure of the deviation from the ideal; in this case, position. If the machine is commanded to move 4 mm, does it move exactly 4.000 mm?  Or if you were to measure it externally, did it only move 3.999? What’s often more important is repeatability, also called precision. Because if the machine can move 3.999 repeatedly when you command 4.0, then adjust the command until it does move to the required position.

As with settling time, accuracy and repeatability are a function of machine rigidity and backlash. The control system measures position at the encoder. Rigidity and backlash add an element of uncertainty to those measurements.

The manufacturing process of a belt, ballscrew, or rack and pinion will affect the accuracy and repeatability. Only the linear motor by natural design measures the load directly and moves it without the backlash and compliance problems that can plague mechanical actuators.

Full closed-loop linear actuation

So why not compensate for the shortcomings of ballscrews, belts, and rack and pinion mechanisms by adding a linear encoder? This is possible, and one term for this in the industry is full closed-loop operation. This allows the position loop of the rotary motor to be closed by linear encoder feedback.

However, adding a linear encoder adds significant costs and complexity. The linear scale must be accurately placed. The read head clearance to the linear scale must be accurately aligned. A cable track for cable management is needed on the carriage. Most servo amplifiers don’t support a second encoder input without additional hardware cost. Servo tuning also will be affected and must be completed again.

If the performance of an existing system must be improved, then full closed-loop control is a viable option. It is generally not a significant cost savings compared to using a linear motor in the first place. Adding full closed-loop control will improve repeatability and accuracy, but does not do much to improve rigidity, settling time and wear. For new applications, it is important to consider a linear encoder on a belt, ballscrew or rack and pinion will really save money in the long run.

Wear and maintenance for linear actuators

All mechanisms wear down. It’s inevitable. Users should understand what part of the mechanism wears and what happens to the system’s performance. In the linear servo, only the linear bearings wear out. But until they utterly fail, that stage will position accurately, at least in the linear direction. Pitch, yaw and carriage roll cannot be detected by the linear encoder and will deteriorate over time.

Some linear bearings require regular lubrication, but self-lubricating linear bearings are commonly available. The same principle applies to linear bearings on a ballscrew, belt or rack and pinion. However, these mechanisms have other moving parts that wear out. The screw itself, the nut, the bearings on the screw, motor bearings, belts, rack, pinion and gearboxes all eventually wear out even with regular lubrication.

From day 1, the performance of these mechanical systems begins to decline. The backlash and stiffness get a little worse every day. Therefore expect position settling time, accuracy, and repeatability to continually degrade as time goes on. The linear motor bearings do eventually wear out, but quite gracefully by comparison.

Environment for linear actuators

Different mechanisms are best suited for different industrial environments. Consider the magnetic field of the magnet track of a linear motor which may attract magnetic particles. A bellows protection system will help keep particles off the magnet track. While linear motors don’t require a cleanroom, they do their best in clean environments free of excessive dust and oil. The linear scale can still work with some interference. However, users should consider a linear motor with an inductive or magnetic linear encoder for very dirty environments.

The ballscrew is used commonly in machine tool and other dirty environments, although the screw also must be protected. Belts and rack and pinion also work well in many environments.

Clean rooms are on the other side of the spectrum, where it is critical to reduce the number of microscopic particles emitted by the actuator.

Linear motors can be easier to make clean room compatible as the wear of linear bearings is the only source of contamination. The wear points of ballscrews, belts, rack and pinion or other mechanisms with mechanical power transmission are generally less desirable for clean room operation due to the number of particles ejected during operation.

Selecting the right actuator

When selecting the right actuator for an application, it is important to consider long-term cost and performance. There are applications with specific constraints which logically eliminate a linear motor from consideration. Other applications have long been the strength of linear motors – long stroke or high speed, fast acceleration, precision and accuracy.

There’s a middle ground where linear motors are often overlooked in favor of the traditional solutions of ballscrews, belts, or rack and pinion. Solving these applications with linear motors can save money in the long run while providing exceptional and stable performance over the life of the machine.

Matt Pelletier, product training engineer, Yaskawa America Inc. Edited by Chris Vavra, web content manager, Control Engineering, CFE Media and Technology, cvavra@cfemedia.com.

MORE ANSWERS

Keywords: linear servo motors, motors and drives, linear actuators

CONSIDER THIS

What is your biggest consideration when choosing a linear servo motor or other actuator for an application?

ONLINE extra

Yaskawa provides a video version detailing selection of linear actuators.

View the original article and related content on Control Engineering
Node: lr2
  Share
|