Industry News
06/19/2012 Part of a European motor efficiency standard allows use of a variable speed drive to meet energy-sa... |
05/31/2012 Variable frequency drives offer simple method of boosting energy efficiency of heavy equipment |
This year, the IMS Research mobile radio division exhibited and presented at the TETRA World Congre... |
After watching the initial adoption of the ErP directive in the motors market, the question arises ... |
Companies are crowd-sourcing their RF databases to aid GPS and improve indoor location accuracy as ... |
Building automation equipment in institutional buildings like schools and hospitals is expected to ... |
03/09/2012 IMS Research estimated 31 million new fieldbus and Ethernet nodes were installed in 2011 and is pre... |
High growth in Brazil is predominately driven by oil and gas and mining expansion, as well as proje... |
02/23/2012 IMS Research predicts sales into the oil and natural gas, mining, and sugar industries will drive g... |
IMS looks back on their initial projections for machinery projections in 2011 and projections going... |
A report by IMS Research indicates that the high price of oil in 2010 and 2011 will increase invest... |
Medium voltage drives sales into the oil and gas industry will outplace the market in 2011, accordi... |
08/31/2011 Consumer-grade smartphones and tablet computers are fast becoming commonplace extensions of industr... |
08/15/2011 A net zero building has a neutral carbon footprint, uses only renewable energy, and is net zero in ... |
Walnut meat kernels have to be dried to optimum moisture content quickly and efficiently. How do yo... |
Increased activity from businesses as well as strong growth in regions like China suggest a rebound... |
If you’re frustrated with the performance of your industrial Ethernet platform, does gigabit Ethern... |
Building a controller has never been easier—or more confusing. This tutorial guide can help determi... |
Maximize reliability, speed, and ease of operation and maintenance by by selecting an appropriate m... |
05/17/2011 There are a variety of cooling systems that will meet the cooling requirements of a facility. |
Node: lr2
|