Industry News


 
Virtualization technology beliefs are debunked, proving to be very beneficial for critical, industr...
The venerable proportional-integral-derivative (PID) algorithm can solve a variety of feedback cont...
IHS Markit predicts that global machinery production revenues will grow 2.2% in Q2 2017 as a result...
The Control Engineering RCEP webcast, “Choosing sensors for the application,” resulted in more ques...
Companies can reduce their electric bill by avoiding energy expenditure spikes, monitoring their en...
Respondents to the 2017 IIoT for Engineers study identified eight key findings regarding familiarit...
Open-loop controls and closed-loop controls each have unique situations where they are needed and t...
Fluid power applications are complex. It can be a challenge to choose between an open- or closed-lo...
Manufacturers looking to find answers quickly to complex problems within factories, buildings, and ...
Thermal imaging has opened the door to entirely new applications that previously may not have seeme...
Key trends in variable-speed, servo and/or stepper, and medium-voltage drives from buying and speci...
Tutorial: Which factors should be considered to determine whether an open-loop or a closed-loop con...
Closing the control loop provides insight into the behavior of the process.
Cover Story: Get help for programmable logic controller (PLC) programming from Control Engineering ...
Data centers have become increasingly important under the Industrial Internet of Things revolution....
Using a standardized methodology to define project quality ensures deliverables fit customer specif...
Inside Machines: Industrial matrix drives were used for a transporter system retrofit to reduce ene...
Adaptive motion controllers can be modified to a controlled process behavior, among other controlle...
Historically, the use of variable frequency drives (VFDs) has been limited to large motors and proj...
The packaging and processing industry is becoming more automated with more companies being bought o...