Industry News
05/05/2017 Using a standardized methodology to define project quality ensures deliverables fit customer specif... |
Inside Machines: Industrial matrix drives were used for a transporter system retrofit to reduce ene... |
04/04/2017 Adaptive motion controllers can be modified to a controlled process behavior, among other controlle... |
Historically, the use of variable frequency drives (VFDs) has been limited to large motors and proj... |
The packaging and processing industry is becoming more automated with more companies being bought o... |
03/07/2017 Knowing how magnetism and electromagnetic induction work are crucial to understanding how an ac ind... |
03/07/2017 Manufacturing automation provides companies many benefits such as improved safety, lower costs, and... |
For the first time in the history of industrial controls, industrial control system (ICS) programmi... |
The terms accuracy, repeatability, and resolution can be found on the spec sheets of many engineere... |
02/21/2017 Healthy ball bearings are one of the most important details for preventing potential disaster in a ... |
Customization and variability are at an all-time high and food producers must keep up with the tren... |
It is essential to perform preventive maintenance (PM) checks on electric motors as a part of manag... |
Low power is not only inefficient, but can also be expensive over the life of an electrical system.... |
01/31/2017 A permanent magnet (PM) motor is an ac motor that uses magnets imbedded into or attached to the sur... |
Providing cost, space, and energy efficiency for VFD applications. |
If the goal is to save money on energy at an industrial facility, taking proper care of the equipme... |
01/13/2017 Motor current analysis provides information on existing issues such as loose connections, burned wi... |
Motor faults and failure can cause disruptions to business operations and lead to loss of productiv... |
01/05/2017 Keep an ear out for leaks, but look at other factors as well. |
It is important to verify and improve short-circuit rating to remain in compliance. |
12/05/2016 The use of variable frequency drives (VFDs) has many benefits including improved process control, e... |
End users desire speed and/or torque control procure and install VFDs to modify existing applicatio... |
10/25/2016 Assessing the motor before repairs and a well thought-out preventive maintenance program can help r... |
Variable frequency drives (VFDs) are designed to reduce energy usage by controlling the speed of th... |
Inside Machines: Lumber machine manufacturer’s moves to servo control yields increased precision, p... |
09/29/2016 Yaskawa Motoman's 6-axis MA1440 arc welding robot features a 6 kg payload and a large 50 mm wrist h... |
09/28/2016 Although VFD manufacturers have made many advances in terms of ease of use, some users still find p... |
Yaskawa Motoman's MH12 six-axis robot is designed for assembly, dispensing, material handling, mach... |
Variable frequency drives (VFDs) have become ubiquitous in manufacturing, and there are many aspect... |
09/21/2016 Strategy combines compressor motor, drive in one package. |
PID loop tuning may not be a hard science, but it’s not magic either. Here are some tuning tips tha... |
05/31/2016 A new control strategy and implementation system optimize variable frequency drive (VFD) efficiency... |
Engineers generally don't get very involved in politics, but that needs to change. Engineering is c... |
Best automation, control, and instrumentation products in 27 categories. |
01/26/2016 Engineers must understand how the components in the HVAC systems they design use power and how they... |
The global market for centrifugal pumps is expected to grow to over $40 billion in 2019, but the oi... |
12/23/2015 The Motion Control and Motor Association outlined several motion trends for 2016 including the Indu... |
Ask Control Engineering: How can variable speed drives increase efficiency? Links to resources on v... |
12/07/2015 High radio frequency (RF) leakage currents in drive-powered systems can be eliminated by using spec... |
Sophisticated, vacuum-compatible motion devices are increasingly being used by product designers an... |
11/27/2015 Respondents to the Consulting-Specifying Engineer 2015 HVAC and Building Automation Systems (BAS) S... |
11/23/2015 Key findings from The Association for Packaging and Processing Technologies Research. |
11/17/2015 Here are some best practices for designing building automation systems (BAS) and controls for HVAC ... |
The ability to program and control robots, servos, and drives with one software package is availabl... |
EASA AR100 details steps to take to clean, repair, and test equipment. |
In a typical wastewater treatment plant, aeration blowers are the largest single consumer of energy... |
Inside Machines: In low- and medium-voltages, three-phase induction motors are the most widely used... |
How product innovations are revolutionizing pump monitoring and process control management. |
09/24/2015 Companies are considering upgrades for primary process control systems, but upgrades for secondary ... |
09/03/2015 Upgrade your next machine design with servo motors to decrease downtime, decrease footprint, increa... |
08/10/2015 Machine designers strive to increase throughput, decrease machine costs, and reduce maintenance cos... |
08/08/2015 Knowing the truth about VFD operation can simplify the selection process for choose a variable freq... |
Below are a few key comparisons between small and large engineering firms that specify HVAC and bui... |
Voltage fluctuations not only affect performance, it can also put the safety of electrical devices ... |
Engineers must understand how the components in the systems they design use power and how they can ... |
06/04/2015 Harmonics mitigation, filtering voltage spikes are two key issues. |
05/22/2015 Servo system selection criteria involves more than just wattage and price. Other important servo cr... |
A general-purpose test system can be viewed as a research and development tool and a production and... |
05/05/2015 Cover story: HMI-historian integration cover story: Integration of historians with human-machine in... |
04/30/2015 Cycling motors on and off could be a way to meet demand; minimize starts, stops, and run time; and ... |
04/13/2015 A rudimentary understanding of how shaft sizes are determined can be helpful to anyone who works wi... |
Multi-phase ac induction motors have traditionally dominated the electric motor industry. The indus... |
02/26/2015 Advice follows on using proportional-integral-derivative (PID) tuning for motion control and roboti... |
02/23/2015 When designing a system and automating it, there are numerous professionals involved with each of t... |
12/03/2014 Hands-on experience helps accelerate the PID learning curve. |
Engineering and IT Insight: Programming and the other associated tasks of design, installation, deb... |
Servo control software improves applications requiring accurate path tracking and low settling time... |
10/30/2014 One-in-four control loops are regulating level, but techniques for tuning PID controllers in these ... |
10/20/2014 For those who are just getting into writing ladder logic and have maybe taken a few classes or seen... |
Engineering and IT Insight: Lazy?! Great control system programmers spend more time in design so th... |
10/15/2014 Correctly setting controls for pumps and circulators is key to achieving energy savings. |
Testing drive-and-motor systems is a three-step process. |
10/06/2014 There is no “one size fit all” formula for legacy migration of control systems, but assessing the a... |
09/29/2014 Cross-referencing really can be an art. If successful it can save a company time and money, whereas... |
Ask Control Engineering blog links to 60 years of motors, drives, and motion control coverage for t... |
Node: lr1
|