Industry News
09/19/2014 Motor design and motion control: Earliest electric motor designs reach back 150 years. While motor ... |
09/19/2014 Automation tales in motion: Great changes have taken place in motion control systems over the past ... |
Compressed air is very common in all industrial facilities and there has been a major push to ident... |
08/28/2014 A college’s decision to use reclaimed water lieu of a cooling tower saves millions of gallons of dr... |
08/28/2014 Automatic control operations can be described as either open-loop or closed-loop. The difference is... |
08/27/2014 Engineering and IT Insight: Good coding habits reduce errors, save time, and can help you become a ... |
Taking advantage of technology enhancements - and introducing a level of unwarranted risk - is a fi... |
Having the guidelines of ISA-88 hierarchy and equipment structure, how can this basis be used to ma... |
08/08/2014 While PID control is often used because of its adaptability to a wide range of applications and ope... |
07/29/2014 New wrist-mounted device augments the human hand with two robotic fingers. |
Engineers must strike the right balance on the centralized/distributed control system design spectr... |
07/22/2014 Engineering and IT Insight: Control programming is programming, even if it uses ladder logic, seque... |
Oversized actuators can add unnecessary costs to the damper if improperly sized |
07/01/2014 When choosing a tuning strategy for a specific control loop, it is important to match the technique... |
Guidance on performance monitoring is featured in a newly published guideline from ASHRAE. |
06/03/2014 Case study: Automated Industrial Machinery (AIM Inc.) moved from an analog interface to servo ampli... |
05/27/2014 Historically, the facility management challenge has been to do more with less. System integration p... |
05/20/2014 Low power factor can drain generation capacity, waste energy, and increase maintenance costs with e... |
Technology Update: Industrial facilities should include a system evaluation, including a harmonic d... |
05/16/2014 A cost-efficient energy recovery chiller allowed a Wisconsin hospital to achieve higher energy effi... |
A few basic differences between control engineers and others in the plant can hinder progress towar... |
After receiving the approval for a control system replacement project, how do you decide between ph... |
Understand the basics to drive greater efficiency. |
03/20/2014 Take advantage of a variety of common technologies and systems to help minimize the energy and cost... |
Ecolabs designed and now manages the wastewater treatment process for a Northern Californian vineya... |
When using a servo motor, one should consider torque, speed, and other applications for a specific ... |
02/03/2014 A variable frequency drive (VFD) often is specified to save money by reducing energy consumption in... |
01/27/2014 In the information age, data centers are one of the most critical components of a facility. If the ... |
01/27/2014 In the information age, data centers are one of the most critical components of a facility. If the ... |
Echelon’s Varun Nagaraj answers one-on-one questions, explaining how the Internet of Things can and... |
12/23/2013 Next generation HMIs create an environment where operators and technicians can move at speed of man... |
According to a report from IHS Inc., tablets are single-handedly driving the global market for LCD ... |
12/11/2013 Application Update: Olmsted County increased the energy processed at its waste-to-energy facility b... |
12/11/2013 Tuning a PID controller correctly can bring the setpoint closer to the constraint with reduced vari... |
11/21/2013 Follow these 10 steps to create a successful sequence of operation, one of the most important desig... |
11/20/2013 VFD configuration for permanent magnet alternating current (PMAC) motors and other considerations c... |
10/22/2013 A basic understanding of frame construction can help minimize motor vibration. |
Consider how a PD controller would work, without an integral function. Would you ever want to use t... |
TSA manufacturing upgraded the speed controls for their thread roller by adding a variable speed dr... |
10/12/2013 Automatic retry can double the noise immunity of real-time industrial Ethernet-based motion network... |
09/16/2013 An analysis on an office building in Milwaukee shows a dramatic difference in chiller operating cos... |
Scotty’s “Captain, I’m giving you all she’s got,” tells Kirk that he’s reached maximum output. The ... |
When migrating or upgrading your automation system, don’t forget to examine this group of areas out... |
Further investigation needed before making a decision on motor repair |
08/14/2013 PLCs have come a long way since the late 1960s and their applications in engineering are both innov... |
Inside Machines: To properly select the appropriate servo motor for a motion control application, f... |
07/03/2013 Engineering and IT Insight: Proper infrastructure, policies, and procedures for manufacturing IT ar... |
05/13/2013 You’ve see the equations, but have you thought about how those elements work together? Part 2: Addi... |
05/09/2013 Calculating your efficiency will point the way to the right decision |
05/06/2013 You’ve seen the equations, but have you thought about how those elements work together? Part 1: The... |
Sports arenas and entertainment facilities involve complex engineering solutions. Five consulting e... |
Revenue for MCCs and soft starters used for oil and gas extraction, manufacturing and transportatio... |
Market growth will return in 2013, driven by the growing number of applications which will be more ... |
04/16/2013 Understanding a particularly conservative PID controller design technique. |
Sometimes we need to think about an individual control loop. Other times we need to consider the la... |
The compound annual growth rate (CAGR) for new motor control Ethernet nodes is projected to be the ... |
As system integration strategies become more complex, the need for improved building automation sys... |
03/21/2013 Engineering and IT Insight: Embedded systems are often mechanically connected to other systems, and... |
03/13/2013 Successful projects follow performance standards from project start to end. |
02/26/2013 Concepts of APC can be implemented a little bit at a time but still make big steps toward getting y... |
02/15/2013 Here is the story of the mechanical, or HVAC, engineer. Take a look at this snapshot of where your ... |
02/14/2013 Cabling—like other components—must be vetted for its ability to withstand the harshest operating co... |
When selecting servo-based motion control systems, it’s all about the application. |
02/13/2013 The ability to balance return inlets requires some thought and evaluation. |
Due to intense competition and the penetration of new lower cost compact drives, profit margins dec... |
01/24/2013 By becoming a building systems integrator, engineers can ensure successful buildings—and a successf... |
Designing efficient and effective data centers and mission critical facilities is a top priority fo... |
01/08/2013 Using an element of object oriented programming can keep data organized and simplify writing code. |
Machine-room-less (MRL) elevator sales in the U.S. are continuing to grow, according to IMS Researc... |
12/27/2012 Air handling units come in all shapes and sizes. Learn to balance and prioritize all of the choices... |
The Kagami-Biraki sake ceremony celebrates the start of U.S. manufacturing of the Yaskawa MV1000 me... |
Colleges and universities bear the important responsibility of molding the minds of future generati... |
Colleges and universities bear the important responsibility of molding the minds of future generati... |
12/10/2012 Analog is holding its own, but more applications depend on digital communication to move growing am... |
With daunting aspects such as ever-changing codes and standards, increasing medical complexity, and... |
Node: lr2
|