News
Breadcrumb
Navigation Menu
News
NewsDisplay
Back
Important considerations when sizing linear and direct-drive technologies
Feb 08, 2023Learning Objectives
- Understand that mechanical data supports machine performance.
- Validate motor and drive sizing with the support of software.
- Consider design long-term versus initial costs in direct-drive systems.
Linear and direct-drive insights
- Direct-drive motors are more suitable for rotary applications, which require more torque at lower speeds than linear motors.
- While sizing an application, using the latest sizing software can reduce the chances of oversizing or undersizing a motor for an application. It also allows people to compare and contrast between motor capabilities.
- When considering both linear and direct-drives, it is important to factor in immediate costs compared to long-term costs.
Node: dxpprd01:8080