USB Driver Installation
This section describes how to install the
USB driver software for SERVOPACK.
The SERVOPACK USB driver cannot be
installed by using the SigmaWin+ installer.
When a SigmaWin+ equipped PC is connected
to the SERVOPACK through a USB connection, use the following procedure to
install the USB driver.
The installation method will vary
depending on the operating system (hereinafter referred to as OS). Use the
correct procedure for your OS.
The installation procedure is explained
assuming that the SigmaWin+ installed folder directory is “C:\Program
Files\SigmaIDE” and that the CD-ROM drive is D drive. Use the folder directory
and drive according to the settings of your PC.
For Windows XP
For Windows 2000
2.Confirming the Installation Status
(1)
Turn on the power to
the PC to start Windows 7 or Windows Vista.
(2)
Connect the
SERVOPACK to the PC using a USB cable, and then turn on the power to the
SERVOPACK.
(3)
When "No driver
found" appeared, click Close.

(4)
Click the Computer,
Property, and Device Manager.

(5)
Double-Click
“YASKAWA SIGMA SERIES”, Click “Update Driver”.
(6)
Click “Browse my
computer for driver software”.
(7)
Select the folder “C:\Program Files\SigmaIDE\SigmaWinPlusJ\Driver\USB” if the SigmaWin+ has already been installed, select
“D:\Driver\USB” if it is not yet installed. Select “Include subfolders” and
then Click Next.

(8)
When “Windows
Security” appeared, Click “Install this driver software anyway”.
(9)
The copy of a
necessary file starts, and wait for a while until finished.
(10) When the installation is completed, click Close.

(11) The driver installation is completed.
(1)
Turn on the power to the PC to start
Windows XP.
(2)
Connect the SERVOPACK to the PC using a
USB cable, and then turn on the power to the SERVOPACK.
(3)
After “The Found New Hardware Wizard” is
appeared,confirm that the Install from a list or
specified location [Advanced] option is selected, and then click Next.

(4)
Insert the SigmaWin+ installation disk
into the CD-ROM drive. (If the CD-ROM is automatically started and the
installation is started, cancel the installation.)
(5)
Select the Search for the best driver in
these locations. option and then select the Include this location in the
search: check box. Click Browse to select the folder “C:\Program
Files\SigmaIDE\SigmaWinPlus\Driver\USB” if the SigmaWin+ has already been
installed, or select “D:\Driver\USB” if it is not yet installed.Click Next.

(6)
The Wizard starts installation by copying
the necessary files. Wait until a message appears informing you that the
installation is finished.

(7)
When the installation is finished, click
Finish.
(8)
This completes the driver
installation.






Use the following procedure to make sure that the system recognizes
the SERVOPACK as a USB device and that the USB driver is installed correctly.