IndexWorks 1.72 Upgrade For Technical Support, Call 1-800-YASKAWA ----------------------------------------- Instructions: ----------------------------------------- TO UPGRADE FROM VERSION 1.70 OR LATER: 1. Copy files from upgrade ZIP file to the directory where IndexWorks was installed (Default is "C:\Program Files\Yaskawa\IndexWorks\"). 4. Run (double-click) IndexWorks1_72.reg file located in the directory where IndexWorks was installed. ----------------------------------------- TO UPGRADE FROM VERSION 1.50 OR LATER: 1. Unregister existing IndexWorks Utility.dll found at [installed path]\Utility.dll To unregister dll: a. Open command prompt window (Start Menu, "run" command) b. Type in command: regsvr32 -u "[full file path]" If the default installation directory was used, the command will be: regsvr32 -u "C:\Program Files\Yaskawa\IndexWorks\Utility.dll" Note: Windows 95 requires command to be entered while within regsvr32's directory. 2. Copy all files from upgrade ZIP file to the directory where IndexWorks was installed (Default is "C:\Program Files\Yaskawa\IndexWorks\"). 3. Register new Utility.dll To register dll: a. Open Command Prompt Window (Start Menu, "Run" command) b. Type in command: regsvr32 "[full file path]" If the default installation directory was used, the command will be: regsvr32 "C:\Program Files\Yaskawa\IndexWorks\Utility.dll" 4. Run (double-click) IndexWorks1_72.reg file located in the directory where IndexWorks was installed.