When using Cam Toolbox, you must also include the PLCopen Toolbox and the Math Toolbox in the main project, otherwise, compile errors will result. For Cam Toolbox v204 and higher – If upgrading from an older version of Cam Toolbox, you must do the following: 1) Include the DataTypes Toolbox v200 or higher in your project. 2) Include PLCopen Toolbox v206 or higher in your project. 3) Remove any Yaskawa supplied datatype files from your project with firmware library definitions such as a. MotionBlockTypes b. PLCTaskInfoTypes c. ControllInfoTypes d. YDeviceCommTypes Starting with MotionWorks IEC v3.0, the new project templates will include the PLCopen and DataTypes Toolboxes.