American National Standards Institute (ANSI) / American Society of Mechanical Engineers (ASME)ANSI/ASME A17.1-2007/ B44-04 Safety Code for Elevators and Escalators Includes Requirements for Elevators,Escalators, Dumbwaiters, Moving Walks, Material Lifts, and Dumbwaiters with Automatic Transfer Devicesusing EN 12016:2004 immunity requirements.
Inverters incorporate electrolytic capacitors and other electronic components that incorporate chemical changes. The characteristics of these components may change during long periods of storage. This document discusses storage place, periodic application of power, and environment-resistance specifications. 2 pages.
This document contains a basic description of configuring, connecting and controlling a Yaskawa AC Drive with either a ControlLogix or CompactLogix PLC on an EtherNet/IP network. Although the description uses a single Yaskawa AC Drive, the principle can be expanded to include a large number of devices. This document and the examples contained herein do not describe all possible methods of connectivity and programming.
This document describes how SI-P3 & SI-P3/V comply to the PROFIdrive standard. PROFIdrive is a standardized method, within the Profibus-DP protocol of accessing and controlling a drive. It allows for the replacement of a drive that conforms to the PROFIdrive profile with any other conforming drive regardless of manufacturer.
Document describes application of Positive Temperature Coefficient thermistors (PTC) to Yaskawa series drives E7, P7, F7, A1000, and Z1000 which include an analog input function to provide motor over-temperatureprotection for motors.
This document describes how to set up a Yaskawa drive to suppress nuisance overload faults that may be encountered with systems that are slightly undersized or unexpectedly operate into the motor service factor.
The purpose of this document is to discuss the methods available in Yaskawa VFDs that can be used to address applications where starting into a rotation cannot be avoided.
The purpose of this application note is to guide users on how to properly write to the drive parameters over Modbus. The application note will take into account the ENTER command, parameter sequence and dependencies as it relates to control method, drive kVA and V/f settings to name a few.
The purpose of this document is to provide basic guidance regarding how to program a Yaskawa drive to run a Baldor SynRM² motor, which is referred to as a ferrite-assisted synchronous reluctance motor. This document is relative specifically to the Baldor EC-Titanium branded motors.
The following application note provides the user with basic instructions on how to quickly configure a Marathon Symax Permanent Magnet motor using a Yaskawa drive.
It looks like you are using Internet Explorer 11 or below, this website isn`t compatible with this and for the best experience please use the latest version of Mozilla Firefox, Google Chrome or Safari.