This record contains:1) An Application Note detailing the methods within the PLCi DLLs and how to create a communication interface with an MPiec controller. Communication capabilities include: variable exchange, file manipulation, and PLC control services.2) An installer package which contains the PLCi communication DLLs.3) An example Visual Studio C# project.4) An example MotionWorks IEC project.
The Linear Flying Shear Application Solution Package (ASP) offers an easy way to implement linear flying shear applications. This solution package was designed for machines that process products spaced at fixed intervals or machines must make dynamic corrections based on a product registration mark. The Linear Flying Shear ASP project can be used as a starting point template on which the user can complete the application, or the ASP can be added as a user library into an existing project. The Linear Flying Shear ASP focuses only on the core motion features required to operate a flying shear and does not include other functionality such as servo enable, homing, manual modes, alarm handling, etc. The user is responsible for incorporating other basic logic functionality required for the application. Two example projects in which the ASP is used as a user library for MotionWorks IEC Versions 2 and 3 (LFS_DemoOnMP2300Siec.zwt and LFS_DemoOnMP3300iec.zwt, respectively) are provided.
User Library for MotionWorks IEC containing POUs with functions that build upon the YDeviceComm firmware library. Email, FTP, and command streaming tools are included.
Example code for implementing a Command & Response interface between a PC program and an MPiec Series Controller. Included are: MotionWorks IEC project using the Comm Toolbox, Visual Basic 6 example code, Visual Studio 2012 example code in VB, Applet file for web browser
User Library for MotionWorks IEC containing POUs with functions that build upon the YDeviceComm firmware library. Email, FTP, and command streaming tools are included.
Starting with Math_Toolbox_v310, several function blocks were removed from the Math_Toolbox. These functions are no longer needed for new applications, but in the event an old project is updated, this Legacy_Math_Toolbox will provide those functions.
It looks like you are using Internet Explorer 11 or below, this website isn`t compatible with this and for the best experience please use the latest version of Mozilla Firefox, Google Chrome or Safari.