A1000 Drive

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

What A1000 enclosure types are available?

01/03/2011

On the A1000 series, if a unidirectional 3-wire control is desired, can the directional digital input (H1-0X = 0) be disabled?

11/13/2013

My drive has a CPF25 fault on it, my V1000 manual has no information on this alarm. What are some troubleshooting techniques to apply?

10/29/2012

Is the A1000 the same physical size as F7?

01/04/2011

Is the A1000 dual rated?

01/04/2011

In troubleshooting LF fault the manual says the output current has exceeded 5% imbalance. How can I calculate this imbalance?

04/01/2014

In Normal Duty mode, is the default carrier frequency higher than 2kHz?

01/04/2011

If the drives carrier frequency is changed , is it necessary to re-autotune the drive?

04/09/2012

I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues?

08/13/2013

I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that?

02/28/2013

How to change motor direction when rotating backwards?

10/30/2012

How do I save and recall parameter settings for User Initialization?

02/28/2013

How do I re-allocate a digital input on a DI-100 or DI-101?

10/03/2013

How do I get a 0-20mA signal out of the analog outputs?

02/28/2013

How do I create a User-Set scaling in the 1000 series drives?

02/28/2013

How does the physical size of the GA800 compare with the A1000?

01/11/2019

How does GA800 differ from A1000 when installing the drive outside of an enclosure?

01/11/2019

How can the design life of the A1000 be twice that of the F7?

01/04/2011

Hbb fault occurs with the H1,H2 and HC jumpered, what else could the issue be?

08/28/2012

Does the A1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else?

02/29/2012

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.