A1000 Drive

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

Will there be a remote keypad option for the A1000?

01/04/2011

Where is the A1000 manufactured?

01/04/2011

Where does the A1000 fit into Yaskawa's family of drives, and what does it offer beyond the F7?

01/03/2011

When will single phase input capacities be available for A1000 and what kind of derating is expected?

01/03/2011

When using 2 option cards, I am receiving an OPE06 fault and am not seeing all the F1 parameters. I am using CN5-B for my encoder feedback card.

10/09/2012

What training is available for A1000?

01/03/2011

What tools are available to help customers convert from G5 (600V) and F7 to A1000?

01/03/2011

What is the warranty determination for new product?

05/22/2014

What is the scan rate of the A1000?

01/04/2011

What is RoHS?

08/18/2015

What is EN61800-5-1 and TUV?

01/04/2011

What is California's Proposition 65?

06/01/2020

What do I do if I am having problems connecting to the A1000 USB port?

09/27/2011

What documentation ships with the A1000?

01/03/2011

What control methods does the A1000 offer?

01/04/2011

What are the new capabilities of DriveWizard Industrial, and will it be backward compatible?

01/14/2019

What are the differences between the A1000 600V and A1000 240/480V models?

01/04/2011

What are the details regarding A1000 12 Pulse?

05/30/2012

What are the A1000's ratings?

01/04/2011

What A1000 enclosure types are available?

01/03/2011

On the A1000 series, if a unidirectional 3-wire control is desired, can the directional digital input (H1-0X = 0) be disabled?

11/13/2013

My drive has a CPF25 fault on it, my V1000 manual has no information on this alarm. What are some troubleshooting techniques to apply?

10/29/2012

Is the A1000 the same physical size as F7?

01/04/2011

Is the A1000 dual rated?

01/04/2011

In Normal Duty mode, is the default carrier frequency higher than 2kHz?

01/04/2011

If the drives carrier frequency is changed , is it necessary to re-autotune the drive?

04/09/2012

I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues?

08/13/2013

I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that?

02/28/2013

How to change motor direction when rotating backwards?

10/30/2012

How do I save and recall parameter settings for User Initialization?

02/28/2013

How do I re-allocate a digital input on a DI-100 or DI-101?

10/03/2013

How do I get a 0-20mA signal out of the analog outputs?

02/28/2013

How do I create a User-Set scaling in the 1000 series drives?

02/28/2013

How does the physical size of the GA800 compare with the A1000?

01/11/2019

How does GA800 differ from A1000 when installing the drive outside of an enclosure?

01/11/2019

How can the design life of the A1000 be twice that of the F7?

01/04/2011

Hbb fault occurs with the H1,H2 and HC jumpered, what else could the issue be?

08/28/2012

Does the A1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else?

02/29/2012

Can we replace simple servo applications using existing PM servo motors?

01/04/2011

Can the 600V models of the A1000 and P1000 be used with a 690VAC input voltage?

01/03/2011

Are there plans for a dedicated 600V micro-drive?

01/03/2011

Are the digital outputs able to be inverted?

06/21/2013

Are the A1000 network communications full function Modbus or Yaskawa standard?

01/04/2011

Are F7 Options compatible with A1000? Can A1000 Options be used with F7?

01/04/2011

Are end caps (NEMA 1 kits) available for the protected chassis versions?

05/31/2012

Are adaptor plates available for mechanical mount retrofitting of F7?

08/17/2012

Are A1000 options compatible with GA800? Can GA800 options be used with A1000?

01/11/2019

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.