G5 Drive 600 Volt

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

Why don't the page numbers in the parameter section of the instruction manual match the page numbers in the body of the manual?

06/11/2014

When dealing with harmonic noise, which is better-- an AC or a DC reactor?

06/20/2013

What is the current rating for the Run and Fault output contacts on a GPD 515/G5?

07/13/2004

What is required to start and stop the GPD515/G5 from the digital operator?

06/08/2007

What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display?

10/27/2005

What are the differences between the set-up of a GPD515/G5 and a F7 drive on DeviceNet when using CM053 or CM056 option cards?

11/28/2005

What are some concerns when the motor cable is over 100 meters?

06/20/2013

UV -- Fault Code Description

06/08/2007

UV3 - Fault Code Description

06/20/2013

UV2 - Fault Code Description

06/20/2013

UV1 - Fault Code Description

06/20/2013

The GPD 515/G5 displays a parameter, but does not let me change it. Why?

07/13/2004

The GPD/515G5 instruction manual (TOE-S616-10.13) (pages 21-22) specifies that input fuses should be used on the installation of these drives.--Is fusing required or is a circuit breaker sufficient protection for the inverter?--If fusing is not required, what characteristics of MCCB should used be to protect the drive adequately?

06/08/2007

SVE -- Fault Code Description

06/08/2007

Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive?

06/12/2014

SC - Fault Code Description

06/08/2007

RR -- Fault Code Description

06/08/2007

RH -- Fault Code Description

06/08/2007

PGO -- Fault Code Description

06/08/2007

PF - Fault Code Description

06/08/2007

OV -- Fault Code Description

06/08/2007

OV - Fault Code Description

06/20/2013

OS -- Fault Code Description

06/08/2007

OPR -- Fault Code Description

06/08/2007

OPE11 -- Fault Code Description

06/08/2007

OPE10 -- Fault Code Description

06/08/2007

OPE08 -- Fault Code Description

06/08/2007

OPE07 - Fault Code Description

06/08/2007

OPE06 -- Fault Code Description

06/08/2007

OPE05 -- Fault Code Description

06/08/2007

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.