G7 Drive

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

When replacing the motor for the application and the heat sink cooling fans. How do I reset Cumulative Motor Operation Time U1-13 and Heat Sink Cooling Fan Operation Time U1-40?

09/16/2013

When reading 42h it does not match U1-03? Using Ethernet or Modbus protocols.

08/31/2012

What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure?

03/14/2006

What is the warranty determination for new product?

05/22/2014

What is the meaning of CAL or CALL on the keypad display?.

10/28/2005

What is the ambient temperature derating (L8-12 setting)?

01/22/2007

What is California's Proposition 65?

06/01/2020

What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display?

10/27/2005

What are the main causes of the VCF/VCN alarm?

12/20/2014

What are some counter-measures to reduce harmonics created by AC drives?

06/08/2007

Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive?

06/12/2014

Is it possible to use auto-tuning without rotating the motor?

07/13/2004

Is it possible to adjust the brightness for the operator display?

07/13/2004

If the drives carrier frequency is changed , is it necessary to re-autotune the drive?

04/09/2012

I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that?

02/28/2013

Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration?

10/27/2005

Can multiple motors be used with a single inverter?

06/20/2013

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.