V1000 Drive

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

Will the V1000 drive be part of the configured drive program?

07/27/2007

Will DriveWizardTM Plus be backward compatible?

07/27/2007

Will DriveWizard Industrial be backward compatible?

01/04/2011

Where is the V1000 manufactured?

07/27/2007

What steps are necessary to connect a Yaskawa V1000 to an MPiec series controller over ethernet?

12/12/2016

What is the warranty determination for new product?

05/22/2014

What is the scan rate of the V1000?

07/27/2007

What is the maximum frequency limitation of the pulse input?

07/27/2007

What is RoHS?

08/18/2015

What is EN954-1 Safety Category 3?

07/27/2007

What is California's Proposition 65?

06/01/2020

What enclosure types are available for the V1000?

07/27/2007

What documentation ships with the V1000?

07/27/2007

What Control Methods does the V1000 offer?

07/27/2007

On the V1000 series drive, should the H1, HC circuit be used with an external 24V supply?

10/21/2013

On the A1000 series, if a unidirectional 3-wire control is desired, can the directional digital input (H1-0X = 0) be disabled?

11/13/2013

My drive has a CPF25 fault on it, my V1000 manual has no information on this alarm. What are some troubleshooting techniques to apply?

10/29/2012

Is the design life of the V1000 is twice that of the V7

07/27/2007

Is the Copy function available with the standard LED keypad on the V1000 and V1000-4X drives?

06/21/2010

Is EtherCat available for Yaskawa Drives?

10/30/2012

Is a remote keypad an option?

07/27/2007

In troubleshooting LF fault the manual says the output current has exceeded 5% imbalance. How can I calculate this imbalance?

04/01/2014

I have an existing DWEZ program that was written for V1000. Can I reuse the program on the GA500?

09/27/2019

If the drives carrier frequency is changed , is it necessary to re-autotune the drive?

04/09/2012

I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues?

08/13/2013

I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that?

02/28/2013

How many connections can DWEZ Pro handle?

07/27/2007

How do I save and recall parameter settings for User Initialization?

02/28/2013

How do I create a User-Set scaling in the 1000 series drives?

02/28/2013

How about the Analog Input Connector Cable?

07/27/2007

Do we have a USB cable interface (instead of serial) for hookup to laptops for DriveWizard Plus?

07/27/2007

Do I need an adapter plate when replacing a V1000 with a GA500?

09/27/2019

CPF00 -- Fault Code Description

06/20/2013

Can the V1000 be applied to HVAC applications?

07/27/2007

Can I reuse the option card that's installed on my V1000 on the GA500? Or do I need to purchase a new card?

11/04/2019

Are V7 Options compatible with V1000? Can V1000 Options be used with V7?

07/27/2007

Are the V1000 network communications full function Modbus or Yaskawa standard?

07/27/2007

Are the V1000 and V1000-4X the same physical size as the V7?

07/27/2007

Are the digital outputs able to be inverted?

06/21/2013

Are common multimeters able to measure the correct output voltage of the VFD?

04/01/2014

After installation of DriveWizard Plus on a Dell PC, the following Windows error is displayed when attempting to launch the application: The application failed to initialize properly (0xc000007b). Click on OK to terminate the application.

01/03/2011

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.