MP940 Machine Controller
FAQs
Question | Posted Date | |
---|---|---|
In a vertical axis application, the motor trips the overtravel switch and coasts to the hard stop. What might be the cause? |
07/23/2001 | |
How many registers are there for each data type (bit, word, long, float), and how are the LONG and REAL data types referenced? |
07/13/2004 | |
How is the MP940 analog input used? |
04/20/2001 | |
How is External Positioning (latch target) setup in an MP920/930 SVB mode over mechatrolink? |
07/13/2004 | |
How can the software limits in the MP controllers be configured? |
08/19/2004 | |
How can a defective ServoPack (SGDH) be replaced in the field when a working MP940 is connected? |
10/11/2002 | |
How are registers in the MP9xx controller monitored from the PC? |
09/06/2004 | |
How are pLimit_PositioningError and sPosition_CompletionWindow used to control positioning accuracy? |
05/21/2001 | |
How are cam tables organized? |
05/21/2001 | |
Does Yaskawa supply an EDS file for the MP940D (DeviceNet)? |
07/13/2004 | |
Does Yaskawa offer a template program for the MP940 when using MotionWorks+? |
06/24/2013 | |
Does the torque limit (sLimit_Torque) need to be set on the MP940? |
05/02/2001 | |
Can the decimal or binary value of multiple inputs be read and compared? |
07/13/2004 | |
Can subroutines be called from "L" or "H" drawings? |
03/05/2002 | |
Are there any tools to monitor or troubleshoot MP920 and MP940 function blocks operation? |
02/22/2005 | |
Are there any third party HMI Manufacturers that have written Memobus Drivers for the Yaskawa MP9xx products? |
04/11/2006 | |
Are there any examples of a "flying shear" or "rotary placer" program using MW+? |
07/22/2002 | |
Are there any documents available to help with an EXOR/Yaskawa system start-up? |
06/24/2013 | |
Are example application programs available for the EXOR HMI when using an MP940 Machine Controller? |
02/13/2014 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.