MP940 Machine Controller
FAQs
Question | Posted Date | |
---|---|---|
Yaskawa offers a great MP940 / MotionWorks+ (MW+) template program, but it is fairly complex. Is there a simplified version of the template program without all of the bells and whistles? |
06/24/2013 | |
Why does the SGDH servopack flash "bb" continuously? |
09/06/2004 | |
When using MotionWorks+, is there a way to tell which version of a project is currently in the RAM memory of the MP940 and the last date it was revised? |
07/13/2004 | |
When running into hardware limits, motion is disabled in both directions. How can the axis be jogged off the limit switch? |
07/13/2004 | |
When an MP940 with a 17-bit encoder is being operated, does the encoder resolution need to be reduced? |
04/27/2001 | |
What version of Sigma II fimware is required if using an option card such as the MP940? |
04/04/2002 | |
Whats the maximum number of User Function blocks that can be used in the MP900 series controllers? |
03/06/2002 | |
What is the reason for the long deceleration when using a Direct Drive Motor system with a Sigma 2 Servopack (SGDH) and MP940? What are the steps to properly tune such a system? |
07/25/2005 | |
What is the procedure to setup a rotary axis in MP controllers using MotionWorks? |
08/19/2004 | |
What is the power-up sequence for the MP940? |
07/13/2004 | |
What is the most common solution to communication errors in a Mechatrolink Network? |
06/24/2013 | |
What is the maximum number of cam data points that can be stored in a cam table? |
07/13/2004 | |
What is the format of the Floating Point data structure in the MP920, MP930, MP940 series products? |
07/13/2004 | |
What is the difference between Z registers and A registers when used in Function Blocks? |
04/30/2002 | |
What is the difference between the I/O on the Sigma II and the MP940? Do both need to be used? |
04/26/2001 | |
What is the difference between MODBUS and Memobus? |
04/26/2001 | |
What is the difference between JEPMC-W6060 and JZSP-CKI01 cables? |
06/25/2014 | |
What is the difference between a YS-13 and YS-15 cable? |
07/13/2004 | |
What is an SVA module? |
06/25/2013 | |
What is an A.9F alarm? |
09/12/2000 | |
What is a "DWG" (drawing)? |
05/02/2001 | |
What I/O cable options are there for the MP940? |
11/29/2004 | |
What are the steps to set up a Mechatrolink or DeviceNet Network on an MP940 with MotionWorks+? |
07/13/2004 | |
What are the recommended programming practices when using function blocks? |
09/06/2004 | |
What are the possible causes of communication failure between an HMI and a MP9xx controller? |
05/03/2001 | |
What are the differences between single-axis and multi-axis function blocks? |
09/21/2004 | |
What are some potential causes of an A.E2 alarm? |
06/24/2013 | |
What are some issues that would cause a web application to drift when using camming with registration, and what are some remedies to this condition? |
07/13/2004 | |
Product Demo Documentation: MP940 |
06/26/2013 | |
Many new computers do not offer serial communication ports. How is communication possible to Yaskawa products if no serial port is available? |
06/25/2013 | |
Is there information regarding DeviceNet Troubleshooting for the MP series products? |
10/30/2001 | |
Is there a wiring example of an MP940 following a Sigma II SGDH servo master? |
07/13/2004 | |
Is there a Register Quick Reference Guide for the MP940 Controller? |
11/04/2003 | |
Is there a procedure outlining the start-up of an MP940 Controller System? |
02/15/2006 | |
Is there a procedure for starting up an MP940 with an absolute encoder? |
07/13/2004 | |
Is there any information available about a free software to use for opening Yaskawa 2D drawings such as dwg and dxf? |
05/15/2014 | |
Is there an example showing an MP940 as a DeviceNet Master controlling NS300's as slave devices? |
09/06/2001 | |
Is there a list of User's Manuals for the MP900 Series Products? |
10/20/2006 | |
Is there a list of technical recommendations for safe guarding an MP940 Servo Control System against overspeed conditions? |
08/29/2005 | |
Is there a list of Ladder Instructions that can be used in the MP900 series products? |
03/08/2002 | |
Is there a guideline on how to use and allocate registers when programming the MP900 series controllers? |
03/06/2002 | |
Is there a detailed procedure on how to read/write parameters from/to fieldbus NS-300/500 modules? |
06/25/2013 | |
Is the MP-940 capable of operating Yaskawa linear motors? |
01/14/2005 | |
Is it possible to transfer cam data from Mircosoft Excel to an MP controller? |
10/26/2005 | |
Is it possible to set up ASCII text fields in an HMI Recipe to specify recipe name so it can be modified and stored in an MP9** Controller? |
11/08/2001 | |
Is it possible to route the POT and NOT signals through DeviceNet on an MP940D? |
09/05/2001 | |
Is it possible to Monitor/Program an MP9** Product over a phone line from a remote location? |
07/13/2004 | |
Is it possible to connect multiple MP940s to one EXOR HMI? |
12/21/2011 | |
Is it possible to connect a TCP HMI to Yaskawa MP Products? |
07/13/2004 | |
Is it possible to connect a Red Lion HMI to Yaskawa MP Products? |
07/13/2004 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.