SMC-3010 LEGEND-MC

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

When using Bluetooth, can I rename the drive so that I can more easily identify it?

01/16/2020

When using an MP920's SVA Servo interface and an absolute encoder on a Sigma II Servopack (SGDH), how is the absolute data requested and confirmed complete in the application program?

09/21/2004

When using an absolute encoder, is it possible to set the absolute zero position through the Fieldbus Network?

01/09/2002

When using 2 option cards, I am receiving an OPE06 fault and am not seeing all the F1 parameters. I am using CN5-B for my encoder feedback card.

10/09/2012

When the personal computer (PC) serial port connection is disconnected from the controller, why does the SMC-2000/3010/4000 controller become unresponsive?

07/13/2004

When the E7 drive trips out on a fault it must be manually reset. Can the E7 be set to restart automatically after a fault?

06/08/2007

When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications?

07/13/2004

When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications?

02/18/2009

When running into hardware limits, motion is disabled in both directions. How can the axis be jogged off the limit switch?

07/13/2004

When replacing the motor for the application and the heat sink cooling fans. How do I reset Cumulative Motor Operation Time U1-13 and Heat Sink Cooling Fan Operation Time U1-40?

09/16/2013

When reading 42h it does not match U1-03? Using Ethernet or Modbus protocols.

08/31/2012

When moving away from a overtravel condition, the Sigma V servo system seems to prevent torque or rapidly enable/disable as the axis is moving out of the overtravel region. Can this situation be prevented?

10/06/2011

When is it necessary to connect an external regen resistor to the SGDG LEGEND amplifier?

01/21/2002

When I install my serial communications option board onto the Z1000 drive in the Z1B cabinet, I recieve alarm OFA00. What am I doing wrong?

02/28/2013

When entering Motor Rated Current (parameter E2-01) into an E7 drive, an OPE02 fault appears on the display. What can cause this, and how is the fault cleared?

06/08/2007

When dealing with harmonic noise, which is better-- an AC or a DC reactor?

06/20/2013

When configuring an IP address in the resource settings of MotionWorks IEC, what are the -TO and -P attributes?

11/10/2017

When an MP940 with a 17-bit encoder is being operated, does the encoder resolution need to be reduced?

04/27/2001

What’s the maximum number of axes that could be controlled and configured by a Compass solution?

05/21/2020

What Z1000 enclosure types are available?

11/29/2011

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.