SMC-3010 LEGEND-MC
Breadcrumb
Navigation Menu
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC - YAI
Single-axis motion controller
The SMC-3010 LEGEND-MC is a legacy product and no longer promoted in the Americas. The SMC-3010 series was a single-axis machine controller with Ethernet communcation that attached to any Yaskawa LEGEND amplifier. Featured 100% digital design, multi-axis control via software, dual programming screens, and high performance and reliability.
TemplateWeb
FAQs
Showing 676 to 750 of 1,000 entries.
Question | Posted Date | |
---|---|---|
In Normal Duty mode, is the default carrier frequency higher than 2kHz? Posted Date: 01/04/2011
|
01/04/2011 | |
In Normal Duty mode, is the default carrier frequency higher than 2kHz? Posted Date: 08/01/2008
|
08/01/2008 | |
In MotionWorks IEC Pro, what is the difference between a 'zipped' and a 'sealed' project? Posted Date: 07/03/2013
|
07/03/2013 | |
In MotionWorks IEC Hardware Configuration, why are the Mechatrolink III axes displayed as offline when the ServoPacks are powered up with no alarms? Posted Date: 06/05/2015
|
06/05/2015 | |
In MotionWorks IEC Hardware Configuration, how can a configured axis be moved from one node number to another? Posted Date: 03/13/2014
|
03/13/2014 | |
In MotionWorks IEC, what does the Permanent as Bootproject mean? Posted Date: 05/03/2017
|
05/03/2017 | |
In MotionWorks IEC, what causes the Misaligned Datatype error and how can it be resolved? Posted Date: 03/18/2013
|
03/18/2013 | |
In MotionWorks IEC, how can Mechatrolink-III be configured to run at the fastest update rate? How can a Mechtrolink-III network be configured to be robust to cabling differences? Posted Date: 03/12/2014 |
03/12/2014 | |
In MotionWorks IEC, how can I compare parameters across multiple drives? Posted Date: 03/12/2014
|
03/12/2014 | |
In MotionWorks IEC, how can an axis be moved from one node number to another? Posted Date: 06/27/2013
|
06/27/2013 | |
I need access to the drive parameters on a Z1000 Bypass. What is the correct procedure to do so? Posted Date: 08/05/2013
|
08/05/2013 | |
In Compass, how do we abort move in auto mode? Posted Date: 05/21/2020 |
05/21/2020 | |
In Compass, can you add decimal variables like injection speed or pressure? Posted Date: 05/19/2020 |
05/19/2020 | |
In a vertical axis application, the motor trips the overtravel switch and coasts to the hard stop. What might be the cause? Posted Date: 07/23/2001
|
07/23/2001 | |
In "rotary shortest" mode, what direction will the motor move if the commanded index is exactly opposite of the current position? Posted Date: 03/18/2002
|
03/18/2002 | |
I just recently added a PG board to my F7 drive, I now have a CPF06 active on my drive and it will not clear, what did I do wrong? Posted Date: 08/28/2012
|
08/28/2012 | |
I have a problem printing a MotionWorks IEC project. One of the error messages I receive says "Missing Source Data." Is there a solution to this issue? Posted Date: 06/28/2013
|
06/28/2013 | |
I have an existing DWEZ program that was written for V1000. Can I reuse the program on the GA500? Posted Date: 09/27/2019
|
09/27/2019 | |
If we have our own software interface, can we implement Compass to our interface? Posted Date: 05/19/2020
|
05/19/2020 | |
If three LEGEND-MC controllers are on a network and each of them is doing point-to-point moves, can the I/O of all controllers be used within the program? Posted Date: 03/21/2002
|
03/21/2002 | |
If the Home switch (HOME) and inputs (EXT1, EXT2, EXT3) to the Sigma III Mechatrolink version Servopack are not used, and are not masked, can they be used as general purpose MP2000 inputs instead? Posted Date: 07/25/2005
|
07/25/2005 | |
If the drives carrier frequency is changed , is it necessary to re-autotune the drive? Posted Date: 04/09/2012
|
04/09/2012 | |
If a variable has both an Initial Value and is marked as Retained, which value will the IEC application use after a Warm Start? What value will be used after a Cold Start? Posted Date: 10/11/2013
|
10/11/2013 | |
I cannot change the V/f pattern parameters from default. Is there a parameter inhibiting my changes? Posted Date: 08/02/2013
|
08/02/2013 | |
I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues? Posted Date: 08/13/2013
|
08/13/2013 | |
I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that? Posted Date: 02/28/2013
|
02/28/2013 | |
I am replacing my V1000 with a GA500. How can I convert the parameters quickly? Posted Date: 09/27/2019
|
09/27/2019 | |
I am replacing my P1000 with a FP605. How can I convert the parameters quickly? Posted Date: 04/07/2022
|
04/07/2022 | |
I am beginning EtherCAT master development. What do I need to know in regards to the Yaskawa drive interface? Posted Date: 03/16/2015
|
03/16/2015 | |
I already have a Partner Account for www.yaskawa.com, can I use it for my Yaskawa Drive Cloud login? Posted Date: 08/03/2018
|
08/03/2018 | |
How to tune with a SigmaLogic? Posted Date: 02/15/2016 |
02/15/2016 | |
How to set up the Multi-turn Limit for an Infinite Axis with an Absolute Encoder Posted Date: 02/18/2009
|
02/18/2009 | |
How to program HOA for P7 drive? Posted Date: 07/17/2012
|
07/17/2012 | |
How to Import POU's in MotionWorks IEC? Posted Date: 04/29/2019
|
04/29/2019 | |
How to identify a G5 vs. G5+ AC drive. Posted Date: 06/20/2013
|
06/20/2013 | |
How to convert a MotionWorks IEC Version 2 Project into Version 3? Posted Date: 12/14/2020
|
12/14/2020 | |
How to convert a MotionWorks IEC Version 2 Library to MotionWorks IEC Version 3? Posted Date: 12/08/2015
|
12/08/2015 | |
How to change motor direction when rotating backwards? Posted Date: 10/30/2012
|
10/30/2012 | |
How to be in auto run on power up? Posted Date: 08/21/2012
|
08/21/2012 | |
How should the upper controller (or DeviceNet master) be programmed in order to establish motion at the NS300 Posted Date: 12/17/2001
|
12/17/2001 | |
How should the Analog Input Module JAPMC-AN2300 be wired for voltage mode or current mode? Posted Date: 04/02/2016
|
04/02/2016 | |
How should an SGDH amplifier be configured if controlled by an SVA-02? Posted Date: 12/22/2011
|
12/22/2011 | |
How should an 8-byte message through Profibus be manipulated to achieve motion with an NS-500 Indexer? Posted Date: 07/13/2004
|
07/13/2004 | |
How much does DriveWizard Mobile and Yaskawa Drive Cloud cost? Posted Date: 08/03/2018
|
08/03/2018 | |
How many registers are there for each data type (bit, word, long, float), and how are the LONG and REAL data types referenced? Posted Date: 07/13/2004
|
07/13/2004 | |
How many monitors can I record with the data logger feature? Posted Date: 04/07/2022
|
04/07/2022 | |
How many monitors can I record with the data logger feature? Posted Date: 09/27/2019
|
09/27/2019 | |
How many latch inputs are on the 400 VAC Sigma-7W Mechatrolink-III Dual Axis Servopack? Posted Date: 11/06/2018
|
11/06/2018 | |
How many latch inputs are on the 400VAC Sigma-7W EtherCAT Dual Axis Servopack? Posted Date: 12/10/2018
|
12/10/2018 | |
How many latch inputs are on the 200 VAC Sigma-7W Mechatrolink-III Dual Axis Servopack? Posted Date: 01/03/2019
|
01/03/2019 | |
How many indexing steps can you make with SigmaLogic and LogicWorks? Posted Date: 09/15/2014 |
09/15/2014 | |
How many digital outputs can be allocated on the Z1000 bypass? Posted Date: 10/07/2013
|
10/07/2013 | |
How many control option cards can the FP605 configured package support? Posted Date: 02/17/2023
|
02/17/2023 | |
How many connections can DWEZ Pro handle? Posted Date: 07/27/2007
|
07/27/2007 | |
How many cam table points are available in the MPiec Series Controllers? Posted Date: 08/15/2013
|
08/15/2013 | |
How long will the Z1000 still be available? Posted Date: 09/03/2019
|
09/03/2019 | |
How long will the absolute encoder battery last on a Sigma-5 or Sigma-7 servo system? Posted Date: 03/17/2016
|
03/17/2016 | |
How long will a Sigma II absolute encoder remember its absolute position data without a battery attached? Posted Date: 07/13/2004
|
07/13/2004 | |
How long is the return number valid? Posted Date: 04/22/2014
|
04/22/2014 | |
How is torque feed forward implemented using an MPiec series controller? Posted Date: 02/08/2016
|
02/08/2016 | |
How is the Sequence Table Executed on SigmaLogic? Posted Date: 03/02/2015
|
03/02/2015 | |
How is the regen capacity (Pn600) set through the IEC Configuration Tool? Posted Date: 01/20/2009
|
01/20/2009 | |
How is the P1000 rated and what are its limitations? Posted Date: 06/29/2012
|
06/29/2012 | |
How is the normal web page displayed when “This web UI requires a modern browser. … “ message is displayed in a Chrome browser? Posted Date: 03/29/2019
|
03/29/2019 | |
How is the MP940 analog input used? Posted Date: 04/20/2001
|
04/20/2001 | |
How is the memory stored in an MP-2000 series controller? Posted Date: 06/25/2013
|
06/25/2013 | |
How is the kW output scaled on the Dual Analog Output option board (Model DS418)? Posted Date: 06/12/2014
|
06/12/2014 | |
How is the inverter reset after an alarm has gone off Posted Date: 07/13/2004
|
07/13/2004 | |
How is the home sensor wired when using an SGDH with an NS600? Posted Date: 07/24/2013
|
07/24/2013 | |
How is the fully-closed encoder option configured when using the JUSP-NS500? Posted Date: 07/13/2004
|
07/13/2004 | |
How is the fully-closed encoder option configured when using the JUSP-NS300? Posted Date: 07/13/2004
|
07/13/2004 | |
How is the fully-closed encoder option configured when using the JUSP-FC100? Posted Date: 07/13/2004
|
07/13/2004 | |
How is the error “The application image could not be bound to the kernel firmware profile!” corrected? Posted Date: 01/04/2019
|
01/04/2019 | |
How is the download error “The sum of static data size and dynamic data size exceeds the physical available data memory size” fixed? Posted Date: 11/28/2018
|
11/28/2018 | |
How is the % tolerance on the incoming voltage specs factored in for an SGDH? Posted Date: 06/25/2013
|
06/25/2013 | |
Showing 676 to 750 of 1,000 entries.
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.