SMC-3010 LEGEND-MC
FAQs
Question | Posted Date | |
---|---|---|
Where is the D1000 manufactured? |
07/15/2015 | |
Where Is the Compile Error Location When Double-Clicking On It? |
03/08/2019 | |
Where is the A1000 manufactured? |
01/04/2011 | |
Where do I send my repair item? |
04/22/2014 | |
Where do I install the network communication option card on the FP605 bypass? |
02/17/2023 | |
Where do I install the input/output option cards when using the FP605 bypass package? |
02/17/2023 | |
Where does the P1000 fit into Yaskawa's family of drives, and what does it offer beyond the P7? |
06/29/2012 | |
Where does the GA800 fit into Yaskawa's family of drives, and what does it offer beyond the A1000? |
01/09/2019 | |
Where does the GA500 fit into Yaskawa's family of drives? |
09/26/2019 | |
Where does the FP605 fit into Yaskawa's family of drives? |
03/29/2022 | |
Where does the A1000 fit into Yaskawa's family of drives, and what does it offer beyond the F7? |
01/03/2011 | |
Where can pin out details for the YS-12 cable be found? |
07/13/2004 | |
Where can I find UL certification documents for Yaskawa MPiec Controller products? |
06/12/2014 | |
Where can I find the supporting documents for UL approval of the MP2000 controllers? |
02/04/2011 | |
Where can I find frequently asked questions for MV1000? |
03/31/2015 | |
Where can I find electrical and mechanical drawings? |
03/26/2021 | |
Where can Error Code Descriptions be found for SigmaLogic? |
10/20/2014 | |
Where are the help files located for SigmaLogic, LogicWorks and Add-on Instructions (AOI)? |
10/09/2014 | |
When will single phase input capacities be available for P1000 and what kind of derating is expected? |
06/29/2012 | |
When will single phase input capacities be available for A1000 and what kind of derating is expected? |
01/03/2011 | |
When will a heatsink through the back solution be available, and what enclosure rating will it be capable of? |
11/29/2011 | |
When using the analog output function on a GPD506/P5, how is the output scaled when output current is selected? |
06/12/2014 | |
When using SMC-2000 analog input, where is the ground (common) signal connected? |
05/22/2001 | |
When using SigmaWin software, what are the units when graphing torque? |
07/13/2004 | |
When using MotionWorks IEC ver3.3.0, how can the error message “Library does not exist” be avoided when saving the Hardware Configuration? |
01/27/2017 | |
When using MotionWorks+, is there a way to tell which version of a project is currently in the RAM memory of the MP940 and the last date it was revised? |
07/13/2004 | |
When using DriveWizard HVAC on a Z1000 Bypass do I connect to the Z1000 Drive or the Electronic Bypass Contol PCB? |
05/23/2013 | |
When using Bluetooth, can I rename the drive so that I can more easily identify it? |
01/16/2020 | |
When using an MP920's SVA Servo interface and an absolute encoder on a Sigma II Servopack (SGDH), how is the absolute data requested and confirmed complete in the application program? |
09/21/2004 | |
When using an absolute encoder, is it possible to set the absolute zero position through the Fieldbus Network? |
01/09/2002 | |
When using 2 option cards, I am receiving an OPE06 fault and am not seeing all the F1 parameters. I am using CN5-B for my encoder feedback card. |
10/09/2012 | |
When the personal computer (PC) serial port connection is disconnected from the controller, why does the SMC-2000/3010/4000 controller become unresponsive? |
07/13/2004 | |
When the E7 drive trips out on a fault it must be manually reset. Can the E7 be set to restart automatically after a fault? |
06/08/2007 | |
When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications? |
07/13/2004 | |
When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications? |
02/18/2009 | |
When running into hardware limits, motion is disabled in both directions. How can the axis be jogged off the limit switch? |
07/13/2004 | |
When replacing the motor for the application and the heat sink cooling fans. How do I reset Cumulative Motor Operation Time U1-13 and Heat Sink Cooling Fan Operation Time U1-40? |
09/16/2013 | |
When reading 42h it does not match U1-03? Using Ethernet or Modbus protocols. |
08/31/2012 | |
When moving away from a overtravel condition, the Sigma V servo system seems to prevent torque or rapidly enable/disable as the axis is moving out of the overtravel region. Can this situation be prevented? |
10/06/2011 | |
When is it necessary to connect an external regen resistor to the SGDG LEGEND amplifier? |
01/21/2002 | |
When I install my serial communications option board onto the Z1000 drive in the Z1B cabinet, I recieve alarm OFA00. What am I doing wrong? |
02/28/2013 | |
When entering Motor Rated Current (parameter E2-01) into an E7 drive, an OPE02 fault appears on the display. What can cause this, and how is the fault cleared? |
06/08/2007 | |
When dealing with harmonic noise, which is better-- an AC or a DC reactor? |
06/20/2013 | |
When configuring an IP address in the resource settings of MotionWorks IEC, what are the -TO and -P attributes? |
11/10/2017 | |
When an MP940 with a 17-bit encoder is being operated, does the encoder resolution need to be reduced? |
04/27/2001 | |
What’s the maximum number of axes that could be controlled and configured by a Compass solution? |
05/21/2020 | |
What Z1000 enclosure types are available? |
11/29/2011 | |
What would cause an "06" communications error code in an HMI when talking to one or more NS600(s)? |
11/21/2001 | |
What will happen to the P7? |
06/29/2012 | |
What will happen to the E7? |
11/29/2011 | |
What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure? |
03/14/2006 | |
What web browser technology is supported by the MPiec Series Controllers? |
01/02/2018 | |
What web browsers are compatible with the MPiec controller's web server? |
01/23/2018 | |
What voltage levels will cause an overvoltage or undervoltage alarm? |
02/06/2009 | |
What voltage levels will cause an overvoltage or undervoltage alarm? |
03/02/2015 | |
What version of Sigma II fimware is required if using an option card such as the MP940? |
04/04/2002 | |
What version of Java is required to view the Machine Operations page of an MPiec Controller? |
07/04/2013 | |
What type of Errors and Alarms are on the controller? |
02/18/2009 | |
What training is available for P1000? |
06/29/2012 | |
What training is available for HV600? |
09/03/2019 | |
What training is available for GA800? |
01/11/2019 | |
What training is available for A1000? |
01/03/2011 | |
What tools are available to help customers convert from P7 to P1000? |
06/29/2012 | |
What tools are available to help customers convert from G5 (600V) and F7 to A1000? |
01/03/2011 | |
What tools are available to help customers convert from F7 and A1000 to GA800? |
01/11/2019 | |
What tools are available to help customers convert from E7 to Z1000? |
11/29/2011 | |
What tools are available to help customers convert from E7 and Z1000 to HV600? |
09/03/2019 | |
Whats the maximum number of User Function blocks that can be used in the MP900 series controllers? |
03/06/2002 | |
What steps are required to upgrade Sigma products to Sigma II? |
04/10/2006 | |
What steps are required to communicate to a LEGEND-MC from a laptop PC via Ethernet? |
07/13/2004 | |
What steps are necessary to connect a Yaskawa V1000 to an MPiec series controller over ethernet? |
02/26/2021 | |
What software tools are available to save F7 drive parameter settings to a PC file? |
09/13/2012 | |
What should the inertia ratio parameter, Pn103, be set to in the Sigma II amplifier when the inertia ratio is not known? |
06/24/2013 | |
What should be done with the CN8 connection when using the Safety Option Module (SGDV-OSA01A)? |
06/09/2023 | |
What settings are needed to configure the E7 Bypass for serial communication control in AUTO mode and keypad speed control in HAND mode? |
06/11/2014 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.