MotionWorks IEC

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

What is the best way to correctly use the RETURN instruction? We had some issues in some cases when the Functions blocks get stuck, or needs an additional trigger.

10/06/2011

What is the best method to convert a STRING into a BYTE array and vice versa? Why is this conversion useful?

04/22/2014

What is a typical cause of error code 4630 when using MC_TouchProbe?

04/02/2016

What does the “E2005 the field offset exceeds the limit” compile error mean?

01/30/2020

What does the compiler message "Internal Error: Overflow. (Specific Code Generator)" mean and what is the remedy?

03/12/2014

What causes the MotionWorks IEC error message "The project cannot be downloaded because it was compiled for a different device or a different version of the connected device. Please select the device version in the Resource Settings Dialog that matches the connected device."

09/13/2018

What can cause a MotionWorks IEC 3.x USB license key to be unrecognized?

01/27/2017

What are the remedies when an I/O configuration error is present in MotionWorks IEC?

10/18/2010

What are some tips for operating a single load with multiple servo motors?

03/12/2014

The Motionworks IEC software stopped running after installing InteractX software? How can I recover from this?

03/04/2010

The MotionWorks IEC Hardware Configuration software is unable to connect to the MPiec controller. What should I check to correct the problem?

09/23/2013

The Hardware Configuration launches, but does not appear after using dual displays, is there a way to reset its position?

08/04/2014

Must the data type be the same for every variable in a calculation? I get a compile error when I try (REAL := REAL * INT).

05/26/2009

It is possible to install a single licensed copy of MotionWorks IEC on multiple computers and move the license from computer to computer?

01/26/2016

Is there information available on replacing a Sigma-5 Mechatrolink ServoPack in a system controlled by an MPiec Series Controller without using MotionWorks IEC software?

09/23/2013

Is there information available file types / extensions associated with Yaskawa motion software products?

05/19/2017

Is there a variable that will show which step of a Sequential Function Chart (SFC) program is currently executing?

07/04/2013

Is there a solution for MotionWorks IEC v2.x to enable the Hardware Configuration to recognize an unknown SGDV model number?

12/20/2017

Is there a solution for display issues when using the MPiec controller's web server with Internet Explorer 10?

06/11/2013

Is there a remedy for recovering a MotionWorks IEC project that shows the error: "No suitable converter for projects created with the version '2.0' of MotionWorks IEC Pro?

09/21/2011

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.