SGDH Sigma II
FAQs
Question | Posted Date | |
---|---|---|
Why does the SGDH servopack flash "bb" continuously? |
09/06/2004 | |
Why does the Servopack display an AF1 alarm when main power is removed? None of the solutions in the User's manual remedy the problem. |
07/13/2004 | |
Where can pin out details for the YS-12 cable be found? |
07/13/2004 | |
When using SigmaWin software, what are the units when graphing torque? |
07/13/2004 | |
When using an absolute encoder, is it possible to set the absolute zero position through the Fieldbus Network? |
01/09/2002 | |
When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications? |
07/13/2004 | |
When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications? |
02/18/2009 | |
What voltage levels will cause an overvoltage or undervoltage alarm? |
03/02/2015 | |
What voltage levels will cause an overvoltage or undervoltage alarm? |
02/06/2009 | |
What version of Sigma II fimware is required if using an option card such as the MP940? |
04/04/2002 | |
What steps are required to upgrade Sigma products to Sigma II? |
04/10/2006 | |
What should the inertia ratio parameter, Pn103, be set to in the Sigma II amplifier when the inertia ratio is not known? |
06/24/2013 | |
What might be the cause of a brake relay chattering (turning on and off rapidly) on a vertical axis? |
07/13/2004 | |
What is the purpose of the Near Output Signal (/NEAR) in Sigma II drives? |
01/13/2003 | |
What is the proper value to enter in Pn600 when Yaskawa Regenerative Resistor Unit is used? |
07/13/2004 | |
What is the maximum setting for parameter Pn281 (PG Divider) given the linear scale pitch and maximum speed of the linear motor? |
07/13/2004 | |
What is the inrush current of an SGDH amplifier? |
04/16/2001 | |
What is the difference between the I/O on the Sigma II and the MP940? Do both need to be used? |
04/26/2001 | |
What is the difference between JEPMC-W6060 and JZSP-CKI01 cables? |
06/25/2014 | |
What is the current requirement of the 24VDC control power supply for 400V Sigma II amplifiers? |
01/03/2002 | |
What is the cause of an A.CC Alarm? |
08/27/2004 | |
What is the approximate maximum number of times the Sigma II Series flash ROM can be written? |
02/14/2006 | |
What is speed feedback compensation and when should it be used? |
07/13/2004 | |
What is an A.E7 alarm and how is it cleared? |
07/13/2004 | |
What is an A.E5 alarm? |
01/22/2002 | |
What is an A.9F alarm? |
09/12/2000 | |
What is an A.09 alarm? |
12/22/2011 | |
What could cause an motor to run away when it is enabled (/S-ON goes low)? |
07/13/2004 | |
What are the pin-outs for SGDH analog monitor connector CN5? |
09/21/2004 | |
What are the minimum parameters required to start-up a Sigma II SGDH type servo amplifier for use with a linear motor? |
07/25/2005 | |
What are some remedies to an A.C9 (Encoder Communications) alarm? |
07/13/2004 | |
What are some potential causes of an A.E2 alarm? |
06/24/2013 | |
What are some potential causes of an A.84 Alarm? |
06/30/2008 | |
What are some of the potential causes of an A.80 Alarm? |
04/12/2006 | |
What are potential implications of using an Electro-Mechanical Relay or Switching Power Supply in conjunction with a Sigma II Servo System to enable the motor? Can A.C9 and A.E2 alarms be symptoms? |
07/13/2004 | |
On a linear motor x-x'-y gantry system, what is the best method to control the two x-axes? |
06/06/2003 | |
Many new computers do not offer serial communication ports. How is communication possible to Yaskawa products if no serial port is available? |
06/25/2013 | |
Is upgrading from Sigma to Sigma II the best option? |
04/13/2006 | |
Is there information available file types / extensions associated with Yaskawa motion software products? |
05/19/2017 | |
Is there a wiring example of an MP940 following a Sigma II SGDH servo master? |
07/13/2004 | |
Is there a way to get 4 bi-directional 'contact speeds' with sigma II (SGDH)? |
05/22/2006 | |
Is there a quick way to reset SGDH servo alarms without using PC software? |
05/21/2001 | |
Is there a procedure for starting-up a Sigma II Servo System with an Absolute Encoder? |
07/13/2004 | |
Is there any information available about a free software to use for opening Yaskawa 2D drawings such as dwg and dxf? |
05/15/2014 | |
Is there an alternative explanation of the term "User Units" pertaining to Yaskawa's electronic gearing built into the Servopacks and JUSP-NSxxx option board products? |
07/13/2004 | |
Is there a list of technical recommendations for safe guarding an MP940 Servo Control System against overspeed conditions? |
08/29/2005 | |
Is there a driver available to communicate between an Exor HMI and a Yaskawa Sigma ServoPack? |
07/13/2004 | |
Is there a compiled list of Sigma II alarms? |
07/13/2004 | |
Is the MP-940 capable of operating Yaskawa linear motors? |
01/14/2005 | |
Is it possible to simply control speed in a Sigma II amplifier without a controller? |
10/24/2002 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.