Support
Frequently Asked Questions
Question | Posted Date | |
---|---|---|
What is the procedure to setup a rotary axis in MP controllers using MotionWorks? |
08/19/2004 | |
What is the procedure to reset an MPiec controller back to factory defaults? |
01/27/2017 | |
What is the procedure to replace an FSP to keep the parameters including the motor parameters in the case of using a third party motor? |
04/02/2016 | |
What is the procedure for changing the motor rotation direction with a LEGEND-MC controller? |
07/13/2004 | |
What is the power-up sequence for the MP940? |
07/13/2004 | |
What is the outer diameter of SGMAV/SGMJV Premium motor power cables? |
03/17/2016 | |
What is the most common solution to communication errors in a Mechatrolink Network? |
06/24/2013 | |
What is the memory capacity for the MP2000 IEC Controllers? |
01/05/2011 | |
What is the memory allocation for the MPiec Controllers? |
01/17/2018 | |
What is the meaning of CAL or CALL on the keypad display?. |
10/28/2005 | |
What is the maximum value of pLimit_PositioningError? |
12/21/2001 | |
What is the maximum size of G file supported by Compass? |
05/21/2020 | |
What is the maximum setting for parameter Pn281 (PG Divider) given the linear scale pitch and maximum speed of the linear motor? |
07/13/2004 | |
What is the maximum sample rate used in the trending graphic on current Drivewizard software? |
12/10/2013 | |
What is the maximum output frequency of the GA500? |
09/27/2019 | |
What is the maximum number of cam data points that can be stored in a cam table? |
07/13/2004 | |
What is the maximum frequency limitation of the pulse input? |
07/27/2007 | |
What is the maximum connection distance of the Bluetooth keypad? |
09/26/2019 | |
What is the life expectancy of a Sigma-5 motor when operating above 40 degrees Celsius (104 F)? |
10/18/2010 | |
What is the lead time if a Sigma SD unit is not in stock? |
02/21/2018 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.