Support
Frequently Asked Questions
Question | Posted Date | |
---|---|---|
What is an A.9F alarm? |
09/12/2000 | |
What is an A.09 alarm? |
12/22/2011 | |
What is a "Multi-Function Digital Input"? |
09/13/2012 | |
What is a "DWG" (drawing)? |
05/02/2001 | |
What is 2-Wire Control and 3-Wire Control? |
07/13/2004 | |
What is +P common |
02/13/2013 | |
What information is available for implementing PLCopen "Function Blocks for Motion Control" in the MP2000 series products? |
07/24/2013 | |
What improvements have been made in BACnet communication? |
05/14/2020 | |
What impedance is the output reactor option? |
05/13/2021 | |
What if an MP2300 module needs to be replaced? Is the module configuration stored in the main CPU? |
12/19/2006 | |
What I/O cable options exist for the NS600? |
07/18/2014 | |
What I/O cable options are there for the NS500? |
09/21/2004 | |
What I/O cable options are there for the NS300? |
09/21/2004 | |
What I/O cable options are there for the MP940? |
11/29/2004 | |
What happens when switching to reverse while the motor is rotating forward (FWD=OFF, REV=ON)? |
11/28/2005 | |
What happens if the STOP button on the Digital Operator is pressed, while the drive is being controlled remotely by START/STOP circuitry connected to the drives I/O terminal block? Can the drive be restarted locally? |
06/07/2007 | |
What happens if a forward command and a reverse command are closed on the terminal block at the same time? |
11/28/2005 | |
What features does the Junma SERVOPACK have compared with other SERVOPACKS? |
08/15/2011 | |
What external keypad kit options are available for the FP605? |
04/04/2022 | |
What environments are suitable for the HV600 drives? |
09/03/2019 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.