Support

Frequently Asked Questions

Didn't find what you were looking for? Try
  Question Posted Date

Is an AC input reactor needed with the Single Phase Converter?

09/12/2017

Is a driver available for the Exor HMI to talk to the JUSP-NS600 Sigma II Indexer application module?

02/22/2005

Is a drawing of part number JUSP-TA50PG-E available?

01/05/2016

Is a drawing and pin-out of part number JUSP-TA50P available?

07/13/2004

Is a drawing and pin-out of part number JUSP-TA36P available?

07/13/2004

Is a braking resistor internally installed?

06/20/2013

In what ways is the U1000 iQpump different from competitor's products?

02/08/2017

In what ways is the U1000 different from competitor’s products?

04/21/2015

In what languages can the GPD 515/G5 display?

07/13/2004

In troubleshooting LF fault the manual says the output current has exceeded 5% imbalance. How can I calculate this imbalance?

04/01/2014

In the MP940 controller, how are the FLASH and COPY switches used?

05/21/2001

In some pumping systems the motor speed is normally about 80% of rated motor speed. However, periodic purging of the pumping system requires the pump to go to full speed for a while, then return to normal. How is this done with the V7 Drive?

10/27/2005

In SigmaWin+ Trace what is the difference between Position Error and Position Amplifier Error?

11/30/2010

In SigmaWin+ Trace, what is the difference between position error, position amplifier error, and motor-load position error?

05/23/2018

In order to identify the parameter causing the OPE alarm, one goes to monitor U1-18. On the Z1000 Bypass cabinet, the parameter states "Z0-00". What does this mean?

10/21/2013

In Normal Duty mode, is the default carrier frequency higher than 2kHz?

01/04/2011

In Normal Duty mode, is the default carrier frequency higher than 2kHz?

08/01/2008

In MotionWorks IEC Pro, what is the difference between a 'zipped' and a 'sealed' project?

07/03/2013

In MotionWorks IEC Hardware Configuration, why are the Mechatrolink III axes displayed as offline when the ServoPacks are powered up with no alarms?

06/05/2015

In MotionWorks IEC Hardware Configuration, how can a configured axis be moved from one node number to another?

03/13/2014

In MotionWorks IEC, what does the Permanent as Bootproject mean?

05/03/2017

In MotionWorks IEC, what causes the Misaligned Datatype error and how can it be resolved?

03/18/2013

In MotionWorks IEC, how can Mechatrolink-III be configured to run at the fastest update rate? How can a Mechtrolink-III network be configured to be robust to cabling differences?

03/12/2014

In MotionWorks IEC, how can I compare parameters across multiple drives?

03/12/2014

In MotionWorks IEC, how can an axis be moved from one node number to another?

06/27/2013

I need access to the drive parameters on a Z1000 Bypass. What is the correct procedure to do so?

08/05/2013

In Compass, how do we abort move in auto mode?

05/21/2020

In Compass, can you add decimal variables like injection speed or pressure?

05/19/2020

In a vertical axis application, the motor trips the overtravel switch and coasts to the hard stop. What might be the cause?

07/23/2001

In "rotary shortest" mode, what direction will the motor move if the commanded index is exactly opposite of the current position?

03/18/2002

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.