Support

Frequently Asked Questions

Didn't find what you were looking for? Try
  Question Posted Date

What is the rating of the GA500’s 24 Vdc output?

09/30/2019

What is the rating of the FP605’s +24 VDC output?

03/31/2022

What is the rated current of the 24VDC holding brake on Sigma II motors?

07/13/2004

What is the purpose of the TEST switch on the front panel of an E7B bypass unit?

06/08/2007

What is the purpose of the Near Output Signal (/NEAR) in Sigma II drives?

01/13/2003

What is the purpose of a softcharge resistor and contactor in a GPD506 / P5 drive?

11/28/2005

What is the proper value to enter in Pn600 when Yaskawa Regenerative Resistor Unit is used?

07/13/2004

What is the proper sequence to reset a SigmaLogic Alarm?

03/08/2016

What is the procedure to setup a rotary axis in MP controllers using MotionWorks?

08/19/2004

What is the procedure to reset an MPiec controller back to factory defaults?

01/27/2017

What is the procedure to replace an FSP to keep the parameters including the motor parameters in the case of using a third party motor?

04/02/2016

What is the procedure for changing the motor rotation direction with a LEGEND-MC controller?

07/13/2004

What is the power-up sequence for the MP940?

07/13/2004

What is the outer diameter of SGMAV/SGMJV Premium motor power cables?

03/17/2016

What is the most common solution to communication errors in a Mechatrolink Network?

06/24/2013

What is the memory capacity for the MP2000 IEC Controllers?

01/05/2011

What is the memory allocation for the MPiec Controllers?

01/17/2018

What is the meaning of CAL or CALL on the keypad display?.

10/28/2005

What is the maximum value of pLimit_PositioningError?

12/21/2001

What is the maximum size of G file supported by Compass?

05/21/2020

What is the maximum setting for parameter Pn281 (PG Divider) given the linear scale pitch and maximum speed of the linear motor?

07/13/2004

What is the maximum sample rate used in the trending graphic on current Drivewizard software?

12/10/2013

What is the maximum output frequency of the GA500?

09/27/2019

What is the maximum output frequency of the FP605?

03/30/2022

What is the maximum number of cam data points that can be stored in a cam table?

07/13/2004

What is the maximum frequency limitation of the pulse input?

07/27/2007

What is the maximum connection distance of the Bluetooth keypad?

09/26/2019

What is the life expectancy of a Sigma-5 motor when operating above 40 degrees Celsius (104 F)?

10/18/2010

What is the lead time if a Sigma SD unit is not in stock?

02/21/2018

What is the latest driver for the EXOR HMI connected to an SMC controller, and does it provide hardware handshaking?

06/24/2013

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.