Support
Frequently Asked Questions
Question | Posted Date | |
---|---|---|
Is a serial converter required when using a Renishaw RESOLUTE encoder? |
05/02/2017 | |
Is a remote keypad an option? |
07/27/2007 | |
Is Apogee/Metasys available for the Z1000 & Z1000 Bypass |
09/12/2012 | |
Is any 3rd party programming software needed for SigmaLogic? |
09/15/2014 | |
Is an Allen Bradley PLC required for SigmaLogic? |
03/02/2015 | |
Is an AC input reactor needed with the Single Phase Converter? |
09/12/2017 | |
Is a driver available for the Exor HMI to talk to the JUSP-NS600 Sigma II Indexer application module? |
02/22/2005 | |
Is a drawing of part number JUSP-TA50PG-E available? |
01/05/2016 | |
Is a drawing and pin-out of part number JUSP-TA50P available? |
07/13/2004 | |
Is a drawing and pin-out of part number JUSP-TA36P available? |
07/13/2004 | |
Is a braking resistor internally installed? |
06/20/2013 | |
In what ways is the U1000 iQpump different from competitor's products? |
02/08/2017 | |
In what ways is the U1000 different from competitor’s products? |
04/21/2015 | |
In what languages can the GPD 515/G5 display? |
07/13/2004 | |
In troubleshooting LF fault the manual says the output current has exceeded 5% imbalance. How can I calculate this imbalance? |
04/01/2014 | |
In the MP940 controller, how are the FLASH and COPY switches used? |
05/21/2001 | |
In some pumping systems the motor speed is normally about 80% of rated motor speed. However, periodic purging of the pumping system requires the pump to go to full speed for a while, then return to normal. How is this done with the V7 Drive? |
10/27/2005 | |
In SigmaWin+ Trace what is the difference between Position Error and Position Amplifier Error? |
11/30/2010 | |
In SigmaWin+ Trace, what is the difference between position error, position amplifier error, and motor-load position error? |
05/23/2018 | |
In order to identify the parameter causing the OPE alarm, one goes to monitor U1-18. On the Z1000 Bypass cabinet, the parameter states "Z0-00". What does this mean? |
10/21/2013 | |
In Normal Duty mode, is the default carrier frequency higher than 2kHz? |
01/04/2011 | |
In Normal Duty mode, is the default carrier frequency higher than 2kHz? |
08/01/2008 | |
In MotionWorks IEC Pro, what is the difference between a 'zipped' and a 'sealed' project? |
07/03/2013 | |
In MotionWorks IEC Hardware Configuration, why are the Mechatrolink III axes displayed as offline when the ServoPacks are powered up with no alarms? |
06/05/2015 | |
In MotionWorks IEC Hardware Configuration, how can a configured axis be moved from one node number to another? |
03/13/2014 | |
In MotionWorks IEC, what does the Permanent as Bootproject mean? |
05/03/2017 | |
In MotionWorks IEC, what causes the Misaligned Datatype error and how can it be resolved? |
03/18/2013 | |
In MotionWorks IEC, how can Mechatrolink-III be configured to run at the fastest update rate? How can a Mechtrolink-III network be configured to be robust to cabling differences? |
03/12/2014 | |
In MotionWorks IEC, how can I compare parameters across multiple drives? |
03/12/2014 | |
In MotionWorks IEC, how can an axis be moved from one node number to another? |
06/27/2013 | |
I need access to the drive parameters on a Z1000 Bypass. What is the correct procedure to do so? |
08/05/2013 | |
In Compass, how do we abort move in auto mode? |
05/21/2020 | |
In Compass, can you add decimal variables like injection speed or pressure? |
05/19/2020 | |
In a vertical axis application, the motor trips the overtravel switch and coasts to the hard stop. What might be the cause? |
07/23/2001 | |
In "rotary shortest" mode, what direction will the motor move if the commanded index is exactly opposite of the current position? |
03/18/2002 | |
I just recently added a PG board to my F7 drive, I now have a CPF06 active on my drive and it will not clear, what did I do wrong? |
08/28/2012 | |
I have a problem printing a MotionWorks IEC project. One of the error messages I receive says "Missing Source Data." Is there a solution to this issue? |
06/28/2013 | |
I have an existing DWEZ program that was written for V1000. Can I reuse the program on the GA500? |
09/27/2019 | |
If we have our own software interface, can we implement Compass to our interface? |
05/19/2020 | |
If three LEGEND-MC controllers are on a network and each of them is doing point-to-point moves, can the I/O of all controllers be used within the program? |
03/21/2002 | |
If the Home switch (HOME) and inputs (EXT1, EXT2, EXT3) to the Sigma III Mechatrolink version Servopack are not used, and are not masked, can they be used as general purpose MP2000 inputs instead? |
07/25/2005 | |
If the drives carrier frequency is changed , is it necessary to re-autotune the drive? |
04/09/2012 | |
If a variable has both an Initial Value and is marked as Retained, which value will the IEC application use after a Warm Start? What value will be used after a Cold Start? |
10/11/2013 | |
I cannot change the V/f pattern parameters from default. Is there a parameter inhibiting my changes? |
08/02/2013 | |
I attempted to run the unit with the digital operator connected directly to the drive. I removed it and connected it back to the bypass board, now the Hand and Auto command are non-responsive. How can I fix this? |
12/03/2012 | |
I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues? |
08/13/2013 | |
I am using the MOP function on the 7 series drives and on my deceleration; the drive is following the speed pot instead of the deceleration time. Why is that? |
02/28/2013 | |
I am replacing my V1000 with a GA500. How can I convert the parameters quickly? |
09/27/2019 | |
I am replacing my P1000 with a FP605. How can I convert the parameters quickly? |
04/07/2022 | |
I am beginning EtherCAT master development. What do I need to know in regards to the Yaskawa drive interface? |
03/16/2015 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.