Support
Frequently Asked Questions
Question | Posted Date | |
---|---|---|
What parameter must be set when using a DC power supply for a SERVOPACK’s main circuit power supply? |
02/26/2019 | |
What P1000 enclosure types are available? |
06/29/2012 | |
What options are available to stop the motor using EtherCAT commands? |
12/22/2015 | |
What options are available to limit torque on the SGDV CANopen over EtherCAT SERVOPACK? |
07/15/2015 | |
What new features does the Z1000 offer beyond those of the E7? |
11/29/2011 | |
What network protocols does the Z1000U support? |
01/21/2015 | |
What motors can the GA500 operate? |
09/30/2019 | |
What might be the cause of a brake relay chattering (turning on and off rapidly) on a vertical axis? |
07/13/2004 | |
What manuals are required to start-up, operate, and program a LEGEND-MC Motion Controller? |
10/30/2001 | |
What makes the HV600 more convenient to program and set up? |
09/03/2019 | |
What keypad options are available for the GA500? |
09/30/2019 | |
What is Yaskawa’s repair policy for Sigma SD? |
02/21/2018 | |
What is Yaskawa DriveCloud, and what products does it support? |
01/14/2019 | |
What is the Yaskawa Solution Center and how do I use it? |
02/22/2019 | |
What is the wiring diagram for the MP920/MP930 programming cable? |
07/13/2004 | |
What is the warranty determination for new product? |
05/22/2014 | |
What is the vertical and horizontal clearance specification (in inches) for mounting any of the GPD506/P5 stand alone drives? |
11/28/2005 | |
What is the SCCR of the GA500? |
09/30/2019 | |
What is the scan rate of the V1000? |
07/27/2007 | |
What is the scan rate of the A1000? |
01/04/2011 | |
What is the recommended system requirement for Compass? Processor, memory, etc. |
05/21/2020 | |
What is the reason for the long deceleration when using a Direct Drive Motor system with a Sigma 2 Servopack (SGDH) and MP940? What are the steps to properly tune such a system? |
07/25/2005 | |
What is the rating of the GA500’s 24 Vdc output? |
09/30/2019 | |
What is the rated current of the 24VDC holding brake on Sigma II motors? |
07/13/2004 | |
What is the purpose of the TEST switch on the front panel of an E7B bypass unit? |
06/08/2007 | |
What is the purpose of the Near Output Signal (/NEAR) in Sigma II drives? |
01/13/2003 | |
What is the purpose of a softcharge resistor and contactor in a GPD506 / P5 drive? |
11/28/2005 | |
What is the proper value to enter in Pn600 when Yaskawa Regenerative Resistor Unit is used? |
07/13/2004 | |
What is the proper sequence to reset a SigmaLogic Alarm? |
03/08/2016 | |
What is the procedure to setup a rotary axis in MP controllers using MotionWorks? |
08/19/2004 | |
What is the procedure to reset an MPiec controller back to factory defaults? |
01/27/2017 | |
What is the procedure to replace an FSP to keep the parameters including the motor parameters in the case of using a third party motor? |
04/02/2016 | |
What is the procedure for changing the motor rotation direction with a LEGEND-MC controller? |
07/13/2004 | |
What is the power-up sequence for the MP940? |
07/13/2004 | |
What is the outer diameter of SGMAV/SGMJV Premium motor power cables? |
03/17/2016 | |
What is the most common solution to communication errors in a Mechatrolink Network? |
06/24/2013 | |
What is the memory capacity for the MP2000 IEC Controllers? |
01/05/2011 | |
What is the memory allocation for the MPiec Controllers? |
01/17/2018 | |
What is the meaning of CAL or CALL on the keypad display?. |
10/28/2005 | |
What is the maximum value of pLimit_PositioningError? |
12/21/2001 | |
What is the maximum size of G file supported by Compass? |
05/21/2020 | |
What is the maximum setting for parameter Pn281 (PG Divider) given the linear scale pitch and maximum speed of the linear motor? |
07/13/2004 | |
What is the maximum sample rate used in the trending graphic on current Drivewizard software? |
12/10/2013 | |
What is the maximum output frequency of the GA500? |
09/27/2019 | |
What is the maximum number of cam data points that can be stored in a cam table? |
07/13/2004 | |
What is the maximum frequency limitation of the pulse input? |
07/27/2007 | |
What is the maximum connection distance of the Bluetooth keypad? |
09/26/2019 | |
What is the life expectancy of a Sigma-5 motor when operating above 40 degrees Celsius (104 F)? |
10/18/2010 | |
What is the lead time if a Sigma SD unit is not in stock? |
02/21/2018 | |
What is the latest driver for the EXOR HMI connected to an SMC controller, and does it provide hardware handshaking? |
06/24/2013 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.