Support
Frequently Asked Questions
Question | Posted Date | |
---|---|---|
What is an A.E5 alarm? |
01/22/2002 | |
What is an A.9F alarm? |
09/12/2000 | |
What is an A.09 alarm? |
12/22/2011 | |
What is a "Multi-Function Digital Input"? |
09/13/2012 | |
What is a "DWG" (drawing)? |
05/02/2001 | |
What is 2-Wire Control and 3-Wire Control? |
07/13/2004 | |
What is +P common |
02/13/2013 | |
What information is available for implementing PLCopen "Function Blocks for Motion Control" in the MP2000 series products? |
07/24/2013 | |
What improvements have been made in BACnet communication? |
05/14/2020 | |
What impedance is the output reactor option? |
05/13/2021 | |
What if an MP2300 module needs to be replaced? Is the module configuration stored in the main CPU? |
12/19/2006 | |
What I/O cable options exist for the NS600? |
07/18/2014 | |
What I/O cable options are there for the NS500? |
09/21/2004 | |
What I/O cable options are there for the NS300? |
09/21/2004 | |
What I/O cable options are there for the MP940? |
11/29/2004 | |
What happens when switching to reverse while the motor is rotating forward (FWD=OFF, REV=ON)? |
11/28/2005 | |
What happens if the STOP button on the Digital Operator is pressed, while the drive is being controlled remotely by START/STOP circuitry connected to the drives I/O terminal block? Can the drive be restarted locally? |
06/07/2007 | |
What happens if a forward command and a reverse command are closed on the terminal block at the same time? |
11/28/2005 | |
What features does the Junma SERVOPACK have compared with other SERVOPACKS? |
08/15/2011 | |
What environments are suitable for the HV600 drives? |
09/03/2019 | |
What energizes (closes) and de-energizes (reopens) the "estop" relay in LEGEND-MC (SMC-3010)? |
07/13/2004 | |
What enclosure types are available for the V1000? |
07/27/2007 | |
What enclosure types are available for the R1000? |
07/15/2015 | |
What enclosure types are available for the D1000? |
07/15/2015 | |
What DriveWizard program does it use, and is it backwards compatible with E7? |
09/13/2012 | |
What do I need to Start Up a SigmaLogic motion axis? |
09/12/2014 | |
What do I do when I receive a "Selected collating sequence not supported by the operating system" error when running DriveWizard 6.2? |
09/13/2012 | |
What do I do in the case of freight damage? |
04/22/2014 | |
What do I do if I am having problems connecting to the A1000 USB port? |
09/27/2011 | |
What does the “E2005 the field offset exceeds the limit” compile error mean? |
01/30/2020 | |
What does the user need that Yaskawa doesn’t offer for using Compass? Is a PC required? |
02/11/2021 | |
What does the compiler message "Internal Error: Overflow. (Specific Code Generator)" mean and what is the remedy? |
03/12/2014 | |
What does the "-(A)" mean in the cable part number? |
07/13/2004 | |
What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |
10/27/2005 | |
What does it mean that, "motor protection time constant for the electrical termal device is 8 minutes"? |
11/28/2005 | |
What does "with volume" and "without volume" refer to? Some V7 manuals and catalogs use this terminology. |
06/20/2013 | |
What documentation ships with the Z1000U Matrix? |
01/21/2015 | |
What documentation ships with the Z1000? |
11/29/2011 | |
What documentation ships with the V1000-4X? |
06/21/2010 | |
What documentation ships with the V1000? |
07/27/2007 | |
What documentation ships with the R1000? |
07/15/2015 | |
What documentation ships with the product? |
01/14/2019 | |
What documentation ships with the product? |
09/03/2019 | |
What documentation ships with the P1000? |
06/29/2012 | |
What documentation ships with the GA500? |
09/30/2019 | |
What documentation ships with the D1000? |
07/15/2015 | |
What documentation ships with the A1000? |
01/03/2011 | |
What could cause motion commands sent to an EtherCAT axis to be executed by a different axis than intended? |
03/07/2014 | |
What could cause an motor to run away when it is enabled (/S-ON goes low)? |
07/13/2004 | |
What could be the problem if a computer cannot communicate to a LEGEND-MC over Ethernet? |
03/19/2002 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.