Support
Frequently Asked Questions
Question | Posted Date | |
---|---|---|
What are the differences between MECHATROLINK-II and MECHATROLINK-III? |
11/05/2013 | |
What are the details regarding P1000 12 Pulse? |
06/29/2012 | |
What are the details regarding A1000 12 Pulse? |
05/30/2012 | |
What are the details of CoE objects 2217h and 2216h? Are these parameters used to achieve an S-curve (jerk) motion? I see the descriptions in my controller after importing the Yaskawa ESI file, but in the Yaskawa CoE user's manual, these are not described. |
02/09/2015 | |
What are the D1000 ratings? |
07/15/2015 | |
What are the concerns when operating a motor with a AC drive rated for less output voltage than the motor namplate . Example: The AC drive rating is 480 VAC and the motor is 600VAC. |
08/19/2004 | |
What are the available jumper settings for the SMC-4000? |
06/25/2013 | |
What are the available jumper settings for the SMC-3010? |
06/25/2013 | |
What are the advantages of "Serial Command Method" when using an NS600 indexer? |
02/20/2003 | |
What are the additional pigtail leads on cables SMCCBLAxx and SMCCBLBxx? |
10/20/2006 | |
What are the A1000's ratings? |
01/04/2011 | |
What are some tips for operating a single load with multiple servo motors? |
03/12/2014 | |
What are some remedies to an A.C9 (Encoder Communications) alarm? |
07/13/2004 | |
What are some potential causes of an A.E2 alarm? |
06/24/2013 | |
What are some potential causes of an A.84 Alarm? |
06/30/2008 | |
What are some possible remedies if the #ININT (Input Interrupt) special label does not work? |
06/24/2013 | |
What are some possible causes for and FGN instruction error ? |
02/18/2009 | |
What are some of the potential causes of the A.E72 alarm? |
02/06/2009 | |
What are some of the potential causes of an A.80 Alarm? |
04/12/2006 | |
What are some methods for physical connections (wiring) to the MP920 218IF Ethernet Module? |
07/13/2004 | |
What are some issues that would cause a web application to drift when using camming with registration, and what are some remedies to this condition? |
07/13/2004 | |
What are some counter-measures to reduce harmonics created by AC drives? |
06/08/2007 | |
What are some concerns when the motor cable is over 100 meters? |
06/20/2013 | |
What are potential implications of using an Electro-Mechanical Relay or Switching Power Supply in conjunction with a Sigma II Servo System to enable the motor? Can A.C9 and A.E2 alarms be symptoms? |
07/13/2004 | |
What are cable leads +BA and -BA used for on cable SMCCBL0XX when using the SMC-4000? |
04/10/2006 | |
What applications is the Single Phase Converter appropriate for? |
02/08/2018 | |
What Add-On Instructions are available with SigmaLogic? |
10/29/2014 | |
What about UL Type enclosed packages? |
05/14/2020 | |
What A1000 enclosure types are available? |
01/03/2011 | |
We have two raycap options (7 & 9). When would I use option 7 verses option 9? |
05/13/2021 | |
UV -- Fault Code Description |
06/08/2007 | |
UV -- Fault Code Description |
06/08/2007 | |
UV3 -- Fault Code Description |
11/16/2009 | |
UV3 - Fault Code Description |
06/20/2013 | |
UV2 -- Fault Code Description |
06/08/2007 | |
UV2 -- Fault Code Description |
11/16/2009 | |
UV2 - Fault Code Description |
06/20/2013 | |
UV1 -- Fault Code Description |
11/16/2009 | |
UV1 - Fault Code Description |
06/20/2013 | |
UL3 -- Fault Code Description |
11/16/2009 | |
UL3 -- Fault Code Description |
06/08/2007 | |
UL3 (blinking) -- Fault Code Description |
06/08/2007 | |
The VG3 or VCD703 - Vector Drive uses terminals 30 and 31 as inputs for a motor thermistor. With no thermistor connected, the drive faults immediately. Is it possible to use a motor without a thermistor? |
06/07/2007 | |
The V7 Drive Jog Reference (S7) command is given. Why doesn't the motor move? |
07/13/2004 | |
The P5/506 bypass panel "Fault" light is ON, but no fault code is shown on the keypad display. What's wrong? |
06/11/2014 | |
The Motionworks IEC software stopped running after installing InteractX software? How can I recover from this? |
03/04/2010 | |
The MotionWorks IEC Hardware Configuration software is unable to connect to the MPiec controller. What should I check to correct the problem? |
09/23/2013 | |
The J7 drive will only allow the parameter to viewed but not changed.What must be done to change parameter values in the J7/305 AC drive? |
06/11/2014 | |
The HV600 is described as a fan and pump drive. Is there new pump control functionality built into the drive? |
09/03/2019 | |
The Hardware Configuration launches, but does not appear after using dual displays, is there a way to reset its position? |
08/04/2014 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.