Support
Frequently Asked Questions
Question | Posted Date | |
---|---|---|
The GUI displays mm. How can it change to inches? |
07/23/2021 | |
The GPD 515/G5 displays a parameter, but does not let me change it. Why? |
07/13/2004 | |
The GPD/515G5 instruction manual (TOE-S616-10.13) (pages 21-22) specifies that input fuses should be used on the installation of these drives.--Is fusing required or is a circuit breaker sufficient protection for the inverter?--If fusing is not required, what characteristics of MCCB should used be to protect the drive adequately? |
06/08/2007 | |
The E7L will not run the motor in Hand or Auto mode. What can cause this? |
10/27/2005 | |
The E7 drive inside the bypass enclosure unit doesn't have the Hand, Off or Auto buttons that are shown in the E7 manual. How can the drive be run locally? |
07/13/2004 | |
The E7B bypass unit with the serial communications, option J or option L control comes set up for the start/stop as well as the speed reference to be controlled through serial communication. Is it possible to maintain start/stop control through serial communication while using an analog signal for speed reference? |
06/11/2014 | |
The Drive Wizard .PARMS file was edited with another program (ie. Microsoft Word, Notepad) and saved. When reopened with DriveWizard, an error code of "File Error" was displayed on-screen. What is the problem and how can this be corrected? |
09/13/2012 | |
The Alarm output on the CACR HR Servopack no longer works. It is always open (or closed) regardless if the servopack is in an alarm state or not. What causes this situation? |
03/12/2002 | |
The AC drive repeatedly displays an OV (Overvoltage) fault when the inverter is stopping. What causes this? |
06/11/2014 | |
The "sleep" function can only be used when PID is enabled. If an analog (0-10VDC or 4-20mA) signal for speed reference is used, is there any way to use "sleep" without enabling PID? |
11/29/2005 | |
SVE -- Fault Code Description |
06/08/2007 | |
Specification of 12 pulse input transformer for GPD505/506- PC5/P5 series AC drive. |
06/12/2014 | |
Sometimes my machine power-up position is incorrect even though I have an absolute encoder on the motor. What is causing this issue? |
05/19/2015 | |
Some shape cutting OEMs consider their front-end interface as their differentiating feature over competitors. How would you make Compass attractive to OEMs like this? |
02/09/2021 | |
Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |
06/12/2014 | |
Serial communication is lost intermittently between the building automation system (BAS) and a Lonworks board on the GPD506 / P5 drive. What might be causing this? |
06/12/2014 | |
SER - Fault Code Description |
06/08/2007 | |
SC - Fault Code Description |
06/08/2007 | |
RR -- Fault Code Description |
11/16/2009 | |
RR -- Fault Code Description |
06/08/2007 | |
RH -- Fault Code Description |
11/16/2009 | |
RH -- Fault Code Description |
06/08/2007 | |
Product Demo Documentation: Sigma FSP |
06/26/2013 | |
Product Demo Documentation: NS300/NS500 |
06/26/2013 | |
Product Demo Documentation: MP940 |
06/26/2013 | |
Product Demo Documentation: MP2300 |
06/26/2013 | |
Power Line Harmonics and Installation Considerations for AC and DC Drives |
06/22/2006 | |
PGO -- Fault Code Description |
06/08/2007 | |
PF -- Fault Code Description |
11/16/2009 | |
PF - Fault Code Description |
06/08/2007 | |
OV -- Fault Code Description |
11/16/2009 | |
OV -- Fault Code Description |
06/08/2007 | |
OV -- Fault Code Description |
06/08/2007 | |
OV - Fault Code Description |
06/20/2013 | |
Other than OLV/PM parameters, is there other causes of OPE08? |
11/27/2012 | |
OS -- Fault Code Description |
06/08/2007 | |
OPR -- Fault Code Description |
06/08/2007 | |
OPR - Fault Code Description |
02/17/2016 | |
OPE -- Fault Code Description |
06/08/2007 | |
OPE11 -- Fault Code Description |
06/08/2007 | |
OPE10 -- Fault Code Description |
06/08/2007 | |
OPE08 -- Fault Code Description |
06/08/2007 | |
OPE07 - Fault Code Description |
06/08/2007 | |
OPE06 -- Fault Code Description |
06/08/2007 | |
OPE05 -- Fault Code Description |
06/08/2007 | |
OPE03 -- Fault Code Description |
06/08/2007 | |
OPE02 -- Fault Code Description |
06/08/2007 | |
oPA - Fault Code Description |
06/08/2007 | |
On what applications should the GPD 506/P5 be used? |
11/29/2005 | |
On the V7 Drive are the Logic inputs and the Logic Common terminal (SC) electrically isolated from the Frequency Reference Common (FC)? |
07/13/2004 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.