Support

Frequently Asked Questions

Didn't find what you were looking for? Try
  Question Posted Date

GF -- Fault Code Description

11/16/2009

GF - Fault Code Description

06/08/2007

FBL -- Fault Code Description

11/16/2009

FAN -- Fault Code Description

06/20/2013

F07 -- Fault Code Description

06/08/2007

F06 -- Fault Code Description

06/08/2007

F05 -- Fault Code Description

06/08/2007

F04 -- Fault Code Description

06/08/2007

F01 -- Fault Code Description

06/08/2007

F00 -- Fault Code Description

06/08/2007

ERR -- Fault Code Description

06/08/2007

EF -- Fault Code Description

06/08/2007

EF -- Fault Code Description

06/08/2007

EF7 -- Fault Code Description

11/16/2009

EF6 -- Fault Code Description

11/16/2009

EF5 -- Fault Code Description

11/16/2009

EF4 -- Fault Code Description

11/16/2009

EF4~8 -- Fault Code Description

06/08/2007

EF2 -- Fault Code Description

06/08/2007

E-15 -- Fault Code Description

06/08/2007

E-10 -- Fault Code Description

06/08/2007

During a generator to line transfer, the drive attempts to catch an already moving motor and faults with OL or OV. What steps can we take to prevent these alarms from occuring?

09/16/2013

During a generator to line power switchover, Uv1 results. Restart is not attempted. A manual reset is required for drives running motors. The transfer takes less than a second. Is there any fix for this issue?

09/16/2013

Do you need to have the Control Power on in order to use the Dynamic Braking features of the Sigma-5 Servopack?

03/06/2014

Do Yaskawa SGDH amplifiers work with Exlar linear actuators?

09/21/2004

Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters?

06/08/2007

Do Yaskawa's MPiec Series Controllers have a real-time clock?

03/12/2014

Do we have a USB cable interface (instead of serial) for hookup to laptops for DriveWizardTM Plus?

08/01/2008

Do we have a USB cable interface (instead of serial) for hookup to laptops for DriveWizard Plus?

07/27/2007

Do the remaining models fit in the same physical space as the discontinued models?

04/21/2014

Do the factory-provided grommets meet the UL Type 4X specification?

06/21/2010

Do Sigma II motors comply with standard NEMA flanges for mounting?

07/25/2005

Do I need to register for Yaskawa Drive Cloud account and if yes, how do I register?

08/03/2018

Does Yaskawa supply an EDS file for the MP940D (DeviceNet)?

07/13/2004

Does Yaskawa supply an EDS file for the MP920 [260-IF] DeviceNet module?

07/13/2004

Does Yaskawa sell the SGDM Sigma II amplifier in North America?

07/13/2004

Does Yaskawa offer USB drivers for communicating to the MP2200 CPU-02 from a PC ?

08/13/2013

Does Yaskawa offer software for selecting the best servomotor for a given application?

04/15/2015

Does Yaskawa offer Sigma II power and encoder cables rated for continuous flex?

06/24/2013

Does Yaskawa offer a template program for the MP940 when using MotionWorks+?

06/24/2013

Does Yaskawa manufacture 115VAC single-phase drives for 3 phase motor operation?

06/20/2013

Does Yaskawa have CAD dwgs. available for their servo system cables?

07/13/2004

Does Yaskawa have an example of a successful implementation of Yaskawa Product on a Shrink-Sleeve Labeling machine?

06/15/2010

Does the Z1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else?

09/13/2012

Does the V1000-4X meet UL?

06/21/2010

Does the V1000-4X meet NSF?

06/21/2010

Does the V1000-4x meet NEMA 4X?

06/21/2010

Does the V1000-4X meet IP66?

06/21/2010

Does the V1000-4X meet BISSC?

06/21/2010

Does the torque limit (sLimit_Torque) need to be set on the MP940?

05/02/2001

Does the sofware limit objects 607D:01h and 607D:02h include the home offset object 607Ch?

03/06/2014

Does the Sigma-5 have a function to reduce position dither when holding position?

07/01/2009

Does the R1000 need to be purchased as a kit similar to the RC5?

07/15/2015

Does the R1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else?

07/15/2015

Does the P1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else?

06/29/2012

Does the P1000 have a functional safety (safe torque off) input?

06/29/2012

Does the Modbus port on the V7 Drive need a termination resistor?

10/27/2005

Does the LEGEND amplifier have a circuit for a brake?

10/20/2006

Does the JUSP-NS500 Profibus Network Indexing module have a GSD file?

06/24/2013

Does the J1000 replace the J7?

09/13/2012

Does the J1000 mount contactor-style, like the J7 did?

08/01/2008

Does the J1000 have dynamic braking capability?

09/13/2012

Does the J1000 have DWEZ capability?

08/01/2008

Does the J1000 have a removable terminal block with parameter copy capability, like the V1000?

09/13/2012

Does the J1000 have any network communications capability?

08/01/2008

Does the D1000 need to be purchased as a kit?

07/15/2015

Does the D1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else?

07/15/2015

Does the A1000 have a USB cable interface (instead of serial) for direct connection to a computer, and do I need anything else?

02/29/2012

Does J1000 have UL Listing for single phase?

08/01/2008

Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration?

10/27/2005

Does BACnet support more than 128 addresses?

05/23/2013

DEV -- Fault Code Description

06/08/2007

CPF23 -- Fault Code Description

06/08/2007

CPF23 -- Fault Code Description

11/16/2009

CPF22 -- Fault Code Description

06/08/2007

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.