Support

Frequently Asked Questions

Didn't find what you were looking for? Try
  Question Posted Date

Where is the D1000 manufactured?

07/15/2015

Where Is the Compile Error Location When Double-Clicking On It?

03/08/2019

Where is the A1000 manufactured?

01/04/2011

Where do I send my repair item?

04/22/2014

Where do I install the network communication option card on the FP605 bypass?

02/17/2023

Where do I install the input/output option cards when using the FP605 bypass package?

02/17/2023

Where does the P1000 fit into Yaskawa's family of drives, and what does it offer beyond the P7?

06/29/2012

Where does the GA800 fit into Yaskawa's family of drives, and what does it offer beyond the A1000?

01/09/2019

Where does the GA500 fit into Yaskawa's family of drives?

09/26/2019

Where does the FP605 fit into Yaskawa's family of drives?

03/29/2022

Where does the A1000 fit into Yaskawa's family of drives, and what does it offer beyond the F7?

01/03/2011

Where can pin out details for the YS-12 cable be found?

07/13/2004

Where can I find UL certification documents for Yaskawa MPiec Controller products?

06/12/2014

Where can I find the supporting documents for UL approval of the MP2000 controllers?

02/04/2011

Where can I find frequently asked questions for MV1000?

03/31/2015

Where can I find electrical and mechanical drawings?

03/26/2021

Where can Error Code Descriptions be found for SigmaLogic?

10/20/2014

Where are the help files located for SigmaLogic, LogicWorks and Add-on Instructions (AOI)?

10/09/2014

When will single phase input capacities be available for P1000 and what kind of derating is expected?

06/29/2012

When will single phase input capacities be available for A1000 and what kind of derating is expected?

01/03/2011

When will a heatsink through the back solution be available, and what enclosure rating will it be capable of?

11/29/2011

When using the analog output function on a GPD506/P5, how is the output scaled when output current is selected?

06/12/2014

When using SMC-2000 analog input, where is the ground (common) signal connected?

05/22/2001

When using SigmaWin software, what are the units when graphing torque?

07/13/2004

When using MotionWorks IEC ver3.3.0, how can the error message “Library does not exist” be avoided when saving the Hardware Configuration?

01/27/2017

When using MotionWorks+, is there a way to tell which version of a project is currently in the RAM memory of the MP940 and the last date it was revised?

07/13/2004

When using DriveWizard HVAC on a Z1000 Bypass do I connect to the Z1000 Drive or the Electronic Bypass Contol PCB?

05/23/2013

When using Bluetooth, can I rename the drive so that I can more easily identify it?

01/16/2020

When using an MP920's SVA Servo interface and an absolute encoder on a Sigma II Servopack (SGDH), how is the absolute data requested and confirmed complete in the application program?

09/21/2004

When using an absolute encoder, is it possible to set the absolute zero position through the Fieldbus Network?

01/09/2002

When using 2 option cards, I am receiving an OPE06 fault and am not seeing all the F1 parameters. I am using CN5-B for my encoder feedback card.

10/09/2012

When the personal computer (PC) serial port connection is disconnected from the controller, why does the SMC-2000/3010/4000 controller become unresponsive?

07/13/2004

When the E7 drive trips out on a fault it must be manually reset. Can the E7 be set to restart automatically after a fault?

06/08/2007

When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications?

02/18/2009

When setting parameter Pn300 (Speed Reference Input Gain) what rated speed should be used for Linear Motor applications?

07/13/2004

When running into hardware limits, motion is disabled in both directions. How can the axis be jogged off the limit switch?

07/13/2004

When replacing the motor for the application and the heat sink cooling fans. How do I reset Cumulative Motor Operation Time U1-13 and Heat Sink Cooling Fan Operation Time U1-40?

09/16/2013

When reading 42h it does not match U1-03? Using Ethernet or Modbus protocols.

08/31/2012

When moving away from a overtravel condition, the Sigma V servo system seems to prevent torque or rapidly enable/disable as the axis is moving out of the overtravel region. Can this situation be prevented?

10/06/2011

When is it necessary to connect an external regen resistor to the SGDG LEGEND amplifier?

01/21/2002

When I install my serial communications option board onto the Z1000 drive in the Z1B cabinet, I recieve alarm OFA00. What am I doing wrong?

02/28/2013

When entering Motor Rated Current (parameter E2-01) into an E7 drive, an OPE02 fault appears on the display. What can cause this, and how is the fault cleared?

06/08/2007

When dealing with harmonic noise, which is better-- an AC or a DC reactor?

06/20/2013

When configuring an IP address in the resource settings of MotionWorks IEC, what are the -TO and -P attributes?

11/10/2017

When an MP940 with a 17-bit encoder is being operated, does the encoder resolution need to be reduced?

04/27/2001

What’s the maximum number of axes that could be controlled and configured by a Compass solution?

05/21/2020

What Z1000 enclosure types are available?

11/29/2011

What would cause an "06" communications error code in an HMI when talking to one or more NS600(s)?

11/21/2001

What will happen to the P7?

06/29/2012

What will happen to the E7?

11/29/2011

What will happen if there is only .5'' clearance from either top or bottom of the drive to an enclosure?

03/14/2006

What web browser technology is supported by the MPiec Series Controllers?

01/02/2018

What web browsers are compatible with the MPiec controller's web server?

04/04/2024

What voltage levels will cause an overvoltage or undervoltage alarm?

03/02/2015

What voltage levels will cause an overvoltage or undervoltage alarm?

02/06/2009

What version of Sigma II fimware is required if using an option card such as the MP940?

04/04/2002

What version of Java is required to view the Machine Operations page of an MPiec Controller?

07/04/2013

What type of Errors and Alarms are on the controller?

02/18/2009

What training is available for P1000?

06/29/2012

What training is available for HV600?

09/03/2019

What training is available for GA800?

01/11/2019

What training is available for A1000?

01/03/2011

What tools are available to help customers convert from P7 to P1000?

06/29/2012

What tools are available to help customers convert from G5 (600V) and F7 to A1000?

01/03/2011

What tools are available to help customers convert from F7 and A1000 to GA800?

01/11/2019

What tools are available to help customers convert from E7 to Z1000?

11/29/2011

What tools are available to help customers convert from E7 and Z1000 to HV600?

09/03/2019

Whats the maximum number of User Function blocks that can be used in the MP900 series controllers?

03/06/2002

What steps are required to upgrade Sigma products to Sigma II?

04/10/2006

What steps are required to communicate to a LEGEND-MC from a laptop PC via Ethernet?

07/13/2004

What steps are necessary to connect a Yaskawa V1000 to an MPiec series controller over ethernet?

02/26/2021

What software tools are available to save F7 drive parameter settings to a PC file?

09/13/2012

What should the inertia ratio parameter, Pn103, be set to in the Sigma II amplifier when the inertia ratio is not known?

06/24/2013

What should be done with the CN8 connection when using the Safety Option Module (SGDV-OSA01A)?

06/09/2023

What settings are needed to configure the E7 Bypass for serial communication control in AUTO mode and keypad speed control in HAND mode?

06/11/2014

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.