Support

Frequently Asked Questions

Didn't find what you were looking for? Try
  Question Posted Date

What screen resolutions are supported by Compass?

05/21/2020

What screen resolutions are compatible with Compass?

04/28/2020

What peripheral components are required for use with the R1000 for UL?

07/15/2015

What peripheral components are required for use with the D1000 for UL?

07/15/2015

What PC tools are available for the FP605?

04/07/2022

What parameter sets the maximum output frequency for V7 series drives?

06/20/2013

What parameter must be set when using a DC power supply for a SERVOPACK’s main circuit power supply?

02/26/2019

What panel options are available for the U1000 Type 1 and Type 3R packages?

03/26/2021

What P1000 enclosure types are available?

06/29/2012

What options are supported on the FP605 configured package?

02/17/2023

What options are supported on the FP605 bypass package?

02/17/2023

What options are available to stop the motor using EtherCAT commands?

12/22/2015

What options are available to limit torque on the SGDV CANopen over EtherCAT SERVOPACK?

07/15/2015

What new features does the Z1000 offer beyond those of the E7?

11/29/2011

What network protocols does the Z1000U support?

01/21/2015

What motors can the GA500 operate?

09/30/2019

What motors can the FP605 operate?

03/30/2022

What might be the cause of a brake relay chattering (turning on and off rapidly) on a vertical axis?

07/13/2004

What manuals are required to start-up, operate, and program a LEGEND-MC Motion Controller?

10/30/2001

What makes the HV600 more convenient to program and set up?

09/03/2019

What keypad options are available for the GA500?

09/30/2019

What is Yaskawa’s repair policy for Sigma SD?

02/21/2018

What is Yaskawa DriveCloud, and what products does it support?

06/19/2022

What is the Yaskawa Solution Center and how do I use it?

02/22/2019

What is the wiring diagram for the MP920/MP930 programming cable?

07/13/2004

What is the warranty determination for new product?

05/22/2014

What is the vertical and horizontal clearance specification (in inches) for mounting any of the GPD506/P5 stand alone drives?

11/28/2005

What is the SCCR of the GA500?

09/30/2019

What is the SCCR of the FP605?

04/12/2022

What is the scan rate of the V1000?

07/27/2007

What is the scan rate of the A1000?

01/04/2011

What is the recommended system requirement for Compass? Processor, memory, etc.

05/21/2020

What is the reason for the long deceleration when using a Direct Drive Motor system with a Sigma 2 Servopack (SGDH) and MP940? What are the steps to properly tune such a system?

07/25/2005

What is the rating of the GA500’s 24 Vdc output?

09/30/2019

What is the rating of the FP605’s +24 VDC output?

03/31/2022

What is the rated current of the 24VDC holding brake on Sigma II motors?

07/13/2004

What is the purpose of the TEST switch on the front panel of an E7B bypass unit?

06/08/2007

What is the purpose of the Near Output Signal (/NEAR) in Sigma II drives?

01/13/2003

What is the purpose of a softcharge resistor and contactor in a GPD506 / P5 drive?

11/28/2005

What is the proper value to enter in Pn600 when Yaskawa Regenerative Resistor Unit is used?

07/13/2004

What is the proper sequence to reset a SigmaLogic Alarm?

03/08/2016

What is the procedure to setup a rotary axis in MP controllers using MotionWorks?

08/19/2004

What is the procedure to reset an MPiec controller back to factory defaults?

01/27/2017

What is the procedure to replace an FSP to keep the parameters including the motor parameters in the case of using a third party motor?

04/02/2016

What is the procedure for changing the motor rotation direction with a LEGEND-MC controller?

07/13/2004

What is the power-up sequence for the MP940?

07/13/2004

What is the power range of FP605 configured packages?

02/17/2023

What is the power range of FP605 bypass packages?

02/17/2023

What is the outer diameter of SGMAV/SGMJV Premium motor power cables?

03/17/2016

What is the most common solution to communication errors in a Mechatrolink Network?

06/24/2013

What is the memory capacity for the MP2000 IEC Controllers?

01/05/2011

What is the memory allocation for the MPiec Controllers?

01/17/2018

What is the meaning of CAL or CALL on the keypad display?.

10/28/2005

What is the maximum value of pLimit_PositioningError?

12/21/2001

What is the maximum size of G file supported by Compass?

05/21/2020

What is the maximum setting for parameter Pn281 (PG Divider) given the linear scale pitch and maximum speed of the linear motor?

07/13/2004

What is the maximum sample rate used in the trending graphic on current Drivewizard software?

12/10/2013

What is the maximum output frequency of the GA500?

09/27/2019

What is the maximum output frequency of the FP605?

03/30/2022

What is the maximum number of cam data points that can be stored in a cam table?

07/13/2004

What is the maximum frequency limitation of the pulse input?

07/27/2007

What is the maximum connection distance of the Bluetooth keypad?

09/26/2019

What is the life expectancy of a Sigma-5 motor when operating above 40 degrees Celsius (104 F)?

10/18/2010

What is the latest driver for the EXOR HMI connected to an SMC controller, and does it provide hardware handshaking?

06/24/2013

What is the keying of the SGMGV & SGMSV motors, and what is the keying of the SGMGV & SGMSV Yaskawa preassembled right-angle cables for motor power, brake, fan, and encoder?

03/13/2014

What is the inrush current of an SGDH amplifier?

04/16/2001

What is the input voltage rating of FP605 configured packages?

02/17/2023

What is the input voltage rating of FP605 bypass packages?

02/17/2023

What is the functional safety rating of the GA500?

09/30/2019

What is the functional safety rating of the FP605?

03/30/2022

What is the format of the Floating Point data structure in the MP920, MP930, MP940 series products?

07/13/2004

What is the factory warranty for Sigma SD?

02/21/2018

What is the difference between Z registers and A registers when used in Function Blocks?

04/30/2002

What is the difference between the JVOP-183 and JVOP-183R? (or what is meant by back lit?)

07/09/2013

What is the difference between the I/O on the Sigma II and the MP940? Do both need to be used?

04/26/2001

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.