Support

Frequently Asked Questions

Didn't find what you were looking for? Try
  Question Posted Date

What is involved with converting from "Relay Type" extended I/O ("I" option) to Solid State I/O ("J" Option) on an SMC-2000?

04/01/2009

What is EN954-1 Safety Category 3?

07/27/2007

What is EN61800-5-1 and TUV?

01/04/2011

What is DriveWizard Mobile, and what products does it support?

01/14/2019

What is a typical cause of error code 4630 when using MC_TouchProbe?

04/02/2016

What is an SVA module?

06/25/2013

What is an SSFDC Memory Card?

06/24/2013

What is Analog Resistive Touch Screen Technology?

12/21/2011

What is an A.F50 Alarm?

03/03/2015

What is an A.E7 alarm and how is it cleared?

07/13/2004

What is an A.E5 alarm?

01/22/2002

What is an A.9F alarm?

09/12/2000

What is an A.09 alarm?

12/22/2011

What is a "Multi-Function Digital Input"?

09/13/2012

What is a "DWG" (drawing)?

05/02/2001

What is 2-Wire Control and 3-Wire Control?

07/13/2004

What is +P common

02/13/2013

What information is available for implementing PLCopen "Function Blocks for Motion Control" in the MP2000 series products?

07/24/2013

What if an MP2300 module needs to be replaced? Is the module configuration stored in the main CPU?

12/19/2006

What I/O cable options exist for the NS600?

07/18/2014

What I/O cable options are there for the NS500?

09/21/2004

What I/O cable options are there for the NS300?

09/21/2004

What I/O cable options are there for the MP940?

11/29/2004

What happens when switching to reverse while the motor is rotating forward (FWD=OFF, REV=ON)?

11/28/2005

What happens if the STOP button on the Digital Operator is pressed, while the drive is being controlled remotely by START/STOP circuitry connected to the drives I/O terminal block? Can the drive be restarted locally?

06/07/2007

What happens if a forward command and a reverse command are closed on the terminal block at the same time?

11/28/2005

What features does the Junma SERVOPACK have compared with other SERVOPACKS?

08/15/2011

What energizes (closes) and de-energizes (reopens) the "estop" relay in LEGEND-MC (SMC-3010)?

07/13/2004

What enclosure types are available for the V1000?

07/27/2007

What enclosure types are available for the R1000?

07/15/2015

What enclosure types are available for the J1000?

09/13/2012

What enclosure types are available for the D1000?

07/15/2015

What DriveWizard program does it use, and is it backwards compatible with E7?

09/13/2012

What do I need to Start Up a SigmaLogic motion axis?

09/12/2014

What do I do when I receive a "Selected collating sequence not supported by the operating system" error when running DriveWizard 6.2?

09/13/2012

What do I do in the case of freight damage?

04/22/2014

What do I do if I am having problems connecting to the A1000 USB port?

09/27/2011

What does the “E2005 the field offset exceeds the limit” compile error mean?

01/30/2020

What does the compiler message "Internal Error: Overflow. (Specific Code Generator)" mean and what is the remedy?

03/12/2014

What does the "-(A)" mean in the cable part number?

07/13/2004

What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display?

10/27/2005

What does it mean that, "motor protection time constant for the electrical termal device is 8 minutes"?

11/28/2005

What does "with volume" and "without volume" refer to? Some V7 manuals and catalogs use this terminology.

06/20/2013

What documentation ships with the Z1000U Matrix?

01/21/2015

What documentation ships with the Z1000?

11/29/2011

What documentation ships with the V1000-4X?

06/21/2010

What documentation ships with the V1000?

07/27/2007

What documentation ships with the R1000?

07/15/2015

What documentation ships with the product?

01/14/2019

What documentation ships with the P1000?

06/29/2012

What documentation ships with the J1000?

08/01/2008

What documentation ships with the GA500?

09/30/2019

What documentation ships with the D1000?

07/15/2015

What documentation ships with the A1000?

01/03/2011

What could cause motion commands sent to an EtherCAT axis to be executed by a different axis than intended?

03/07/2014

What could cause an motor to run away when it is enabled (/S-ON goes low)?

07/13/2004

What could be the problem if a computer cannot communicate to a LEGEND-MC over Ethernet?

03/19/2002

What Control Methods does the V1000 offer?

07/27/2007

What control methods does the P1000 offer?

06/29/2012

What Control Methods does the J1000 offer?

08/01/2008

What control methods does the A1000 offer?

01/04/2011

What changes must be made in the program when switching from a 218IF-01 (JAPMC-CM2300-E) card to a 218IF-02 (JAPMC-CM2302-E) card on the MP2000 series controller platform?

03/10/2015

What causes ‘CPU Status: Stopped’ and how can it be fixed?

09/12/2014

What causes the MPiec Controller’s WebUI to report "Not a valid firmware file" when uploading a firmware?

06/13/2016

What causes the MotionWorks IEC error message "The project cannot be downloaded because it was compiled for a different device or a different version of the connected device. Please select the device version in the Resource Settings Dialog that matches the connected device."

09/13/2018

What causes FLT_BSY output to come on at a SigmaLogic AOI block?

09/15/2014

What causes an E19A alarm on the NS600 indexer and how is the error corrected?

07/13/2004

What CASE Software is available for the V1000-4X?

06/21/2010

What CASE Software is available for the J1000?

08/01/2008

What can cause a MotionWorks IEC 3.x USB license key to be unrecognized?

01/27/2017

What are the Z1000 ratings?

09/13/2012

What are the vibration specifications for Sigma II Motors?

06/30/2008

What are the V1000-4X's ratings?

06/21/2010

What are the units of the Sigma 2 Servopack (SGDH) Parameters, Pn301 (Contact Input Speed1), Pn302 (Contact Input Speed2), Pn303(Contact Input Speed3) and Pn304 (Jog Speed) when a Direct Drive motor is connected?

09/06/2004

What are the system requirements for DriveWizard Mobile?

08/03/2018

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.