Support

Frequently Asked Questions

Didn't find what you were looking for? Try
  Question Posted Date

Specification of 12 pulse input transformer for GPD505/506- PC5/P5 series AC drive.

06/12/2014

Sometimes my machine power-up position is incorrect even though I have an absolute encoder on the motor. What is causing this issue?

05/19/2015

Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive?

06/12/2014

Serial communication is lost intermittently between the building automation system (BAS) and a Lonworks board on the GPD506 / P5 drive. What might be causing this?

06/12/2014

SER - Fault Code Description

06/08/2007

SC - Fault Code Description

06/08/2007

RR -- Fault Code Description

06/08/2007

RR -- Fault Code Description

11/16/2009

RH -- Fault Code Description

06/08/2007

RH -- Fault Code Description

11/16/2009

PUF -- Fault Code Description

06/08/2007

PUF -- Fault Code Description

11/16/2009

Product Demo Documentation: Sigma FSP

06/26/2013

Product Demo Documentation: NS300/NS500

06/26/2013

Product Demo Documentation: MP940

06/26/2013

Product Demo Documentation: MP2300

06/26/2013

Power Line Harmonics and Installation Considerations for AC and DC Drives

06/22/2006

PGO -- Fault Code Description

06/08/2007

PF -- Fault Code Description

11/16/2009

PF - Fault Code Description

06/08/2007

OV -- Fault Code Description

11/16/2009

OV -- Fault Code Description

06/08/2007

OV -- Fault Code Description

06/08/2007

OV - Fault Code Description

06/20/2013

Other than OLV/PM parameters, is there other causes of OPE08?

11/27/2012

OS -- Fault Code Description

06/08/2007

OPR -- Fault Code Description

06/08/2007

OPR - Fault Code Description

02/17/2016

OPE -- Fault Code Description

06/08/2007

OPE11 -- Fault Code Description

06/08/2007

OPE10 -- Fault Code Description

06/08/2007

OPE08 -- Fault Code Description

06/08/2007

OPE07 - Fault Code Description

06/08/2007

OPE06 -- Fault Code Description

06/08/2007

OPE05 -- Fault Code Description

06/08/2007

OPE03 -- Fault Code Description

06/08/2007

OPE02 -- Fault Code Description

06/08/2007

oPA - Fault Code Description

06/08/2007

On what applications should the GPD 506/P5 be used?

11/29/2005

On the V7 Drive are the Logic inputs and the Logic Common terminal (SC) electrically isolated from the Frequency Reference Common (FC)?

07/13/2004

On the V1000 series drive, should the H1, HC circuit be used with an external 24V supply?

10/21/2013

On the J7 drive, can the input reference terminal FR still be used when the drive is programmed for Up/Down control?

06/20/2013

On the GPD 515/G5, If Terminal 1 to 11 are closed, but the GPD515/G5 inverter still does not run. What is wrong?

07/13/2004

On the GPD 515/G5, can the 15V at pin-15 power a proximity sensor?

07/13/2004

On the GPD503, why does the Stop LED continue to flash after the drive has stopped runnning?

06/20/2013

On the A1000 series, if a unidirectional 3-wire control is desired, can the directional digital input (H1-0X = 0) be disabled?

11/13/2013

On an MPiec Series Controller, what information is cleared when the "Initialize SRAM" feature is executed?

08/16/2013

On an MP2600iec, is it possible to use the CN-13 latch input instead of the CN-1 latch input?

02/28/2017

On a linear motor x-x'-y gantry system, what is the best method to control the two x-axes?

06/06/2003

On a GPD 506/P5 Bypass unit, what is the Normal/Test switch used for and when would it be needed in an operation?

07/13/2004

OL4 -- Fault Code Description

09/13/2012

OL3 -- Fault Code Description

06/08/2007

OL3 -- Fault Code Description

06/08/2007

OL3 -- Fault Code Description

06/08/2007

OL3 -- Fault Code Description

06/21/2010

OH -- Fault Code Description

06/08/2007

OH -- Fault Code Description

06/08/2007

OH4 -- Fault Code Description

11/16/2009

OH3 -- Fault Code Description

06/08/2007

OH3 -- Fault Code Description

11/16/2009

Off -- Fault Code Description

09/19/2013

My drive has a CPF25 fault on it, my V1000 manual has no information on this alarm. What are some troubleshooting techniques to apply?

10/29/2012

Must the data type be the same for every variable in a calculation? I get a compile error when I try (REAL := REAL * INT).

05/26/2009

Many new computers do not offer serial communication ports. How is communication possible to Yaskawa products if no serial port is available?

06/25/2013

Many HMI products have a battery compartment. What is the battery used for?

05/22/2001

LF -- Fault Code Description

06/08/2007

I’m using a third-party EtherCAT master. What do I need to know in regards to the Yaskawa drive interface?

03/16/2015

I want the motor never to run below a certain speed and I am using PID, but there may be times when this low speed will be "too much". Is there a solution for this?

11/29/2005

It is possible to install a single licensed copy of MotionWorks IEC on multiple computers and move the license from computer to computer?

01/26/2016

I there a list of troubleshooting items to follow when using the SMC4000 and a Sigma Absolute Encoder?

12/21/2011

Is upgrading from Sigma to Sigma II the best option?

04/13/2006

Is the Z1000 the same physical size as E7

11/29/2011

Is the V1000-4X rated for outdoor use?

06/21/2010

Is the V1000-4X corrosion-resistant?

06/21/2010

Is the V1000-4X coated with food-grade paint?

06/21/2010

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.