MV1000 Drive Startup and Field Troubleshooting
Class Name/Number: | MV1000 Drive Startup and Field Troubleshooting / TRM015-MV1000 View Related Curriculum |
Class Cost: | $1100 |
Duration: 3 Days
Class Topics:
The MV1000 class is designed for technicians and engineers that need an overall understanding of the product. Both hardware and software will be explained with props, pictures and hands on exercises. First the student will learn about the overall drive layout and construction. Next, the student will learn the proper startup procedure using a real MV1000 drive. Using the drive's fault codes, the student will also learn how to identify problems pertaining to drive components (like cooling fans and power cells) and the proper method of replacing them. Basic drive parameters will be discussed as well as drive monitors and auto tuning.
Class topics include but are not limited to:
- Overview of Drive Specifications
- Elementary Review
- Keypad Usage
- Start-up Procedure using actual unit
- Field Troubleshooting
- How to change Power Cells and Fans
Class Materials:
Students will receive a copy of the class training manual as well as selected product user and instruction manuals in paper and/or electronic format.
COVID Policies During Training Classes:
Yaskawa America, Technical Training Services follows the Center for Disease Control’s (CDC’s) recommendation of social distancing at least six feet during factory training classes held at the Yaskawa America facility in Waukegan, IL. To meet these recommendations, we’ve physically rearranged the classrooms and limited the number of students enrolled in the class.
Students and instructors must adhere to Yaskawa's safety protocol for mask or face shield utilization in all Yaskawa training facilities, which follow local, state or federal mask orders or revised CDC guidelines. Students should bring with them and may wear during the class, a facemask or face shield approved by the CDC for COVID-19 face protection based on Yaskawa’s safety protocol level at the time of their scheduled class.
Safety:
This training class requires the use of low level voltages (120Vac, 208Vac and 460Vac). To ensure a level of safety for the student while working with training class equipment using these voltages, TTS follows an Arch Flash Policy that is consistent with NFPA 70E. Each student attending this class must wear non-melting, untreated, natural fiber long pants as well as steel toe electrical hazard (EH) rated safety shoes. Each student must also wear the proper personal protective equipment supplied by Yaskawa America.
This training class also requires the use of medium level voltages (2300Vac and 4160Vac). To ensure a level of safety for the student while working with training class equipment using these voltages, each student attending this class must wear non-melting, untreated, natural fiber long pants as well as steel toe electrical hazard (EH) rated safety shoes. Each student must also wear the proper personal protective equipment supplied by Yaskawa America.
Prerequisites:
1. No prerequisites, however, it would be helpful if the attendee has some experience programming any of Yaskawa's drives as well as prior involvement with medium voltage products.
If you're not sure if this class is right for you, call and speak with one of Yaskawa's Product Training Engineers at 1-800-YASKAWA (927-5292) dial 41.
Class Format:
This three day class is held from 8:30 am to 5:00 pm, with a one-hour lunch and two 15-minute breaks.
The class consists of approximately 50% hands-on exercises and 50% lecture.
Continuing Education Units:
Continuing Education Units will be awarded to those students that attend this training class in its entirety and pass the certification test with a score of 90% or better. Yaskawa does not provide partial CEU credits for less than 100% attendance. As an IACET Accredited Provider, Yaskawa America Inc. offers CEUs for its programs that qualify under the ANSI/IACET Standard. Yaskawa America, Inc. is accredited by IACET to offer 2.1 CEUs for this program.
Class Cost:
$1100 per student. Contact Yaskawa for pricing at 1-800-YASKAWA (927-5292) dial 41. The fee that you will be charged includes all training documents, a light snack each morning, and a lunch each day. Costs associated with travel, lodging, and evening meals are not included and are the student's responsibility.
To Enroll:
To enroll in any scheduled class, go to Request Training or call 1-800-YASKAWA (927-5292), dial 41. Class sizes are limited, so call early to reserve your seat.
Cancellation/Refund Policy:
Yaskawa reserves the right to cancel a scheduled class at anytime due to low student enrollment. In this situation the student will be asked to reschedule or the tuition cost will be refunded. Yaskawa is not liable for any charges incurred by the customer (i.e.; airline, hotel, and rental car) due to cancellation.
A student may cancel their enrollment more than one week before the start of the class with no penalty. A student wishing to cancel their enrollment within one week of the class start date will be subject to these charges:
- The cancellation fee for end users, if canceling within one week for a scheduled factory class is 0% of the total class tuition fee.
- The cancellation fee for Drives and Motion Distributors, if canceling within one week of a scheduled factory training class is 100% of the total tuition fee.
- The cancellation fee for end users and distributors, if canceling an on-site class within three weeks of a scheduled class date is 100% of the class tuition and logistical fees.